show the entry list
ProTool -- Operation and maintenance -- Diagnosing errors
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
Why can you not transfer the configuration from the PC to the Windows CE-based panel?
Interruption of setup when updating ProTool (Pro/Lite) V5.2 from SP2 to SP3. Error message: "Cannot process Ptreg.dat"
Error message when connecting tags again
Memory problems with graphics
Error message when configuring a tag in a ProTool/Pro PC project with OPC connection
ProTool V3.00 Font problems / incorrect character sets
ProTool -- Setting up development environments -- Installing and upgrading software
How do you do an operating system update (OS update) on operator panels?
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
Interruption of setup when updating ProTool (Pro/Lite) V5.2 from SP2 to SP3. Error message: "Cannot process Ptreg.dat"
Only one language version ProTool /Lite /Pro can be installed at any one time
Installing ProTool without ProAgent
Function keys are lost in the configuration
ProTool: Switching from integrated to standalone/not integrated
Various versions of ProTool/Pro/Lite on one operating system
Installation of ProTool V6.0 or  ProTool V6.0 Service Packs aborted with error message "-132" 
Installation of ProTool V6.0 SP1 in MS Windows 2000 SP3
What should you watch out for to ensure successful installation of ProTool Lite, ProTool and ProTool/Pro?
Complete uninstallation of ProTool/Lite, ProTool and ProTool/Pro
Advantages of Configuring with ProTool integrated in STEP 7
Upgrade installation from ProTool/Pro V6.0 SP3 to MS Windows XP Professional
Interruption of setup when updating ProTool (Pro/Lite) V5.2 from SP2 to SP3. Error message: "Cannot process Ptreg.dat"
Part number:

QUESTION:
What can cause the appearance of an error message when updating ProTool (Pro/Lite) V5.2 from SP2 to SP3?

ANSWER:
At a level of about 35% completion of updating your setup aborts with the message "Cannot process Ptreg.dat".

Cause:
There are multiple different versions of the "PTREG.DLL" file on your computer.

Remedy:
Via "Start > Find > Files or Folders…" find all the files with the name "PTREG.DLL" on your local hard disks. Delete all them except the one in the ProTool directory.

Note:
The correct file must have the following properties:
"Version 5.3.0.23 of 04.08.2000 02:11"
You can have these file properties displayed by right-clicking the "PTREG.DLL" file in the ProTool directory and selecting "Properties".

Keywords:
Update


 Entry ID:7268288   Date:2001-04-26