show the entry list
Network transitions and links (DP) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you parameterize IO Link master and devices across gateways with the S7 Port Configuration Tool (S7-PCT)?
How do you configure the DP/PA link or the Y link in the external master / STEP 7 V12 (TIA Portal)?
How do you link the AS-i Slaves to an S7-300 CPU with integrated PROFINET interface using the IE/AS-i Link?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 via PROFIBUS using S7 Communication and incorporating an IE/PB Link gateway?
Where do you find sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 using S7 communication and incorporating an IE/PB link gateway?
Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB
How do you configure a ring redundancy with FDC 157-0 DP/PA couplers and active field distributors (AFDs)?
How do you connect a SIMATIC S7-300 as DP slave to a Y link in the hardware configuration of STEP 7?
Which options do you have for accessing PROFIBUS devices from a PC behind an IWLAN/PB link PN IO or an IE/PB link PN IO?
How do you connect the IM 157/IM 153-2 in the DP/PA Link to an external master or a SIMATIC S5? (GSD tool)
Incorporating new LINK modules in PCS7 V4.02
Set-up restrictions when using universal modules
Reduced user data capacity when using the diagnostics
Reading the input data of a DP slave configured by a different DP master
How do you configure an S7-300 CPU or a CP342-5 as DP slave to an S7-400H as DP master using a Y-link?
Configuration of the I/O Data on DP/DP Coupler
Retrieve Diagnostics of the DP/AS-i Link 20E
Configuring I/O addresses with DP/AS-i Link 20E
What are the special features of input/output addressing with the DP/DP coupler?
Where do you find sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway?
Part number:

Description
This entry contains sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway.
A CP443-1 Advanced is used, which is configured as a PROFINET IO controller, in the S7-400. The S7-300 is connected as an I slave to the PROFINET IO controller via an IE-to-PB link.

The sample program consists of a STEP 7 project containing the configuration of the S7-400 as a PROFINET IO controller, as well as the configuration of the S7-300 as an I slave.

QS_IE-PB-LINK-Routing.zip ( 321 KB )

The document below contains

  • An overview of the sample program and plant configuration used to create the sample programs
  • Information about installing and commissioning the sample program
  • Information about how to use the sample programs
  • Other notes, tips and tricks, etc.

NET_communication_from_IE_to_PB_via_routing_en.pdf ( 397 KB )

More information
More information about communication between PC station and SIMATIC S7 via network components is available in the entries below.
 
Description Entry ID
S7-CPs for Industrial Ethernet Configuration and Commissioning Part A - General Application 30374198
Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual 30564821
CPU-CPU Communication with SIMATIC Controllers (Compendium) 20982954
Network Gateway IE/PB Link PN IO for Industrial Ethernet / Manual Part BL1 19299692
From PROFIBUS DP to PROFINET IO 19289930
SIMATIC PROFINET System Description 19292127

 Entry ID:50562572   Date:2011-08-03