show the entry list
WinCC flexible ES -- Setting up development environments -- Installing and upgrading software
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
What do you have to do if you can no longer access symbols and data blocks of STEP 7 from an integrated WinCC flexible project?
Which security measures help against unauthorized access to computer systems with WinCC flexible?
Compatibility Tool for Automation and Drive Technology
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
Why can you not select the installed languages in the Runtime Loader of PC Runtime?
When you install or uninstall WinCC flexible, why are some fonts no longer available for STEP 7 Basic V10.5?
How do you do an operating system update (OS update) on operator panels?
Why can't you install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 after installing WinCC flexible 2008?
What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?
What are the solutions offered for working with different versions of WinCC flexible?
What can cause the installation to abort or prevent successful starting of WinCC flexible?
Where can you procure HSPs (Hardware Support Packages) for WinCC flexible?
What might be the cause for not all the user interface languages being available for selection?
What might be the causes of unsuccessful MSDE installation (Microsoft Desktop Engine)?
What are the possible causes of the Setup program not starting for the installation of WinCC flexible?
How can you clear the cause of the message "Please reboot before installing any more programs"?
How do you uninstall WinCC flexible 2004?
How do you install ProAgent in SIMATIC WinCC flexible?
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?
How can you install WinCC flexible from the hard disk?
ProTool -- Setting up development environments -- Installing and upgrading software
How do you do an operating system update (OS update) on operator panels?
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
Interruption of setup when updating ProTool (Pro/Lite) V5.2 from SP2 to SP3. Error message: "Cannot process Ptreg.dat"
Only one language version ProTool /Lite /Pro can be installed at any one time
Installing ProTool without ProAgent
Function keys are lost in the configuration
ProTool: Switching from integrated to standalone/not integrated
Various versions of ProTool/Pro/Lite on one operating system
Installation of ProTool V6.0 or  ProTool V6.0 Service Packs aborted with error message "-132" 
Installation of ProTool V6.0 SP1 in MS Windows 2000 SP3
What should you watch out for to ensure successful installation of ProTool Lite, ProTool and ProTool/Pro?
Complete uninstallation of ProTool/Lite, ProTool and ProTool/Pro
Advantages of Configuring with ProTool integrated in STEP 7
Upgrade installation from ProTool/Pro V6.0 SP3 to MS Windows XP Professional
ProTool -- Operation and maintenance -- Diagnosing errors
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
Why can you not transfer the configuration from the PC to the Windows CE-based panel?
Interruption of setup when updating ProTool (Pro/Lite) V5.2 from SP2 to SP3. Error message: "Cannot process Ptreg.dat"
Error message when connecting tags again
Memory problems with graphics
Error message when configuring a tag in a ProTool/Pro PC project with OPC connection
ProTool V3.00 Font problems / incorrect character sets
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
Part number:

Description
If you install WinCC flexible on a computer on which ProTool is already installed, under certain circumstances ProTool can no longer be started from STEP 7. You can use the following remedies for this:

Note
Pay attention to the compatibility of the products STEP 7, WinCC flexible and ProTool in Entry ID: 64847781. For example, the versions STEP 7 V5.5, WinCC flexible 2008 SP3 and ProTool V6.0 are not compatible.

WinCC flexible 2008
 
No. Action
1. Call ProTool once via the Windows Start menu after installing WinCC flexible.
2. Open the ProTool project from STEP 7.

WinCC flexible 2008 SP2

Remedy 1
 
No. Action
1. Open the STEP 7 Manager.
2. Select the menu command "Help > About...".
3. Click on the "Update menus..." button.

Remedy 2
 
No. Action
1. Uninstall ProTool as described in Entry ID:18697689.
2. Install ProTool.
3. Start ProTool and create a new project.
4. Close ProTool (no need to save the project).

Remedy 3
 
No. Action
1. Uninstall ProTool as described in Entry ID:18697689.
2. Install ProTool.
3. Start ProTool and create a new project.
4. Close ProTool (no need to save the project).
5. Open the STEP 7 Manager.
6. Select the menu command "Help > About...".
7. Click on the "Update menus..." button.

 
Workaround
Open the ProTool project by double-clicking on the ProTool operator panel in NetPro.

 Entry ID:22057057   Date:2013-05-03