show the entry list
ProSave -- ProSave in general -- Working with ProSave
What should you watch out with regard to licenses for WinCC flexible and panels?
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
Which version of Image of the relevant operator panels can be used for the corresponding version of ProTool?
Error message when transferring the Pocket Internet Explorer to a Windows CE Panel with ProSave
How do you backup/restore with a Windows-based panel?
What connections are there between the version designations in WinCC flexible?
How to Backup and restore a program on a text or graphic-based panel?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you do an operating system update (OS update) on operator panels?
Specification of the installation path for shared files in the standalone installation of ProSave V6.0 SP2
Micro Panels -- Setting up systems -- Installing and upgrading OS operating systems/software
Where can you procure HSPs (Hardware Support Packages) for WinCC flexible?
How do you do an operating system update (OS update) on operator panels?
Touch Panel / Operator Panel -- Setting up systems -- Installing and upgrading OS operating systems/software
How do you do an operating system update (OS update) on operator panels?
Where can you procure HSPs (Hardware Support Packages) for WinCC flexible?
Update of ProTool/Pro Runtime on the OP 37 Pro
Mobile Panels -- Setting up the system -- Installing and upgrading OS operating systems/software
What might be the cause for an operator panel of the MP 277 or Mobile Panel 277 series no longer running/starting after a restore procedure via memory card (MMC/SD)?
Where can you procure HSPs (Hardware Support Packages) for WinCC flexible?
How do you do an operating system update (OS update) on operator panels?
WinCC flexible ES -- Setting up development environments -- Installing and upgrading software
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
What do you have to do if you can no longer access symbols and data blocks of STEP 7 from an integrated WinCC flexible project?
Which security measures help against unauthorized access to computer systems with WinCC flexible?
Compatibility Tool for Automation and Drive Technology
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
Why can you not select the installed languages in the Runtime Loader of PC Runtime?
When you install or uninstall WinCC flexible, why are some fonts no longer available for STEP 7 Basic V10.5?
How do you do an operating system update (OS update) on operator panels?
Why can't you install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 after installing WinCC flexible 2008?
What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?
What are the solutions offered for working with different versions of WinCC flexible?
What can cause the installation to abort or prevent successful starting of WinCC flexible?
Where can you procure HSPs (Hardware Support Packages) for WinCC flexible?
What might be the cause for not all the user interface languages being available for selection?
What might be the causes of unsuccessful MSDE installation (Microsoft Desktop Engine)?
What are the possible causes of the Setup program not starting for the installation of WinCC flexible?
How can you clear the cause of the message "Please reboot before installing any more programs"?
How do you uninstall WinCC flexible 2004?
How do you install ProAgent in SIMATIC WinCC flexible?
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?
How can you install WinCC flexible from the hard disk?
Multi Panel -- Setting up systems -- Installing and upgrading OS operating systems/software
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
How do you do an operating system update (OS update) on operator panels?
What settings do you have to make on an MP 377 to reset the operator panel to the factory settings?
What is the installation procedure for SIMATIC WinAC MP 2008?
What might be the cause for an operator panel of the MP 277 or Mobile Panel 277 series no longer running/starting after a restore procedure via memory card (MMC/SD)?
Where can you procure HSPs (Hardware Support Packages) for WinCC flexible?
ProTool -- Setting up development environments -- Installing and upgrading software
How do you do an operating system update (OS update) on operator panels?
Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?
Interruption of setup when updating ProTool (Pro/Lite) V5.2 from SP2 to SP3. Error message: "Cannot process Ptreg.dat"
Only one language version ProTool /Lite /Pro can be installed at any one time
Installing ProTool without ProAgent
Function keys are lost in the configuration
ProTool: Switching from integrated to standalone/not integrated
Various versions of ProTool/Pro/Lite on one operating system
Installation of ProTool V6.0 or  ProTool V6.0 Service Packs aborted with error message "-132" 
Installation of ProTool V6.0 SP1 in MS Windows 2000 SP3
What should you watch out for to ensure successful installation of ProTool Lite, ProTool and ProTool/Pro?
Complete uninstallation of ProTool/Lite, ProTool and ProTool/Pro
Advantages of Configuring with ProTool integrated in STEP 7
Upgrade installation from ProTool/Pro V6.0 SP3 to MS Windows XP Professional
How do you do an operating system update (OS update) on operator panels?
Part number:

Description
Below we provide you with an overview of when you must update an operating system and how to do the update depending on the software used.

  1. "Operating system update" or "Reset to factory settings" with
    WinCC (TIA Portal)

The PDF document includes instructions for how to do an "Operating system update" or "Reset to factory settings" (booting) using the WinCC (TIA Portal) software.

Note
As from WinCC V11 you no longer need an operating system update in the different versions (for example, WinCC V11 SP1, WinCC V11 SP2, etc.). When you transfer a project, all the currently associated system files (DLLs) are also transferred automatically to the operator panel. The Basic Panels are the exception here.

Attachment 1: WinCC_TIA_Portal.pdf ( 433 KB )

Contents
1 Operating System Update with WinCC (TIA Portal)
     1.1 Operating System Update (OS Update)
     1.2 Reset Operator Panel to Factory Settings (Booting)
          1.2.1 Operator Panel with Defective Operating System
          1.2.2 Operator Panel with Intact Operating System
2 Additional Information
     2.1 Cable Connection between PC and Operator Panel
          2.1.1 Operating System Update
          2.1.2 Reset Operator Panel to Factory Settings (Booting)
     2.2 Set Image Path / File in ProSave
          2.2.1 Image Path in WinCC (TIA Portal)
          2.2.2 Image Path in WinCC flexible 2008
     2.3 Determine MAC Address
3 Problem Analysis
     3.1 Disconnection of RS232/PPI Multi Master Cable
     3.2 Check Box Cannot be Selected in ProSave
     3.3 Check Box Cannot be Deselected in ProSave
     3.4 Error Message when Transferring the Configuration
     3.5 Comfort Panel "Reset to factory settings" (Booting)
     3.6 MP 377 "Reset to factory settings" (Booting)
     3.7 Connection to Operator Panel Cannot be Established
          3.7.1 Check Transfer Type and Address on the Operator Panel
          3.7.2 Check Cable Connection and Connectors
          3.7.3 Check PG/PC Interface on the Configuration Computer.

  1. "Operating system update" or "Reset to factory settings" with WinCC flexible

The PDF document includes instructions for how to do an "Operating system update" or "Reset to factory settings" (booting) using the WinCC flexible software.

Attachment 2: WinCC_flexible.pdf ( 783 KB )    

  1. "Operating system update" or "Reset to factory settings" with ProTool

The PDF document includes instructions for how to do an "Operating system update" or "Reset to factory settings" (booting) using the ProTool software.

Attachment 3: ProTool.pdf ( 566 KB )    

  1. "Operating system update" or "Reset to factory settings" with ProSave (standalone)

The PDF document includes instructions for how to do an "Operating system update" or "Reset to factory settings" (booting) using the ProSave software.

Attachment 4: ProSave.pdf ( 786 KB )    

System messages
The table below shows some of the possible system messages that can be displayed when the configuration is to be transferred to the operator panel and the version of the operator panel's operating system does not match the Engineering Software installed.
 
System messages
No image found. Waiting for image update…,
Incorrect operating system version on the operator panel. Update the operating system? (0800:000011)
Downloading is not possible. The "version of the device" in your WinCC flexible project and the version of the device's operating system are not compatible. Do you want to update the operating system of the HMI device?
Transfer is not possible. The "version of the operator panel" in your WinCC flexible project and the version of the operator panel's operating system are not compatible. Update the operating system of the operator panel via "Project > Transfer > Update operating system" (if necessary, "Reset to factory settings").
Table 01

The following Entry IDs contain additional information on this topic:
 
Topic Entry ID
What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? 35677293
Relations between WinCC flexible and the version designations 21742389
Relations between the image version of the operator panel concerned and the version of ProTool used 28263711
Serial cable assignment for transferring the configuration to a Windows-based device 21401061
Bus terminating elements for PROFIBUS subnetworks 187276
Table 02

Additional Keywords
Update OS, Operating system, Boot, Boot Loader, Transfer settings, RS232/PPI multimaster cable, Freeport, PPI, USB, Boot settings, Reboot, Basic, Comfort, Advanced, Professional, Panel Factory Settings, Panel Overall Reset, Panel Reset
 

 Entry ID:19701610   Date:2012-11-13