show the entry list
WinCC -- Operation and maintenance -- Diagnosing errors (evaluating diagnostics files)
How do you use the "SIMATIC Diagnostics Tool" (SDT) to collect diagnostics and system data?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
What do the error messages "Transfer buffer too small", "TagQueue overflow" and "Messages are lost" mean?
Why does the error "S7OPCIAX" occur in the event display?
How can you recognize resource bottlenecks in advance from WinCC and react to them accordingly?
Where can you find a description of the error messages of the Global Script diagnostics window in WinCC RT?
How can I determine the name of an action via the error message "Execute Error in Action @xxx"?
What can be the cause of the WinCC error message "More than 10000 actions in work" (up to V6.2: "More than 5000 actions in work")?
How can you back up the data of the Windows event viewer?
How do you save the diagnostics data of the Windows system monitor (performance monitor) in a file?
How can you define the amount of memory required for the performance indicator log of the Windows system monitor (performance monitor)?
Where can I find explanations of the error messages of the WinCC diagnostics files License.log, WinCC_SStart_xx.log and WinCC_Sys_xx.log ?
How do you evaluate and remedy "OnErrorExecute"-type configuration errors?
How do you write outputs from the "APDiag" diagnostic tool to a file?
How do you use the diagnostic tool "APDiag" to debug C scripts?
How do you determine the function name from the function ID in the case of APDiag-OnErrorExecute messages?
How do you start the "APDiag" script diagnostics tool?
OS - WinCC -- Operation and maintenance -- Diagnosing errors
Why do you get the license error message "YMAINR9999 missing" although you are using only the license-free basic diagnostics?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
How can you back up the data of the Windows event viewer?
How do you create a memory dump for diagnostics purposes in WinCC and PCS 7?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Why are the DCOM settings of the WinCC OPC server reset after activating the OS Runtime?
Why is the message "Network not ready yet." displayed when an AutoStart is configured on the OS?
Why are the STEP 7 ActiveX controls (OCX) not shown on the OS server and OS client?
Why aren't all the block icons updated during OS compilation?
What are the causes of PCS 7 control technology and system messages and what measures are to be taken to clear them?
Why does the OS Login Box disappear sometimes in the background?
Length of mapped message texts
What should I do if the Split Screen Wizard closes with an error message?
Why do I get an error message when calling the loop display of a faceplate?
What is the meaning of the WinCC messages "PLC fault synchronous" and "PLC fault asynchronous"?
Why does it take 3 to 5 minutes for the Login Box to open on the client or until the message "No authorization for operation" is displayed?
What might be the cause that the hierarchy display in the overview area of the SIMATIC PCS 7 OS does not work?
Error Message "Group display: Tag .Eventstate does not exist"
Why does "?????" appear as a text on the range selector buttons in the overview area in OS runtime even though the text is available in the SIMATIC Manager?
Why does the error message 10111001 "The group display hierarchy has not been updated" appear?
How can you back up the data of the Windows event viewer?
Part number:

Instructions:
Information, warnings and errors relating to hardware or the operating system are stored in the Microsoft Windows event viewer. For diagnosing it might be necessary to make the data of the event viewer available for the Siemens Technical Support.

Procedure in Windows NT 4.0
 
No. Procedure
1 Call the event viewer with "Start > Programs > Administration (General) > Event Viewer".
2 Using the menu item "Protocol > System" or "Protocol > Application" you can switch to the protocol concerned.
3 Save the data from both protocols in each case with "Protocol > Save as..." and select the file type *.EVT.
4 If possible, archive the stored protocols before sending them to Technical Support, for example in a .zip archive. This greatly reduces the volume of data to be transferred.
Table 01

Procedure in Windows 2000/2003 Server/XP
 
No. Procedure
1 Call the event viewer from the Control Panel with "Administrative Tools > Event viewer".
2 You can switch between log files for System and Applications in the tree structure in the window on the left.
3 Save the application log file and the system log file selecting *.EVT as file type.
4 If possible, archive the stored log files before sending them to Technical Support, for example in a .zip archive. This greatly reduces the volume of data to be transferred.
Table 02

Procedure in Windows Vista/Windows 7/2008 Server
 
No. Procedure
1 Call the event viewer.
Start > Control Panel > System and Security > Administrative Tools> Event Viewer    VIEW: Category or
Start > Control Panel > All System Control Elements > Administrative Tools> Event Viewer    VIEW: Large/small symbols
2 In the tree structure you switch to "Windows Logs" in the window pane on the left. Double-click to open this.
3 Select the subitem "Application" in the window pane on the left. Right-click to open the pop-up menu and select the "Save all events as..." function. Save the complete application protocol as an *.EVTX file.
Select the subitem "System" in the window pane on the left. Right-click to open the pop-up menu and select the "Save all events as..." function. Save the complete system protocol as an *.EVTX file.
4 If possible, archive the stored log files before sending them to Technical Support, for example in a .zip archive. This greatly reduces the volume of data to be transferred.
Table 03

Collecting diagnostics files centrally
How to gather together the diagnostics and system information of your computers on one central computer is described in Entry ID 65976201.

 Entry ID:15386411   Date:2013-11-12