show the entry list
ES - SIMATIC Manager -- Product information – System description
Which components and controllers can be used to set up a PROFINET field bus in PCS 7?
What should you watch out for when replacing a defective CPU in a PCS 7 plant configuration to ensure that no process object licenses are booked in duplicate?
What are the options for implementing the security products SCALANCE S, CP443-1 Advanced and CP1628 in the PCS 7 environment?
How do you procure documentation for PCS 7 V8.0 (including the PCS 7 V8.0 Manual Collection)?
How are the licenses for the AS and OS counted in PCS 7 V7.0 onwards?
What actions lead to loss of "AS RT PO" licenses with PCS 7?
What are the requirements for using the CPU_RT block with PCS 7 V7.0?
Important notes on the documentation for PCS 7 V7.0 SP1
Acknowledgement-triggered reporting of SIMATIC PCS 7 V6
Compilation of frequently asked questions about PCS 7 V6.0
How do you install an OPC application for operation in the "SIMATIC HMI" user group?
MS Windows 2000 settings for OS client / supplement to the SIMATIC PCS 7 V6.x Readme file
Correction of the english SIMATIC PCS 7 V6.0 Readme
How do you count the number of process objects (PO) for the PCS 7 licenses?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Full-text search in the electronic manuals SIMATIC PCS 7 V6.0
What are the options for redundancy and high availability in PCS 7 V6.1 SP1?
What actions lead to loss of "AS RT PO" licenses with PCS 7?
Part number:

Description:
The following actions lead to loss of AS RT PO licenses if they have not been booked back previously.
 
No. Action Remedy
1 Deleting the PCS 7 project or S7 program Book the process objects back before deleting.
2 Moving the S7 program to another AS Book the process objects back before moving.
3 Loading an S7 program into multiple ASs Create a separate S7 program for each automation system.
4 Using a project backup in which not all the POs have been configured Book the process objects back before backing up.
5 Replacing the CPU including the RAM card
If you replace just the CPU or just the RAM card, the AS is recognized as previous target system and the POs are not booked again.
Book the process objects back before replacing the components.
6 Loading the AS from different ESs with multiproject engineering.
If the project is distributed to multiple ESs from the central ES, when loading the AS, the POs are booked by the loading ES even if they have already been booked by another ES.
Transfer the existing licenses to the central ES only and select the central ES in the "Automation License Manager" search list of the other ES.

Open the relevant single project of the remote ES from the central ES.

Notes:

  • To find out how many process objects are configured and booked, open the pop-up menu of the multiproject or project and select the item "PCS 7 License information...".
  • A detailed description of licensing process objects is available in the manual "SIMATIC Process Control System PCS 7 CFC for SIMATIC S7" in Entry ID: 27002752.

Creation environment:
This entry has been created with PCS 7 V7.1.

Keywords: 
License loss

 Entry ID:38849821   Date:2009-10-20