show the entry list
ES - SIMATIC Manager -- Product information – System description
Which components and controllers can be used to set up a PROFINET field bus in PCS 7?
What should you watch out for when replacing a defective CPU in a PCS 7 plant configuration to ensure that no process object licenses are booked in duplicate?
What are the options for implementing the security products SCALANCE S, CP443-1 Advanced and CP1628 in the PCS 7 environment?
How do you procure documentation for PCS 7 V8.0 (including the PCS 7 V8.0 Manual Collection)?
How are the licenses for the AS and OS counted in PCS 7 V7.0 onwards?
What actions lead to loss of "AS RT PO" licenses with PCS 7?
What are the requirements for using the CPU_RT block with PCS 7 V7.0?
Important notes on the documentation for PCS 7 V7.0 SP1
Acknowledgement-triggered reporting of SIMATIC PCS 7 V6
Compilation of frequently asked questions about PCS 7 V6.0
How do you install an OPC application for operation in the "SIMATIC HMI" user group?
MS Windows 2000 settings for OS client / supplement to the SIMATIC PCS 7 V6.x Readme file
Correction of the english SIMATIC PCS 7 V6.0 Readme
How do you count the number of process objects (PO) for the PCS 7 licenses?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Full-text search in the electronic manuals SIMATIC PCS 7 V6.0
What are the options for redundancy and high availability in PCS 7 V6.1 SP1?
Important notes on the documentation for PCS 7 V7.0 SP1
Part number:

Description:
An error has been discovered in the PCS 7 documentation.
In the manual "Product Brief on Software Updates from V5.1/V5.2 to PCS 7 V7.0 SP1", chapter 6 "Guide - Basic Procedure for Updating Software", step 23 states that the Project Migrator is only to be run in the case of a software update with new functions. This step must also be carried out in software updates without new functions.


Fig. 01

 Entry ID:32049393   Date:2008-10-29