With the correct wiring, how can you avoid exceeding the common-mode voltage (Ucm) and subsequent measured value overflow or underflow in the analog input module 6ES7 331-1KF0.-0AB0?
-
Entry
-
Associated product(s)
When operating the module, a maximum voltage of 2V is specified for the difference of potential Ucm (common-mode voltage) between the "M-" input terminals.
This data is available in the manual S7-300 Module Data, chapter 6.
Link to manual: Entry ID 8859629
The common-mode voltage can be slightly exceeded with open inputs and when potential-free measuring transducers are connected. Therefore you must take the following measures for isolated 4-wire measuring transducers and potential-free voltage sensors:
- Connect M- of the inputs to each other and to the module ground.
- Disable unused channels and likewise connect M- to the module ground.
- In the case of disabled channels on the front connector, if long, open cables are connected, we recommend a jumper between M+ / S- and M-. This avoids sources of interference from these open cables.
Measurements for determining the error voltage between the "M-" terminals for determining the Ucm are not practical, because even high-ohm measuring devices cause equipotential bonding.
Fig. 01
Fig. 02
- German
- French
- Italian
- Spanish
- Chinese (simplified)
- You want to discuss in our forum and exchange experiences with other users
- You have a technical question / problem: Ask the Technical Support
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry