show the entry list
NCM S7 for Ind. Ethernet V 4 with CP 443-1 (6GK7 443-1EX02-0XE0)
Part number:

DESCRIPTION:
This Service Pack is required for the diagnostics of the new module CP443-1 with NCM S7 IE V 4.

Major extensions:
The CP 443-1 is supplied in a new version. This new version can be recognized by the change in the MLFB. It is thus not possible for NCM S7 V4.02 to perform diagnostics. This Service Pack enters the new MLFB in the NCM. It is thus possible to do diagnosis of these modules.
You can configure the new modules with the previous MLFB. When loading the parameters, a difference is made between online and offline configurations. This can be ignored and the parameters will still be loaded. It is however not possible to use the new properties of the modules with NCM V 4.02.
If you use STEP7 V 5 with Service Pack 2 and the relevant NCM with Service Pack 2, then the configuring and diagnostics functionalities are supported completely.

Installation:
Unpack the Service Pack servpack.exe and the diag_ie.reg file is read into the computer. Double-click it to execute it. The relevant entries are then made accordingly.
Read the instructions in the Readme.txt file.

Service Pack
 servpack.exe (17 KB)

 Entry ID:927431   Date:1999-07-22 
I regard this article....as helpfulas not helpful                                 
related links
Service Pack for NCM
Service Pack for NCM S7 for PROFI ...
Conversion firmware for CP 443-1 ...
Service Pack for NCM V4.02 Ind. E ...
CP 443-1: clearing errors with th ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour