|
QUESTION:
Are the drivers on the SIMATIC NET CD 07/2001 released for
WinCC V5.0 + SPx?
ANSWER:
No, you can only use these drivers for WinCC V5.1 and
higher.
If you are using older modules such as CP1413 or CP5412, then
you must continue using the drivers on SIMATIC NET CD 05/2000.
In this case the SIMATIC NET CD 07/2001 must not be
installed on the OS.
Keywords:
Compatibility; Device driver; Driver CD
|