|
This FAQ applies only to the SINAMICS G120/G120D Control Units without “-2” in the product name and MICROMASTER 4 inverters.
The following example explains how to switch between fixed frequency operation and analogue setpoint:
Set the fixed frequency as the main setpoint and the analogue as the additional setpoint (P1000 = 23).
Normally the main setpoint and the additional setpoint sum together in the setpoint channel. To switch between both frequencies you have to enable or disable the particular frequency. Parameterize a digital input (e.g. DIN 3) to disable the additional setpoint (P1074) and sets the fixed frequency (P1022).
relevant parameter
| Function |
Parameter |
Description |
Setting |
Description |
| User access level |
P0003 |
Defines user access level to parameter sets |
3 |
Allows extended access |
| Selection of frequency setpoint |
P1000 |
Selects frequency setpoint source (main setpoint + additional setpoint) |
23 |
Fixed frequency + Analog setpoint |
| Fixed frequency 3 |
P1003 |
Defines fixed frequency |
e.g. 10Hz |
|
| Function of digital input 3 |
P0703 |
Selects function of digital input 3 |
99 |
Enable BICO parameterization |
| Fixed freq. selection Bit 2 |
P1022 |
Defines origin of fixed frequency selection |
722.2 |
DIN 3 |
| Disable additional setpoint |
P1074 |
Disables additional setpoint |
722.2 |
DIN 3 |
Result:
- DIN 1 = ON / OFF 1
- DIN 2 = reverse
- DIN 3 = enable fixed frequency / disable additional setpoint
|