show the entry list
Industrial Ethernet PC CPs -- Product information -- System description
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
How can you display the security status of the CP1628 over the Online View in the Security Configuration Tool (SCT)?
What are the requirements for changing from CP1613 A2 to CP1623?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
In which order should you install the software of the Development Kit DK16xx PN IO in order to load the configuration or firmware of the CP1616 via NCM PC?
What are the requirements for using the S7 routing function and which modules can you implement?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What is the difference between SoftNet and HardNet communication processors?
PROFIBUS PC CPs -- Product information -- System description
What are the requirements for using the S7 routing function and which modules can you implement?
Notes on using the DPC2 starting with SIMATIC NET CD 07/2001
How do you create a GSD file for the CP 5614 in COM PROFIBUS V3.3 in order to link it as a DP slave to a DP master system?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What is the difference between SoftNet and HardNet communication processors?
PROFIBUS PC software -- Product information -- System description
Support of SNMP variables by SIMATIC NET
Red cross in the OPC Scout Navigator
What should you watch out for in particular when implementing the Runtime Callable Wrapper (RCW) with the SIMATIC NET CD Edition 2006?
What are the special features of the changed startup behavior of the OPC data access server with SIMATIC NET CD Edition 2006?
Optimum OPC operating mode of an application
What is the connection between version designations of the SIMATIC NET PC software?
What should you watch out for if you change symbols in the STEP 7 project when using the OPC server of the SIMATIC NET PC software?
Notes on using the DPC2 starting with SIMATIC NET CD 07/2001
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
Industrial Ethernet PC software -- Product information -- System description
How do you terminate the SINEMA Server application so that the license is no longer occupied and can be moved?
Support of SNMP variables by SIMATIC NET
Red cross in the OPC Scout Navigator
What should you watch out for in particular when implementing the Runtime Callable Wrapper (RCW) with the SIMATIC NET CD Edition 2006?
General information on the OPC server
Optimum OPC operating mode of an application
Which functions does SINEMA E provide and how do you operate SINEMA E to use them?
What is the connection between version designations of the SIMATIC NET PC software?
What should you watch out for if you change symbols in the STEP 7 project when using the OPC server of the SIMATIC NET PC software?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What are the special features of the changed startup behavior of the OPC data access server with SIMATIC NET CD Edition 2006?
How do I find examples, explanations and further information about SNMP and the SIMATIC NET SNMP OPC server?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
Part number:

Configuration Notes:
The SIMATIC NET OPC server is included in the SIMATIC NET PC software. With the SIMATIC NET OPC server, you can connect a PC station to S7 stations, S5 stations or third-party devices for data exchange via PROFIBUS or Industrial Ethernet.

The following communication services are available for communication via Industrial Ethernet:

  • S5-compatible communication and S7 communication
    S5-compatible communication be used for data exchange with S7 stations, S5 stations and third-party devices. S7 communication can only be used for data exchange with S7 stations.
    You need one of the following SIMATIC NET PC software packages to be able to use these communication services including SIMATIC NET OPC server:
    • SOFTNET S7 Lean - for up to 8 connections via normal Ethernet network cards, CP1612 or CP1512.
    • SOFTNET S7 IE - for up to 64 connections via normal Ethernet network cards, CP1612 or CP1512.
    • S7-1613 - for up to 120 connections via CP1613 (A2) or CP1623.
       
  • PROFINET IO controller
    You need the following SIMATIC NET PC software to operate a PC station as PROFINET IO controller:
    • SOFTNET PN IO - for up to communication via normal Ethernet network cards, CP1612 or CP1512.
  • Fault-tolerant S7 communication
    You need the following SIMATIC NET PC software if you wish to configure fault-tolerant S7 connections for communication between S7-400H system and PC station:
    • S7-REDCONNECT - for communication via CP1613 (A2) or CP1623.  

The following communication services are available for communication via PROFIBUS:

  • S7 communication
    S7 communication can only be used for data exchange with S7 stations. You need one of the following SIMATIC NET PC software packages if you want to use S7 communication including SIMATIC NET OPC server for data exchange:
    • SOFTNET S7 PB - for communication via CP5611 (A2), CP5621 or CP551x.  
    • S7-5613 - for communication via CP5613/14 (A2).
       
  • FDL protocol
    The FDL protocol can be used for data exchange with S7 stations and S5 stations. You need one of the following SIMATIC NET PC software packages if you want to use the FDL protocol including SIMATIC NET OPC server for data exchange:
    • SOFTNET DP - for communication via CP5611 (A2), CP5621 or CP551x.  
    • CP5613/5614 (A2) - here you do not need any other software, because the protocol driver is supplied with the hardware.
       
  • FMS protocol
    The FMS protocol can be used for data exchange with S7 stations and S5 stations. You need the following SIMATIC NET PC software package if you want to use the FMS protocol including SIMATIC NET OPC server for data exchange:
    • FMS-5613 - for communication via CP5613/14 (A2).
       
  • PROFIBUS DP slave
    You need the one of the following SIMATIC NET PC software packages to operate a PC station as PROFIBUS DP slave:
    • SOFTNET DP slave - for communication via CP5611 (A2), CP5621 or CP551x.  
    • CP5614 (A2) - here you do not need any other software, because the protocol driver is supplied with the hardware.
      More information is available in the manual of the DP Base programming interface in Entry ID 1653531.
      Note:
      On the S5 side, an IM308C or a CP5431 is used as DP master.
  • PROFIBUS DP master
    You need the one of the following SIMATIC NET PC software packages to operate a PC station as PROFIBUS DP master:
    • SOFTNET DP - for communication via CP5611 (A2), CP5621 or CP551x.  
    • CP5613/14 (A2) - here you do not need any other software, because the protocol driver is supplied with the hardware.
      More information is available in the manual of the DP Base programming interface in Entry IDs 1653531 and 25011749.
      Note:
      On the S5 side, an IM308C is used as DP slave.

Keywords:
OPC server, S5 link, S5 connection, S7 connection, Send, Receive, DP Base, SOFTNET

 Entry ID:8782948   Date:2008-04-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour