show the entry list
FM 352, 452 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the FM352 cam controller (6ES7352-1AH02-0AE0) in STEP 7 Professional V11 and higher?
What I need to take care if an old FM 352(6ES7352-1AH01-0AE0) will be replaced by a new FM 352(6ES7352-1AH02-0AE0)?
What should you watch out for when writing machine data to the FM352?
Which function modules (FM) can be used remotely in an ET 200M?
How can you prevent losing the absolute value encoder adjustment/cam parameters when you restart your CPU or FM?
What do you need to watch out for when loading parameters with the commissioning software for the FM352?
Changing dynamization times in operation by "fast cam" on an FM352
FM352/452: Processing of process alarms
Changing dynamization times in operation by "fast cam" on an FM352
Part number:

QUESTION:
Why, after changing one or more dynamization times of cams using the "Fast Cam" function, is there no longer correct dynamization?

ANSWER:
You have changed one or more dynamization times of cams on the FM352 using the "Fast Cam" function. Afterwards dynamization is no longer correct. Even the dynamization of cams whose dynamization times have not been changed is possibly incorrect.
The problem occurs only when you change the dynamization times of cams 16 to 127, not however with cams 0 to 15.

Problem description:

  • The dynamization time of a cam 16 to 127 is changed during operation to a smaller or the same time value.
  • The dynamization time of this cam was previously the greatest dynamization time of all the parameterized cams.
  • After change, the dynamization is incorrect.

Problem solution:

  • With cams 0 to 15 any one cam with any cam start, any cam end and any track specification is parameterized with a dynamization time.
  • The dynamization time is greater than the dynamization time entered in each case with "Change Fast Cam".
  • This auxiliary cam must also be set to "Valid". You can disable its switching function by setting "none" as effective direction.
    The disadvantage here is that the speed measuring cycle of the module is always based on the dynamization time of the auxiliary cam.
  • Even without auxiliary cams, changing the dynamization time a second time leads to subsequent correct dynamization. For this you must call the "Change Fast Cam" function twice with identical parameters.

Keywords:
FM module, Cam controller

 Entry ID:8781159   Date:2001-10-01 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour