show the entry list
Industrial Ethernet PC software -- Product information -- System description
How do you terminate the SINEMA Server application so that the license is no longer occupied and can be moved?
Support of SNMP variables by SIMATIC NET
Red cross in the OPC Scout Navigator
What should you watch out for in particular when implementing the Runtime Callable Wrapper (RCW) with the SIMATIC NET CD Edition 2006?
General information on the OPC server
Optimum OPC operating mode of an application
Which functions does SINEMA E provide and how do you operate SINEMA E to use them?
What is the connection between version designations of the SIMATIC NET PC software?
What should you watch out for if you change symbols in the STEP 7 project when using the OPC server of the SIMATIC NET PC software?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What are the special features of the changed startup behavior of the OPC data access server with SIMATIC NET CD Edition 2006?
How do I find examples, explanations and further information about SNMP and the SIMATIC NET SNMP OPC server?
PROFIBUS PC software -- Product information -- System description
Support of SNMP variables by SIMATIC NET
Red cross in the OPC Scout Navigator
What should you watch out for in particular when implementing the Runtime Callable Wrapper (RCW) with the SIMATIC NET CD Edition 2006?
What are the special features of the changed startup behavior of the OPC data access server with SIMATIC NET CD Edition 2006?
Optimum OPC operating mode of an application
What is the connection between version designations of the SIMATIC NET PC software?
What should you watch out for if you change symbols in the STEP 7 project when using the OPC server of the SIMATIC NET PC software?
Notes on using the DPC2 starting with SIMATIC NET CD 07/2001
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
Red cross in the OPC Scout Navigator
Part number:

QUESTION:
What is the meaning of the red cross in the Navigator window of the OPC Scout?

ANSWER:
The OPC client of SIMATIC Net (OPC Scout) provides the option of using the OPC Navigators to browse the address space of an OPC Server. Here, you get a display of the variables known to the OPC Server, i.e. which exist in its address space. If no variable has been defined as yet, then the corresponding icon is crossed out in red. You can define variables manually via "New Definition". These "Items" are entered in the address space of the server. When the OPC Server is connected again, these variables are then known and the red cross disappears. This is not an error but just the fact that there are not (yet) any variables known to the server.



WARNING:
The address space of an OPC Server is a hierarchical list of variable names. However, this does not mean that they can also be added (AddItems) or "productized". The syntax check of a variable is run only when the "AddItems" call is made.

Keywords:
Object display


 Entry ID:8763769   Date:2001-09-24 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour