show the entry list
Panel PC -- Setting up and parameterizing hardware -- Connecting devices
What are the order numbers of the back-up batteries for SIMATIC IPCs and SIMATIC Field PGs?
What do you need to watch out for when operating SIMATIC software on SIMATIC IPC227D and IPC277D?
Why is the UPS not recognized via USB interface when a Panel PC 477-HMI or -HMI/RTX is operating with a SITOP DC UPS module?
What options exist for ordering missing plug-in terminal strips for the power supply of panels?
Why should a SIMATIC PC not be switched on in the buffered UPS mode?
What must be considered when installing a SIMATIC Panel PC 477 (DC 24V version)?
Plug-in strips for Panel PCs
How do you connect the PS Expansion Board of the CPU 41x-2 PCI V3.4 to the internal voltage supply of the Box PC 627?
Can I use a keyboard with USB interface and internal USB hub for the SIMATIC Panel PCs 670 and 870?
Can I use a keyboard with USB interface and internal USB hub for the SIMATIC Panel PCs 670 and 870?
Part number:

Instructions:
You may use a keyboard with USB (Universal Serial Bus) interface and internal USB hub for the "SIMATIC Panel PCs" if you meet the requirements for the USB specification version V1.1.

Keywords:
USB host controller, USB classes, Parallel interface, EIDE, SCSI, Firewire


 Entry ID:8759488   Date:2007-08-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour