|
Description: For connection configuration you use the
"SR_Config.exe" tool. The download for this and a detailed
description are available on the Customer Support site in Entry ID
2997327.
Note:
This tool is no longer required from SIMATIC NET CD 7/2001
onwards.
For Fetch/Write you always need two connections:
- One connection for Fetch (Fetch passive)
- One connection for Write (Receive passive)
Open the "SR_Config.exe" tool and select an access point.

Fig. 1: Selecting the access point
Create a connection to the controller and define parameters for it.
The parameter "S5 Access" has the value "1" (read only).
Since only reading is permitted on the Fetch connection, the
"S5 Access" parameter must be set to "1".
Fig. 2: S5_Access_read_only ( 15 KB )
Create another connection to the controller and define the
parameters for it The parameter "S5 Access" has the value
"2" (write only). Since only writing is permitted on
the Write connection, the "S5 Access" parameter must be set to
"2".
Fig. 3: S5_Access_write_only ( 15 KB )
Important: Make sure that the values for the
"S5_Access" parameters are different. Parameterization is identical
for the S5 and the S7.
Keywords: S5 Access, State path
|