show the entry list
WinCC -- Operation and maintenance -- Diagnosing errors (evaluating diagnostics files)
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
What do the error messages "Transfer buffer too small", "TagQueue overflow" and "Messages are lost" mean?
Why does the error "S7OPCIAX" occur in the event display?
How can you recognize resource bottlenecks in advance from WinCC and react to them accordingly?
Where can you find a description of the error messages of the Global Script diagnostics window in WinCC RT?
How can I determine the name of an action via the error message "Execute Error in Action @xxx"?
What can be the cause of the WinCC error message "More than 10000 actions in work" (up to V6.2: "More than 5000 actions in work")?
How can you back up the data of the Windows event viewer?
How do you save the diagnostics data of the Windows system monitor (performance monitor) in a file?
How can you define the amount of memory required for the performance indicator log of the Windows system monitor (performance monitor)?
Where can I find explanations of the error messages of the WinCC diagnostics files License.log, WinCC_SStart_xx.log and WinCC_Sys_xx.log ?
How do you evaluate and remedy "OnErrorExecute"-type configuration errors?
How do you write outputs from the "APDiag" diagnostic tool to a file?
How do you use the diagnostic tool "APDiag" to debug C scripts?
How do you determine the function name from the function ID in the case of APDiag-OnErrorExecute messages?
How do you start the "APDiag" script diagnostics tool?
WinCC -- Configuring alarms and messages -- Configuring Alarm Logging
How do you calculate the memory requirement of a server or central archive server (CAS)?
How can I create a message in WinCC if, when backing up an archive, the backup path is not available, cannot be reached or the data medium is full?
How can you switch off the message 1000915 "Terminal adapter <MAC-address> disconnect"?
How can I avoid the whole screen being filled when I open a picture using the OpenPicture function via LoopInAlarm?
How can you increase the timeout for starting and terminating Alarm Logging / Tag Logging?
What do the error messages "Transfer buffer too small", "TagQueue overflow" and "Messages are lost" mean?
Which functions do the different variable types have for the individual messages?
How can you get specific messages to flash in the alarm list until the user has acknowledged them?
What format is best suited for defining the AlarmLogging-event variables?
What do you do if alarms are not displayed at Runtime?
How can you assign the functions of the toolbar buttons of WinCC Alarm Logging OCX to external buttons?
How can I delete individual messages from a group message?
When are alarms initiated by the limit monitoring in WinCC if the limit values are supplied indirectly?
What should I watch out for when assigning the names of message types, message classes and group messages?
Why isn’t there display of the "Comment" toolbar button of the Alarm Logging Control in Runtime?
How can you display process values formatted in an Alarm Logging message line?
How can I change the state texts of the message classes from +, -, * to actual text of my own?
How can you check the configuration of the Alarm Logging to see whether there is multiple use of message, status and acknowledge tags or whether the message tags are not configured?
At Runtime, how can you determine the message texts or process-associated values when a message appears in the associated, user-specific action "GMsgFunction()"?
How do you display and operate alarms in Runtime?
What is the structure of the format instruction for displaying the contents of WinCC tag values at Runtime in the user text blocks of a message?
How can you create messages whose message texts consist of a fixed part and a variable part?
What do the statuses of the status and acknowledge tags look like in the Alarm Logging?
What statuses can a message go through at Runtime?
How can I use the limit-value monitoring function of Alarm Logging to monitor the free drive space of a hard disk?
Why after WinCC Runtime starts is a message displayed with the text "..... already used"?
How can you configure user-defined message classes?
How can you change the acquisition cycle of the WinCC Alarm Logging?
How can you use the status tag of a message?
What should you watch out for in particular with the "Loop in Alarm" function?
How can you export, change and then reimport message texts?
What do the error messages "Transfer buffer too small", "TagQueue overflow" and "Messages are lost" mean?
Part number:

If you get at least one of the following messages, this indicates that messages are getting lost in WinCC. These messages are to be found, for example, as entries in the WinCC LOG files in the "Diagnostics" directory:

  • ALGRT : Transfer buffer too small
  • ALGRT : TagQueue overflow
  • ALGRT : Messages are lost

One remedy here is to enlarge the "Queue". You make this change in "Regedit".

IMPORTANT
As a general rule, no warranty can be provided for direct changes made to the Registry, because this is the sole responsibility of the user. In any event, you are advised to make a backup of the Registry before undertaking the actions described here. Furthermore, these settings are computer-specific.  This means that when you copy the project to another computer, you must make the settings again.

Use the following procedure:

  1. "Start > Run...", enter "regedit".
  2. Search for the code:
    HKEY_LOCAL_MACHINE\SOFTWARE\SIEMENS\WINCC\Alarm Logging\CONSTANTS
  3. Search for the name " InputQueue". If this entry does not exist, enter a new value (right-click -> "New > DWORD value").
  4. Enter the following value or change the existing value accordingly:
    InputQueue ="10000"


    Fig. 01

    The default value for the queue entries is 1500 in Alarm Logging. If you get the above-mentioned messages, you can increase the value, as in our example, to 10000.

This remedy only helps in the case of a temporary overload of the system, for example at system start-up. In the case of permanent system overload, the error messages are just delayed.

Note:
In the WinCC Information System, under "General Information > Performance Data > Message System", there is an indication of the "message load without loss".

 Entry ID:850372   Date:2010-10-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour