show the entry list
WinCC ProAgent -- Product information -- Information on WinCC ProAgent
Why do you get the message "WinCC ProAgent Module has stopped working" in SIMATIC WinCC/ProAgent V7.0 SP3?
With which Microsoft Windows operating systems is SIMATIC WinCC/ProAgent compatible?
What are the system requirements and order of installation for SIMATIC WinCC/ProAgent?
ProAgent editor cannot be seen in WinCC
Assignment of a block pair (FB/DB) to an S7-GRAPH step sequence
Displaying comparators in the ProAgent standard image
Installation of WinCC, AS OS Eng. Tool and ProAgent
Generating error - Error Create Variables for Connections
Standstill of the progress display when generating
Using function key F10 with an FI45
Installation ProAgent V4.02 for WinCC parallel to STEP7 V5.0
Using function key F10 with an FI45
Part number:

QUESTION:
How can I use the function key F10 with an FI45 with ProAgent?

ANSWER:
If you use this key with an FI45 project with WinCC ProAgent, then you must install the file available here for downloading. This file contains the parameterization required.

Procedure:
Copy the WCC_FI45.EXE file into a separate directory and then start it with a double-click. Copy the extracted PAWinCC_.key file into the "...\Keyboard" directory of the FI45. Using the tool KEYLIGHT (in the \Keyboard catalog) you can activated the new Key file. For more details see the FI45 instruction manual.

Wcc_fi45.exe (18 KB)

 Entry ID:814230   Date:1999-04-26