QUESTION:
What information is there available on the OPC server of WinAC?
ANSWER:
General information on OPC, creating items, synchronous and
asynchronous reading, writing and monitoring of items is available
on the Customer Support pages in Entry ID 6077526 or in the
Internet under http://www.opcfoundation.org.
- Information on monitoring items with the WinAC OPC
server
Monitoring items is restricted to the logging on of items and
enabling the group concerned. The OPC server then checks the items
and if there is a change of value, then an event is triggered to
the application. The OPC server works with an internal cycle time
that you can set yourself. In the case of the WinAC OPC server the
smallest value is 100ms. In this cycle the OPC server checks the
items and where appropriate triggers an event to the application.
This procedure is only useful if the items can be read from the OPC
cache and their contents make no noise. Since with the OPC server
of WinAC the items are always read from the device and never from
the OPC cache, this option is not recommended. Likewise, you
should not forget that there is always noise with process control
(e.g. at the analog outputs). For this reason the number of events
cannot be predicted.
Note:
The WinAC OPC server sporadically generates two events for a
change in value. The first event provides the preliminary contents
and the second event the proper contents. This property interferes
when using soft direct keys if feedback is needed in the
application. Applying the button triggers synchronous writing and
the contents are fed back by Monitoring of items.
- Synchronous reading / writing
Calling this method keeps the application waiting until the
communication is completed. You should only use this method for
critical signals such as soft direct keys for the non-maintained
command mode.
- Asynchronous reading / writing
This method is the best for communications. The data transfer
is triggered and the applications runs again. There is feedback per
vent about the successful transfer. You should use this method for
large volumes of data and simultaneous low loading of the operating
system.
- Increasing performance
Set operations are one of the most effective means of design
high-performance applications.
Tasks such as creating items in a group or reading and writing
items can be executed by calling a method. For this you must know
as programmer that this results in a change of cycle to the OPC
server and the lower-level driver interfaces. Summing up, a large
number of cycle changes can cause an extreme deterioration in
performance. The OPC interface also offers set operations for this.
In other words, creating 1000 items can be done in a loop for each
individual item or in one set operation. The latter gives maximum
performance.
Example:
In VB, 1000 items are created in a group. This can look like
this:
FOR i=1 TO 1000
Item="MB" & i ‚ a variable is added to the Item
string -> MB1 to MB1000
MyGroup.OPCItems.AddItem (Item, ... )
NEXT
Each AddItem call creates a change of cycle. The following formula
is significantly faster:
FOR i=1 TO 1000
Items(i)="MB" & i
NEXT
MyGroup.OPCItems.AddItems (1000, Items, ... )
The items are configured in an array and stored in a group with a
method call to the OPC server.
You can increase performance not only by using set operations, but
also through the definition of items used.
Example:
In VB, a data buffer of 1000 bytes is requested. The buffer is
organized in a coherent area in the CPU.
FOR i=1 TO 1000
Items(i)="MB" & i
NEXT
MyGroup.OPCItems.AddItems (1000, Items, gServerHandles, ... )
MyGroup.AsyncRead (1000, gServerHandles, ... )
Creating of items and reading of items are done by set operation.
Asynchronous reading is used and the data is supplied per event.
The program can continue to work.
Items(1)="MB0:INT[1000]"
MyGroup.OPCItems.AddItems (1, Items, gServerHandles, ... )
MyGroup.AsyncRead (1, gServerHandles, ... )
Another optimization is to define single item as an array. This
optimization step is for when transferring a coherent data area
from the controller.
Keywords:
OPC specification, OPC foundation, OPC communications,
Client-server
|