|
Description
The Split Screen Wizard closes with the following error message:
Possible causes Probably, when copying the project, you have set the write protection for SSM-relevant (Split Screen Manager) files. Check whether the files in the following directories have the write protection activated:
- SSM
- Wscript
- GraCS
- Library
You can deactivate the write protection using the DOS command "attrib–r/s" or via the file properties in the Windows Explorer.
Note
The write protection is usually set when you copy the project from a CD to the hard disk.
|