QUESTION:
Can I slot an FM350 counter module in Rack 1 if am using an
interface module IM365 for the extension?
ANSWER:
In the case of a connection via the interface module IM365 it
is not possible to have communication via the K bus. But since the
FM350 does not need communication via the K bus, it can be slotted
in Rack 1.
Important:
The power consumption for the complete extended Rack 1 must not
exceed 0.8 A, because the power supply is from Rack 0.
Keywords:
Interface, Hardware configuration
|