|
Data record routing is a function within SIMATIC S7 modules. SIMATIC PDM uses this function to access parameters and functions of field devices with PROFIBUS DP, PROFIBUS PA and HART communication. SIMATIC PDM is a component of the Engineering Station (ES) and communicates with the automation system (AS) over Ethernet. The automation system forwards the request to the field device means of PROFIBUS DP. This procedure of data transfer between Ethernet and PROFIBUS DP is called data record routing.
Requirements for data record routing The automation system must have the interfaces below for data record routing:
- Ethernet interface, for example the interface of the CPU or communications processor CP 443-1.
- Ethernet interface, for example the interface of the CPU or communications processor CP 443-5.
This FAQ response gives you an overview of this ES/AS components supported by PCS 7 for data record routing.
Note
A list of modules released for a specific version of PCS 7 is available on the PCS 7 CD / DVD, the "Manuals" folder, and in Entry ID 39709060 entitled " Which modules and their firmware versions are released for PCS 7 and how can you upgrade them?".
- Interfaces of the Engineering Station (ES)
- AS components in PCS 7 V8.x
- AS components in PCS 7 V7.x
- AS components in PCS 7 V6.x
- AS components in PCS 7 V5.x
- Data record routing with IE/PB Link
- FAQs, descriptions of application, and manuals
1. Interfaces of the Engineering Station (ES)
Data record routing is possible with the ES components below.
| Hardware |
Remark |
| CP 1613 |
6GK1161-3AA00 |
PCI |
| CP 1613 A2 |
6GK1161-3AA01 |
PCI |
| CP 1623 |
6GK1162-3AA00 |
PCI Express |
| Desktop adapter network card (IE General) |
A5E00718412 |
PCI |
| A5E01579552 |
PCI Express |
Table 01
Restriction
- CP 1613 is supported as from PCS 7 V5.0 SP1.
2. AS components in PCS 7 V8.x
PCS 7 V8.x supports the interfaces below for data record routing:
- Communications processors
- Interfaces of the CPU
Communications processors
| Communications processors supported |
| CP 443-5 Extended |
6GK7 443-5DX02-0XE0 as from firmware V3.2
6GK7 443-5DX03-0XE0
6GK7 443-5DX04-0XE0
6GK7 443-5DX05-0XE0 |
The firmware update of CP 443-5 Ext. with order number 6GK7 443-5DX02-0XE0 to V3.3 is available in Entry ID: 12011123. Configure the module in the HW Config still as V3.2. |
| CP 443-1 |
6GK7 443-1EX02-0XE0
6GK7 443-1EX10-0XE0
6GK7 443-1EX11-0XE0
6GK7 443-1EX20-0XE0
6GK7 443-1EX30-0XE0 |
|
Table 02
Interfaces of the CPU CPUs as from firmware V5.1 support the interfaces of the CPU for data record routing. The following versions are possible:
- Standard CPU with PROFIBUS DP interface
- Standard CPU with PROFIBUS DP interface and Ethernet interface
The matrix below shows the versions of PCS 7 with which you can use the interfaces of the CPU for data record routing.
| PDM data record routing over the interfaces of the CPU |
Standard CPU as from V5.1 |
Standard CPU PN as from V5.1 |
| PCS 7 V8.0 |
Yes |
Yes |
Table 03
Note
If the interface of the CPU is used for data record routing, that CPU must be configured in the HW Config with at least firmware V5.1 or higher.
You can use the AS components below for data record routing.
| Hardware supported |
| Y link and IM 153 Redundancy Bundle |
No restrictions |
| DP/PA link / IM 157 |
No restrictions |
| DP/PA coupler |
Ex: 6ES7 157-0AD00-0XA0 and successor products |
| Not Ex: 6ES7 157-0AC80-0XA0 as from release 3 and successor products |
| ET 200M |
6ES7 153-2AA01-0XB0 and successor products |
| ET 200iS |
No restrictions |
| ET 200iSP |
No restrictions |
Table 04
Note
Note the released modules of your version of PCS 7 in Entry ID: 57385626.
3. AS components in PCS 7 V7.x
PCS 7 V7.x supports the interfaces below for data record routing:
- Communications processors
- Interfaces of the CPU
Communications processors
| Communications processors supported |
| CP 443-5 Extended |
6GK7 443-5DX02-0XE0 as from firmware V3.2
6GK7 443-5DX03-0XE0
6GK7 443-5DX04-0XE0 |
The firmware update of CP 443-5 Ext. with order number 6GK7 443-5DX02-0XE0 to V3.3 is available in Entry ID: 12011123. Configure the module in the HW Config still as V3.2. |
| CP 443-1 |
6GK7 443-1EX02-0XE0
6GK7 443-1EX10-0XE0
6GK7 443-1EX11-0XE0
6GK7 443-1EX20-0XE0 |
|
Table 05
Interfaces of the CPU CPUs as from firmware V5.1 support the interfaces on the CPU for data record routing. The following versions are possible:
- Standard CPU with PROFIBUS DP interface
- Standard CPU with PROFIBUS DP interface and Ethernet interface
The matrix below shows the versions of PCS 7 with which you can use the interfaces of the CPU for data record routing.
| PDM data record routing over the interfaces of the CPU |
Standard CPU as from V5.1 |
Standard CPU PN as from V5.1 |
| PCS 7 V7.0 |
CPU cannot be configured |
CPU cannot be configured |
| PCS 7 V7.0 SP1 / SP2 / SP3 |
Yes |
Yes |
| PCS 7 V7.1 |
Yes |
Yes |
| PCS 7 V7.1 SP1 / SP2 / SP3 |
Yes |
Yes |
Table 06
Note
If the interface of the CPU is used for data record routing, that CPU must be configured in the HW Config with at least firmware V5.1 or higher.
You can use the AS components below for data record routing.
| Hardware supported |
| Y link and IM 153 Redundancy Bundle |
No restrictions |
| DP/PA link / IM 157 |
No restrictions |
| DP/PA coupler |
Ex: 6ES7 157-0AD00-0XA0 and successor products |
| Not Ex: 6ES7 157-0AC80-0XA0 as from release 3 and successor products |
| ET 200M |
6ES7 153-2AA01-0XB0 and successor products |
| ET 200iS |
No restrictions |
| ET 200iSP |
No restrictions |
Table 07
Note
Note the released modules of your version of PCS 7 in Entry ID: Extend the hardware catalog of your version of PCS 7 as required by installing a PCS 7 Service Pack (SP).
4. AS components in PCS 7 V6.x
PCS 7 V6.x supports the interfaces below for data record routing:
- Communications processors
- Interfaces of the CPU
Communications processors
| Communications processors supported |
| CP 443-5 Extended |
6GK7 443-5DX02-0XE0 as from firmware V3.2 |
The firmware update for V3.3 is available in Entry ID: 12011123. Configure the module in the HW Config still as V3.2. |
| CP 443-1 |
6GK7 443-1EX02-0XE0
6GK7 443-1EX10-0XE0
6GK7 443-1EX11-0XE0 |
|
Table 08
Interfaces of the CPU Standard CPUs as from firmware V5.1 support the PROFIBUS DP interfaces of the CPU for data record routing.
The matrix below shows the versions of PCS 7 with which you can use the interfaces of the CPU for data record routing.
| PDM data record routing over the interfaces of the CPU |
Standard CPU as from V5.1 |
| PCS 7 V6.0 |
CPU cannot be configured |
| PCS 7 V6.1 |
CPU cannot be configured |
| PCS 7 V6.1 SP1 |
Yes using the PCS 7 HSP from Entry ID 26685708. |
| PCS 7 V6.1 SP2 / SP3 / SP4 |
Yes |
Table 09
Note
If the interface of the CPU is used for data record routing, that CPU must be configured in the HW Config with at least firmware V5.1 or higher.
You can use the AS components below for data record routing.
| Hardware supported |
| Y link and IM 153 Redundancy Bundle |
No restrictions |
| DP/PA link / IM 157 |
No restrictions |
| DP/PA coupler |
Ex: 6ES7 157-0AD00-0XA0 and successor products |
| Not Ex: 6ES7 157-0AC80-0XA0 as from release 3 and successor products |
| ET 200M |
6ES7 153-2AA01-0XB0 and successor products |
| ET 200iS |
No restrictions |
| ET 200iSP (as from PCS 7 V6.1) |
6ES7 152-1AA00-0AB0 and successor products |
Table 10
Note
Note the released modules of your version of PCS 7 in Entry ID: Extend the hardware catalog of your version of PCS 7 as required by installing a PCS 7 Service Pack (SP).
By extending to PCS 7 V6.1 SP4 you can figure the CPUs below with the firmware V5.1 to V5.3.
| Configurable CPUs |
Order number |
| CPU 414-3 DP |
6ES7 414-3XM05-0AB0 |
| CPU 416-2 DP |
6ES7 416-2XN05-0AB0 |
| CPU 416-3 DP |
6ES7 416-3XR05-0AB0 |
| CPU 417-4 |
6ES7 417-4XT05-0AB0 |
Table 11
5. AS components in PCS 7 V5.x The interfaces of the Standard CPU cannot be used for data record routing with PCS 7 V5.x. Standard CPU/CPU PN with firmware V5.1 or higher cannot be configured. Therefore, for data record routing use the communications processors listed below.
| Communications processors supported |
| CP 443-5 Extended |
6GK7 443-5DX02-0XE0 as from firmware V3.2 and successor products |
The firmware update for V3.3 is available in Entry ID: 12011123. Configure the module in the HW Config still as V3.2. |
| CP 443-1 |
6GK7 443-1EX02-0XE0 and successor products
6GK7 443-1EX10-0XE0 and successor products |
|
Table 12
You can use the AS components below for data record routing.
| Hardware supported |
| Y link and IM 153 Redundancy Bundle |
No restrictions |
| DP/PA Link |
No restrictions |
| DP/PA coupler |
Not Ex: 6ES7 157-0AD00-0XA0 and successor products |
| Ex: 6ES7 157-0AC80-0XA0 as from release 3 and successor products |
| ET 200M |
6ES7 153-2AA00-0XB0 and successor products |
| ET 200iS |
No restrictions |
Table 13
Note
Note the released modules of your version of PCS 7 in Entry ID: Extend the hardware catalog of your version of PCS 7 as required by installing a PCS 7 Service Pack (SP).
6. Data record routing with IE/PB link If the combination of CPU and communications processor does not support data record routing, the IE/PB link can be used as a data record gateway. In this way, for example, you can access diagnostics and maintenance data from intelligent field devices and field components over SIMATIC PDM.
You can use the IE/PB links below for data record routing.
| Hardware supported |
| IE/PB Link |
6GK1411-5AA00 |
| IE/PB Link PN IO |
6GK1411-5AB00 |
Table 14
7. FAQs, descriptions of application, and manuals
| No. |
Title |
Entry ID |
| 1 |
FAQ - Which requirements have to be fulfilled to perform a STEP 7 routing by means of a PG/PC Station? |
16620173 |
| 2 |
FAQ - What is the difference between Routing and Data Record Routing? |
7000978 |
| 3 |
FAQ - Inter-subnetwork data record routing with a gateway CPU |
20983154 |
| 4 |
FAQ - Which modules and their firmware versions are released for PCS 7 and how can you upgrade them? |
39709060 |
| 5 |
Description of application - Connecting third-party IOs to PCS 7 by means of an IE/PB Link PN IO |
31536572 |
| 6 |
Manual - Process Device Manager SIMATIC PDM |
37565982 |
| 7 |
Function manual - SIMATIC Process Control System PCS 7 Maintenance Station |
57347315 |
Table 15
Additional Keywords
System requirements Hardware requirements
|