show the entry list
Micromaster 4 -- Commissioning and operation -- Optimizing performance
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Boost setting for v/f characteristic and heavy duty starting.
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How can I optimize the standard motor identification routine (MOT-ID) for VC and SLVC?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How can I reverse the drive automatically to clear an overload in a material feed system?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How is the feedback signal configured when using PID control?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How is droop control used in load sharing applications?
MICROMASTER 4 (MM4): How do I set up Torque Control on the MM440?
MICROMASTER 440 (MM4): Shut down the MM440 in the event of loss of Vector action
MICROMASTER 440 (MM4), SINAMICS G120 (CU2x0x): How can I use Sensorless Vector Control (SLVC) on the MM440 or SINAMICS G120 (CU2x0x)?
MICROMASTER 4 (MM4): What is to be understood by "Fast current limit"?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How is the stator resistance set?
Micromaster 4 -- Commissioning and Operation -- Utilising Functions
MICROMASTER 4 (MM4): What are the different ways of selecting variable torque operation using P0205, P0500 and P1300?
MICROMASTER 4 (MM4): How do I set up Torque Control on the MM440?
MICROMASTER 4 (MM4), SINAMICS G120: How can I parameterize the flying restart function?
How can a MICROMASTER 440 be switched ON / OFF using a setpoint?
How to control a MICROMASTER 420 using pushbuttons (without relay interconnection).
MICROMASTER 4 (MM4), SINAMICS G120: How do I conduct a 50/60Hz change-over?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How do I use the JOG function in Torque Control?
MICROMASTER 4 (MM4): How do I use the positioning feature on the MM440?
MICROMASTRER 440 (MM4): Are there any problems switching from speed control to torque control with MM440 (SW above 2.0) while running?
MICROMASTER 4 (MM4): How do I use different parameter sets with the MM440/MM430?
MICROMASTER 4 (MM4): How do I set up Torque Control on the MM440?
Part number:
This FAQ applies only to the SINAMICS G120/G120D Control Units without “-2” in the product name and MICROMASTER 4 inverters.

The Torque Control on the MM440 functions extremely well and can be used for tension control etc. providing a few simple set up rules are followed:

  1. Set the drive up in Sensorless Vector Control first. See the FAQ  "MM440: Sensorless Vector Control (SVC)" (FAQ ID: 7494205).
    Check the drive functions correctly in SVC, as Torque Control operates using SVC.
     
  2. Select the source of the Torque Control setpoint using parameter P1500. Parameter P2003, the reference torque, should be used to define the 100% torque value.
    For example, P1500 = 2 will select the analogue input, 0-10V.
     
  3. Enable Torque Control by setting P1300 = 22.

  4. The actual torque (in Nm) can be monitored (whether in Torque Control or not) using r0031; setting P0005 = 31 displays this in the display in place of output frequency. Compare this with the desired torque or the motor torque to give an idea if the scaling is correct.
      
  5. If necessary, torque control loop stability may be tuned using the current control parameters P1340 and P1341, but this is not usually necessary.  

Warning
Remember Torque Control means that if there is no load the motor might run at maximum frequency, so some other limit may be needed, such as a maximum frequency setting (P1082) or an indication of a threshold frequency such as P0731 = 53.4 (refers to P2155) (see below).

 

Tip 1: Working with Torque and Frequency Control
It is often useful to operate with Frequency and Torque control signals from two separate inputs. This is best achieved by operating the MM440 in Sensorless Vector Control, with the main frequency setpoint derived from analogue input 1, and the torque limit signal derived from the second analogue input (terminals 10 AN+ and 11 AN-). In practice, this means either Frequency or Torque can be in continuous control, while the second input acts as a limiting control, with the controls crossing over as necessary.

parameterization

  • P1000 = 2 (Frequency setpoint from AN1)
  • P1300 = 20 (Sensorless Vector Control)
  • P1500 = 0
  • P1522 = 755.1 (Upper torque limit from AN2)

The second analogue input may be scaled by setting P0756 - P0761... index 1.
The reference torque may be adjusted using P2003.

Tip 2: Working with Negative Torque (e.g. in an unwinder application)
In the above example, if the torque is negative, for example in an unwinding application, AN2 may be connected to P1523, the lower torque limit setting. It is necessary to rescale the AN2 to allow negative values to be set (e.g. 0 to 10V = 0 to -100% torque).
The frequency setpoint may also be scaled appropriately (e.g. AN1 0 to 10V = 0 to -50Hz).

Tip 3: Working with Positive and Negative Torque
If AN2 is to control both positive torque and negative torque, then it is necessary to adjust both P1522 (for example 0 to 100%) and P1523 (for example 0 to -100%) using AN2. This can be achieved by using the inversion of signal that occurs in the PID loop.

  • Connect AN2 to PID feedback P2264 = 755.1
  • Now connect the scaled output r2272 (normally the same) to the upper torque limit P1522 = 2272.
  • Now connect the Error value r2273 (normally 2272 multiplied by -1) to the lower torque limits P1523 = 2273.
  • Both the upper and lower torque limits are continuously adjustable from AN2.

The drive will now operate at either one of these limits, or an alternative setpoint such as frequency, current limit etc.

note
FAQ: "How do I use the JOG function in Torque Control?" Entry-ID: 16818432

 Entry ID:7714804   Date:2013-04-03