Description: The attached document contains a description of the various memory concepts. To give you a better overview, the various memory concepts in the document are described in separate tables. The last chapter of the document includes a list of the various SIMATIC S7-300 controllers and C7 devices and their associated memory concepts.
The document is divided into the following chapters:
- Overview of the Memory Areas and Memory Concept
1.1 Memory Areas
1.2 Memory Concept
1.2.1 Load Memory
1.2.2 Main Memory
1.2.3 System Memory
1.3 Determining the Memory Parameters of a CPU
- SIMATIC S7-300 CPUs and C7 Devices Without Bay
2.1 Graphic Display of the Memory Concept
2.2 Load Memory
2.3 Main Memory
2.4 Application of the Buffer Battery
- SIMATIC S7-300 CPUs and C7 Devices With MC Bay
3.1 Graphic Display of the Memory Concept
3.2 Load Memory
3.3 Main Memory
3.4 Application of the Buffer Battery
- SIMATIC S7-300 CPUs and C7 Devices With MMC Bay
4.1 Graphic Display of the Memory Concept
4.2 Load Memory
4.3 Main Memory
4.4 Application of the Buffer Battery
- Memory Concepts of SIMATIC S7-300 CPU Types and C7 Device Types in Detail
5.1 Memory Concepts of SIMATIC S7-300 CPU Types
5.2 Memory Concepts of C7 Device Types
Attachment 01: Speicherkonzepte_bei_SIMATIC_S7-300_e.pdf ( 396 KB )
Important: The memory concept for the SIMATIC CPU 318-2DP is similar to that for the SIMATIC S7-400 CPUs (see Entry ID:7302549).
Information on SIMATIC S7-300 CPUs with/without memory card (MC) is available in the following entries.
- Data of the individual CPUs is available in the manual "SIMATIC PLC S7-300, CPU Specifications CPU 312 IFM to CPU 318-2 DP ", section 1.4 in Entry ID: 8860591
- Notes on the various types of memory card and their properties are available in "SIMATIC PLC S7-300, CPU Specifications CPU 312 IFM to CPU 318-2 DP", section 1.1 in Entry ID: 8860591
Information on SIMATIC S7-300 CPUs with micro memory card (MMC) is available in the following entries.
- Data of the individual CPUs is available in the manual "CPU 31xC and CPU 31x: Specifications", chapters 6 and 7 in Entry ID: 12996906
- Notes on the various types of micro memory card and their properties are available in "S7-300 CPU 31xC and CPU 31x, Specifications", sections 4.1, 6.1 and 7.1 in Entry ID: 12996906
- Notes on overall reset of the CPU can be found in the manual "S7-300 CPU 31xC and CPU 31x, Specifications", section 4.2, in Entry ID: 12996906
Information independent of the type of memory card (MC or MMC)
- Notes on the topic of "How can you back up your program from the load memory?" are available in Entry ID: 299133
- Notes on the topic of "What is the effect of the STEP 7 function "Copy RAM to ROM"?" are available in Entry ID: 15389520
Keywords:
CPU selection, Memory cards
|