show the entry list
PROFIBUS PC CPs -- Product information -- System description
What are the requirements for using the S7 routing function and which modules can you implement?
Notes on using the DPC2 starting with SIMATIC NET CD 07/2001
How do you create a GSD file for the CP 5614 in COM PROFIBUS V3.3 in order to link it as a DP slave to a DP master system?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What is the difference between SoftNet and HardNet communication processors?
Industrial Ethernet PC CPs -- Product information -- System description
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
How can you display the security status of the CP1628 over the Online View in the Security Configuration Tool (SCT)?
What are the requirements for changing from CP1613 A2 to CP1623?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
In which order should you install the software of the Development Kit DK16xx PN IO in order to load the configuration or firmware of the CP1616 via NCM PC?
What are the requirements for using the S7 routing function and which modules can you implement?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What is the difference between SoftNet and HardNet communication processors?
What is the difference between SoftNet and HardNet communication processors?
Part number:

Configuration Notes:
Every communication uses different protocol layers of the ISO-OSI 7-layer model (e.g. transport layer). The protocol layers can be realized both through software on the communication processor and through software on the computer. If the computer is to do this task, then you have SoftNet card. If the work is done by the communication processor itself, then you speak of a HardNet card.
For the definition of whether you have a HardNet or SoftNet, therefore, it is important to know where the data exchange between the layers takes place. SoftNet communication processors simulate the required protocol via the computer and use the card only for the physical adapting of the signals to the bus system.

A HardNet card on the other hand has its own processor that handle the protocol processing independently. The driver software in the operating system (e.g. Windows NT) for this communications processor simply adds layers 6 and 7 to the protocol.

If you have to make a decision about which communications processor you want to use, then you must take the loading of the computer into account. If your computer is already heavily loaded by an application (e.g. WinCC), then it is always recommended to use a HardNet card.

Keywords:
System requirements, Minimum requirements, Performance

 Entry ID:7028809   Date:2007-12-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour