show the entry list
STEP 7 -- Working with projects -- Defining network topologies
How can I determine the actual status of all S7 connections (standard and high available)?
What is the difference between "normal routing" and data record routing?
S7-300 CPU 31x -- Product information -- Background and system information
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when using the alarm numbering procedure?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
What is the maximum number of parameters that can be assigned to an FC and FB in the S7-300 CPU?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Why is only a warm start available for S7-300?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Which entries deal with consistent data in conjunction with distributed I/O?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
What are the requirements for using the S7 routing function and which modules can you implement?
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices?
Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC
Status of the run-time meter after overall reset
Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables?
Local data addressing with S7-300 / S7 400
S7 300 run-time meter doesn't give any value
S7-400 CPU 41x -- Product information -- Background and system information
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Behavior of the CPU after power off without back-up battery
I/O addressing with DP slaves
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What is the difference between a restart (warm restart), cold restart and hot restart of a S7-400 CPU?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
Which entries deal with consistent data in conjunction with distributed I/O?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
What are the requirements for using the S7 routing function and which modules can you implement?
CPU does not work in RUN
What does "Correction factor" mean in the "Diagnostics/Clock" tab of the CPU's Properties dialog?
What is multicomputing mode and what are the differences to operating in the segmented subrack?
Differing information on the requirement of offline/ online memory
How can I get an overview of the S7-400 memory concept?
PROFIBUS S7-300/400 CPs -- Product information -- System description
What is the difference between "normal routing" and data record routing?
Which modules can you use when implementing software redundancy?
What are the functional restrictions of old releases and firmware versions for the S7-400 CPUs operating in conjunction with the CP443-5 Extended V6.1?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Meaning of the numeric display in the NCM diagnostics buffer
Which protocols does CP 342-5 support?
Different block behavior of the FC5 and FC50 for Ind. Ethernet S7 300 CPs
What are the requirements for using the S7 routing function and which modules can you implement?
What properties, advantages and special features does the DP protocol offer?
What properties, advantages and special features does the FMS protocol offer?
What properties, advantages and special features does the S7 protocol offer?
What properties, advantages and special features does the FDL protocol offer?
Network transitions and links (DP) -- Product information -- System description
What is the difference between "normal routing" and data record routing?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What are the requirements for operating the DP/ASi-Link Advanced as DP master on a CP 443-5 Extended?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What are the requirements for using the S7 routing function and which modules can you implement?
How is the DP/PA link structured?
Unidirectional data transfer with the DP/DP coupler
Documentation for the DP/PA coupler in Dutch, Danish, Finnish, Swedish, Portuguese and Greek
What is the difference between "normal routing" and data record routing?
Part number:

Description
Routing is the transfer of data beyond network boundaries. In this case you can send data from a sender to a receiver over various networks. For this you need special device technology that provides this functionality.

Data Record Routing is an extension of "normal routing" and is used for drives, for example and by SIMATIC PDM when the programming device is not connected directly to the PROFIBUS DP subnet to which the target device is also connected, but to the PROFINET interface of the CPU, for example.

The data sent with data record routing includes the parameter assignment of the field devices participating (slaves) and also device-specific information (setpoint values and limit values, for example). In data record routing, the structure of the target address depends on the data content, that is on the slave for which the data is destined.

With the PG you can use data record routing to read and edit a parameter record already on the field device or send it to the field device if the PG is already assigned as target slave to another subnet.

The field devices themselves do not have to support data record routing, because these devices do not forward the information content.

The following S7-300 CPUs and components of distributed IO devices support data record routing:
 
CPU Version
CPU 313C-2 DP V3.3
CPU 314C-2 DP V3.3
CPU 314C-2 PN/DP V3.3
CPU 315-2 DP V3.0
CPU 315F-2 DP V3.0
CPU 315-2 PN/DP V3.1
CPU 315F-2 PN/DP V3.1
CPU 317-2 DP V3.3
CPU 317F-2 DP V3.3
CPU 317-2 PN/DP V3.1
CPU 317F-2 PN/DP V3.1
CPU 319-3 PN/DP V2.7
CPU 319F-3 PN/DP V2.7
IM154-8 PN/DP CPU V3.2
IM154-8F PN/DP CPU V3.2
IM154-8FX PN/DP CPU V3.2
IM151-8 PN/DP CPU V2.7
IM151-8F PN/DP CPU V2.7
Table 01

S7-400 CPUs firmware version V5.1 onwards support data record routing. For this the CPUs must also be configured in a higher firmware version.
 
CPU Version
CPU 412-1 V5.1
CPU 412-2 DP V5.1
CPU 412-2 PN V6.0
CPU 414-2 DP V5.1
CPU 414-3 DP V5.1
CPU 414-3 PN/DP V5.1
CPU 414F-3 PN/DP V6.0
CPU 416-2 DP V5.1
CPU 416-3 DP V5.1
CPU 416F-3 DP V5.1
CPU 416-3 PN/DP V5.1
CPU 416F-3 PN/DP V5.1
CPU 417-4 V5.1
CPU 412-5H PN/DP V6.0
CPU 414-5H PN/DP V6.0
CPU 416-5H PN/DP V6.0
CPU 417-5H PN/DP V6.0
Table 02

The following communications processors (CPs) support data record routing:
 
CP Order number Version
CP443-5 Extended 6GK7443-5DX02 V3.0
CP443-5 Extended 6GK7443-5DX03 V4.0
CP443-5 Extended 6GK7443-5DX04 V6.0
Table 03

The following gateways support data record routing:
 
CPU Order number
IE/PB Link 6GK1411-5AA00
IE/PB Link 6GK1411-5AB00
IWLAN/PB Link 6GK1417-5AB00
IWLAN/PB Link 6GK1417-5AB01
Table 04

Additional Information
Refer to the manuals of the CPUs to see whether or not the data record routing function is supported. The manuals of the above-mentioned CPUs, gateways and CPs are available in the following Entry IDs:
  
Manual Entry ID
SIMATIC S7-300 CPU 31xC and CPU 31x:
Technical data
12996906
SIMATIC S7-400 Automation System
S7-400 CPU Specifications
53385241
IM 154-8 PN/DP CPU (ET 200pro) 44251850
IM 151-8 PN/DP CPU (ET 200S) 47409312
IE/PB Link 19299692
IWLAN/PB Link 41297182
Table 05

More information about data record routing is available in Entry IDs 19257092 and 7808062.

Note
Data record routing by means of the backplane bus is not supported for an I slave. The data for these modules cannot be routed over the backplane bus.

Additional Keywords
Process device communication, Field device communication

 Entry ID:7000978   Date:2012-11-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour