show the entry list
WinCC Web Navigator -- Product information -- Checking compatibility
Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x?
Which WinCC/Web Navigator client can be connected to which WinCC/Web Navigator server?
WinCC -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
Important note on Microsoft Patches KB 943459 and KB 971468
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
How can you find out which Microsoft Patches are installed on the PC?
Further information on the Catalog ST80 with regard to WinCC Communication
Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x?
With which Microsoft Windows operating systems is SIMATIC WinCC/ProAgent compatible?
Which security patch do you need for installing SIMATIC WinCC V6.0?
Drivers on the SIMATIC NET CD 07/2001 and WinCC
Notes on using WinCC V5.1 with "SIMATIC NET 7/2001 SP4"
Microsoft Windows language versions released for SIMATIC WinCC V5.1
Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x?
Part number:

Configuration Notes
The requirements for the WinCC Web Navigator hardware and operating system are given in the WinCC Web Navigator Help under "Start > SIMATIC > WinCC > Web Navigator > Web Navigator Information System > Contents > Requirements > Hardware and Software".

Operating system and software requirements for SIMATIC WinCC Web Navigator V1.x:
WinCC Web Navigator V1.x Compatibility list ( 72 KB )
 

Operating system and software requirements for SIMATIC WinCC Web Navigator V6.x:
WinCC Web Navigator V6.x Compatibility list ( 64 KB )
 

Operating system and software requirements for SIMATIC WinCC WebNavigator V7.0:
WinCC Web Navigator V7.0 Compatibility list ( 66 KB )

Operating system and software requirements for SIMATIC WinCC Web Navigator V7.2:
Detailed information is available in the manual here: Link

Notes on WinCC Web Server V1.x

  • If the server is being used as a standalone computer and is only installed as server because of the WinCC/Web Navigator client, then please do a customized installation of Microsoft Windows NT 4.0 and do not install the "Domain Controller" option.
  • Microsoft Internet Information Server (IIS)
    The IIS is contained on the Microsoft Windows 2000 CD. It is installed automatically in Microsoft Windows 2000 Server. In the case of Microsoft Windows 2000 Professional, you have to install the IIS afterwards by way of "Start > Settings > Control Panel > Software > Add/Remove Windows Components".
    You can install the IIS in Microsoft Windows NT 4.0 with the 5-language Option Pack CD supplied.
  • If the server is being used as a standalone computer and is only installed as server because of the WinCC/Web Navigator client, then please do a customized installation of Windows 2000 and do not install the "File Transfer Protocol (FTP) Server" and "SMTP Service" options.

Notes on WinCC Web Client V6.x and V7.x

  • You must disable the Windows firewall in Windows XP SP2 on Web Clients with WinCC Basic system V6.0 SP3, V6.0 SP4 or WinCC File Server.
  • Using the MSI technology when installing the Web Client means that the "MS Installer" service is required on the target computer. However, this is not available in Windows NT V4.0. You can install the service via the "instmsiw.exe" file on the "Web Navigator" product CD.
  • Access to intranet / Internet or TCP/IP connection to the Web Server

Notes on WinCC Web Server V6.x and V7.x

  • You must disable the Windows firewall in Windows XP SP2 on computers with WinCC Basic system V6.0 SP3, V6.0 SP4 or WinCC File Server.
  • In order to use more than 3 clients, you must install the server version Windows 2000 Server or Windows Server 2003, because the workstation version is limited to three clients.
  • Access to intranet / Internet or TCP/IP connection to the Web client
  • Microsoft Internet Information Server (IIS):
    The IIS is on the Microsoft Windows 2000 CD. It is installed automatically in Microsoft Windows 2000 Server. In the case of Microsoft Windows 2000 Professional, you have to install the IIS afterwards by way of "Start > Settings > Control Panel > Software > Add/Remove Windows Components".
    In the case of Microsoft Windows XP, you have to install the IIS afterwards via "Start > Settings > Control Panel > Software > Add/Remove Windows Components".
     The IIS is already installed in Microsoft Windows Vista. You have to activate this by going to "Start > Control Panel > Programs and Functions > Enable/Disable Windows Functions > Internet Information Services". Details on the settings are available in the WinCC Information System under "Options > WinCC/WebNavigator > WinCC/WebNavigator Installation Notes > Installation of the WinCC/Web Navigator Server > Installation of the Internet Information Service (IIS)". 
     The IIS is already installed in Microsoft Windows 7. You have to activate this by going to "Start > Control Panel > Programs and Functions > Enable/Disable Windows Functions > Internet Information Services". Details on the settings are available in the WinCC Information System under "Installation Notes > Installation Requirements > Software Requirements for the Installation > Windows 7 and Windows Server 2008: Microsoft Internet Information Server (IIS)".
  • If you wish to have the information published in an intranet, you need the following:
    - A network-compatible computer and a LAN connection (LAN = Local Area Network).
    - A system for name resolution, the computer name resolved in IP addresses (IP = Internet Protocol). This step is not mandatory, but it permits you to use "alias names" instead of IP addresses for the connection with your server.
  • If you wish to have the information published in the Internet, you need the following:
    - An internet connection and an IP address from your internet service provider (ISP). You can only publish in the internet if you have a connection to the internet that is provided to you by the internet service provider.
    - A network card that supports the connection with the internet.
    - A DNS registration (DNS = Domain Name System) for your IP address. This step is not mandatory, but it permits you to use "alias names" instead of IP addresses for the connection with your server.
  • If the server is being used as a standalone computer and is only installed as server because of the WinCC/Web Navigator client, then please do a customized installation of Windows 2000. Do not install the "File Transfer Protocol (FTP) Server" and "SMTP Service" options.
Additional Keywords
System requirements, Hardware and software, 24842694, 8719041, 13682280, 19195356, 19236782, 17233440, 19196010, 22065702, 23991658
 Entry ID:6944907   Date:2013-06-17