show the entry list
PROFIBUS S7-300/400 CPs -- Setting up and parameterizing hardware -- Setting up modules for distributed operation
What are the differences between the integrated DP interface of a CPU (e.g. CPU 315-2 DP) and the DP interface of the CP 342-5?
Notes on linking a CP342-5 as DP slave to a DP master with STEP 7
S7-300 CPU 31x -- Configuring and programming communication -- Configuring the PROFIBUS interface
How do you activate the "Prioritized OCM communication" function to improve the OP communication performance?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
Transfer of analog values from and to the PROFIBUS DP slave
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
What are the differences between the integrated DP interface of a CPU (e.g. CPU 315-2 DP) and the DP interface of the CP 342-5?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
What are the options for exchanging data between CPUs via MPI/PROFIBUS DP?
Direct data exchange (internode communication) between two CPU modules
S7 routing via PROFIBUS with S7-300
Rules for accessing the CPU 315-2 DP on distributed I/O (integrated DP interface of CPU 315-2 DP)
Startup of the S7-300 CPUs when slave is not available
Routing with compact CPU and C7-635 as DP slave
How can you tell whether your S7-300/400 master supports DPV1 functions?
What are the differences between the integrated DP interface of a CPU (e.g. CPU 315-2 DP) and the DP interface of the CP 342-5?
Part number:

Configuration Notes:
The fundamental differences between the integrated DP interface of a CPU and the DP interface of the CP 342-5 are shown in the tables below.
 

Configured as

CP 342-5

CPU 315-2

DP master

In more recent releases of the CP 342-5/CP342-5 FO (6GK7 342-5DA01-0XE0, 6GK7 342-5DA02-0XE0 or
6GK7 342-5F00-0XE0), you can select the DP slaves directly from the standard catalog.

The CP342-5
(6GK7 342-5DA00-0XE0) only supports standard slaves. Consequently, you can only use the slaves that are contained in the HW Catalog under "PROFIBUS-DP > CP 342-5 as DP-Master" or "PROFIBUS-DP > DP V0-Slaves". Whenever GSD files are used, please bear in mind that you can only use DP standard slaves here, too.

You can select all the DP slaves directly from the standard catalog.

DP slave

The I/O modules are configured via universal modules which are then adapted in accordance with the slave's actual I/O data.

Table 1: Differences in configuration

 

CP 342-5

CPU 315-2

Data transfer between the CPU and the CP takes place via special block calls (FC1 "DP_SEND" and FC2 "DP_RECV"). The user is free to select the source or target areas of the data being received or sent. You can use a data block, the bit memory address area or the I/O area for this.

As the I/O area cannot be accessed directly, the I/O addresses may occur repeatedly if there is more than one CP in use.

You can find a description of these blocks in the "SIMATIC NET NCM S7 for PROFIBUS" manual under Entry ID: 1158693.

As in centrally plugged-in modules, the DP slave data is located in the CPU's I/O area. This data can be accessed directly via load and transfer commands, such as "U E 1.0".

Table 2: Programming the data transfer

The volume of project data supported by the modules is release-dependent.
Various modules are compared in the table below:
 

DP master interface

Max. number of DP slaves

I/O area as a ...

DP master

DP slave

CPU 315-2DP
(6ES7 315-2AF03-0AB0)

64

1 KB

244 bytes

CPU 316-2DP
(6ES7 316-2AG00-0BA0)

125

2 KB

244 bytes

CPU 318-2DP
(6ES7 318-2AJ00-0AB0)

125

8 KB

244 bytes

CP 342-5
(6GK7 342-5DA00-0XE0)

124

240 bytes

86 bytes

CP 342-5
(6GK7 342-5DA02-0XE0)

124

2160 bytes

240 bytes

Table 3: Differences in the volume of project data

 

CP 342-5

CPU 315-2

The entire data area (up to 2160 bytes) can be regarded as consistent if the following procedure is followed:

  • The received data can only be analyzed if the block signals that new data has been received error-free.
  • The data being sent is left unchanged until the block reports that the data has been transmitted error-free.

If the procedure differs, this results in a data consistency of 32 bytes.

SFC calls (SFC14/15) have to be used in order to transmit consistent data measuring 3 or 4 bytes in length. SFC14 "DPRD_DAT" is used to read and SFC15 "DPWR_DAT" is used to write consistent data.

The maximum number of pieces of consistent data is dependent on the CPU used. You can find these details in the "CPU Data" manuals.

Table 4: Differences in consistent data

 

CP 342-5

CPU 315-2

CPs 342-5 (from 6GK7 342-5DA02-0XE0) or CPs 342-FO (6GK 342-5DF00-0XE0) support baud rates of up to 12 MB.

Exception:
CP 342-FO supports neither 3 nor 6 MB.

Previous releases of CPs
(6GK7 342-5DA00-0XE0 or
6GK7 342-5DA01-0XE0) only support baud rates of up to 1.5 MB.

The integrated interfaces of the CPU support baud rates of up to 12 MB.

Table 5: Differences in the supported baud rate

You can find further information about this topic in the following Entry IDs:
 
Topic: Entry ID:
Frequent user errors when using the CP 342-5 as DP master 18208090
Version of the function blocks needed to operate a CP 342-5? 187699
What should you watch out for when upgrading the CP 342-5 or fitting spare parts? 7806643
CP342-5 manual 8773570
Manual "SIMATIC NET NCM S7 for PROFIBUS", chapter 4 "DP Master Mode" 1158693

 Entry ID:689920   Date:2003-09-04 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour