show the entry list
ProTool -- Creating HMI configurations -- Creating pictures
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Programming the "Set_Bit" function by pressing a button on Windows-based devices
Picture change on the TP170A as tag function
CPU functions for S7-300 with OP7/OP17
Entering an S5TIME" variable in ProTool/Pro to provide values for a timer in the SIMATIC controller
Showing an "S5TIME" variable from a SIMATIC logic control with ProTool/Pro
Configuring the TAB order ProTool
Subsequent insertion of pictures in the configuration
Graying in the OP display of bitmap graphics
Description of the default name "PIC_xx" for a ProTool/Pro screen
Can I also program function keys in the message image?
Special characters and language-specific characters
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Settings required for implementation of the ProTool function "Start Program"
Display of help texts for a certain image object on a Touch Panel
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panel 170?
How do you configure screen selection on a line or graphics operator panel via controller job 51?
How do you configure screen selection on a Windows-based operator panel via controller job 51?
How can you make a screen selection on an OP3 via the controller?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can the display for the danger and warning area of an analog display be made in color?
How can you optimize the response time when changing screens via the controller?
How do you monitor and control tags on panels on which the status/control object is not available?
Touch Panel / Operator Panel -- Creating HMI configurations -- Tips and tricks for configuring
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How do you create a time switch with WinCC flexible?
How can you use scripts to dynamize objects in WinCC Comfort and WinCC Advanced?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panels and OP 177B?
Button as pure illuminated indicator with a TP170A
Height of a textbox in a standard configuration (ProTool V6.0)
CPU functions for S7-300 with OP7/OP17
Picture change on the TP170A as tag function
"Tahoma" is the only font that can be used with OP/TP 170A/B and C7-635
How can you implement an OP73 as a handheld?
Picture change on the TP170A as tag function
Part number:


QUESTION:
I want to trigger a picture change via a tag on the TP170A. How can I do this?

ANSWER:
Link the "Select_picture_fixed" function to a tag.

Note:
In the dialog field of the Tag properties, in the Options tab, you must select the "Read Continuously" option. Otherwise the tag is read only if it is contained in the picture currently being displayed.

If you do not set the check mark and the tag is not read in the picture, then the function is not executed when the value of the tag changes.

Keywords:
Picture configuration

 Entry ID:6835690   Date:2001-03-05 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour