show the entry list
OS - WinCC -- Operation and maintenance -- Diagnosing errors
Why do you get the license error message "YMAINR9999 missing" although you are using only the license-free basic diagnostics?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
How can you back up the data of the Windows event viewer?
How do you install the User Mode Process Dumper for diagnostics with WinCC and PCS 7?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Why are the DCOM settings of the WinCC OPC server reset after activating the OS Runtime?
Why is the message "Network not ready yet." displayed when an AutoStart is configured on the OS?
Why are the STEP 7 ActiveX controls (OCX) not shown on the OS server and OS client?
Why aren't all the block icons updated during OS compilation?
What are the causes of PCS 7 control technology and system messages and what measures are to be taken to clear them?
Why does the OS Login Box disappear sometimes in the background?
Length of mapped message texts
What should I do if the Split Screen Wizard closes with an error message?
Why do I get an error message when calling the loop display of a faceplate?
What is the meaning of the WinCC messages "PLC fault synchronous" and "PLC fault asynchronous"?
Why does it take 3 to 5 minutes for the Login Box to open on the client or until the message "No authorization for operation" is displayed?
What might be the cause that the hierarchy display in the overview area of the SIMATIC PCS 7 OS does not work?
Error Message "Group display: Tag .Eventstate does not exist"
Why does "?????" appear as a text on the range selector buttons in the overview area in OS runtime even though the text is available in the SIMATIC Manager?
Why does the error message 10111001 "The group display hierarchy has not been updated" appear?
OS - WinCC -- Working with projects -- Analyzing error messages
What is the meaning of the message: "Cannot find server, start project locally?"?
What is the meaning of the WinCC messages "PLC fault synchronous" and "PLC fault asynchronous"?
Meaning of "UNC-name"
Communication of WinCC Server Standby to PLC via a connection of the Named Connections type with PCS 7 V6.0
What is the meaning of the WinCC messages "PLC fault synchronous" and "PLC fault asynchronous"?
Part number:

Description
The messages "PLC fault synchronous" and "PLC fault asynchronous" are triggered when a synchronous or asynchronous fault is triggered in the PLC.

These can be the following:
 

AS errors, synchronous:

OB 121: Programming error

OB 122: I/O access error

AS errors, asynchronous:

OB 80: Time error (e.g. exceeding cycle time)

OB 81: Power supply error (e.g. battery error)

OB 82: Diagnostics interrupt (e.g. defective fuse on a signal module)

OB 83: Remove/plug interrupt

OB 84: CPU hardware error (e.g. interface error)

OB 85: Program runtime error

OB 86: Subrack failure

OB 87: Communications error

You can delimit these faults by proceeding as follows:

  1. Read out the diagnostics buffer of the CPU.
    (Select CPU in the SIMATIC Manager, right click "Target System" to open the "Module Properties", select the "Diagnostics Buffer" tab).
  2. Evaluate the local variables of the fault OBs.
    Double-click the relevant OB in the block container. With a small STL program transfer the contents of the required local variables into a marker byte or a data block that you have created beforehand. The relevant commands are as follows, for example:

    L

    #OB80_EV_CLASS

    T

    MB80

    or

    L

    #OB80_FLT_ID

    T

    DB1.DBB0

  3. Finally, you must load the modified OB or data block into the PLC.

If you can't clear the cause of the fault message, you have the option of suppressing the message in WinCC Runtime. For this refer to the FAQ "Inhibit messages in Runtime", Entry ID: 25288354.

 Entry ID:673584   Date:2010-11-02 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour