Description: You can use any mouse pointer of your choice. For example, under "<Drive>:\WINNT.400\Cursors" is a selection of different mouse pointers.
Instructions:
| No. |
Procedure |
| 1 |
Open the dialog box via "Start > Run". |
| 2 |
Enter "regedit". |
| 3 |
Go to the path: "HKEY_CURRENT_USER\Software\SIEMENS\WinCC\Graphic-Settings\Cursors" |
| 4 |
Here you can specify the cursor you want to use instead of the default cursor. Enter the path and complete name of the cursor.

Fig. 01
|
Note: With "ActionCursor" you change the cursor for all objects - except text list and I/O field - on which a direct connection or an action has been configured under "Properties > Event > Mouse".
With "IOFieldActionCursor" you can change the cursor for the I/O fields for which you have configured an action under "Properties > Event > Mouse".
With "IOFieldEditCursor" you change the cursor for the I/O fields in which a value can be entered.
The codes "TextlistActionCursor" and "TextlistEditCursor" have the same significance as the I/O codes but are valid exclusively for text lists.
Important: In general, no warranty can be given for direct changes in the Registry because this is entirely the responsibility of the user. In any event, you are advised to make a backup of the registry before undertaking the actions described here. Furthermore, these settings are computer-specific. This means that when you copy the project to another computer, you must make the settings again there.
Note: Information regarding the dynamization of mouse pointers in WinCC V6.0 can be found in Entry ID: 15222441.
Keywords: Pointer dynamization
|