Configuration Notes: With STEP 7 V5.1 there is a new
structure and different behavior of the group messages for the HMI
systems. Previously there were seven group messages. There are now
21 group messages in the new version. The seven original messages
are contained in three groups of seven. The following table lists
the new messages.
|
Message |
Group |
|
AS fault synchronous incoming
AS fault asynchronous incoming
Module fault incoming
Stop/abort fault incoming
H/F system fault incoming
Communications fault incoming
Fault in CP/FM module incoming |
Group 1 |
|
AS fault synchronous outgoing
AS fault asynchronous outgoing
Module fault outgoing
Stop/abort fault outgoing
H/F system fault outgoing
Communications fault outgoing
Fault in CP/FM module outgoing |
Group 2 |
|
Message about AS fault synchronous
Message about AS fault asynchronous
Message from module
Stop/abort message
H/F system message
Communications message
Message from CP/FM module |
Group 3 |
The three groups always contain the same messages for the
different status options of the message (incoming, outgoing, status
unknown).
Because of the properties of the message class "OS Instrumentation
and Control Message" the IC messages do not have an
"incoming/outgoing" display in the message line. Therefore an extra
"incoming" and the "outgoing" message is sent for each individual
message.
The message of the type "outgoing" is however only displayed when
the message of the type "incoming" has also been acknowledged
beforehand. If not, then the message is not displayed again.
Group 3 is needed, because after an update of the message
picture or WinCC ON/OFF (struck-out message), a status is no longer
available. With this type of message supplementary values are
transferred with the event ID and these values contain the status
information. Since the message is always of the type "incoming"
here, it can only be indicated that a message of this type was
here. The user must then look in the diagnostics buffer of the CPU
himself to find out the reason for the message.
Below is the assignment of the organization blocks in STEP 7 to
the individual group messages. This list does not presume to be
complete. It is rather an indication of the possible causes. The
user has to find the associated detailed information in the
diagnostics buffer of the CPU based on the time stamp of the
message concerned.
|
Message |
Detailed information in the
CPU |
|
AS fault synchronous |
OB121, OB122 |
|
AS fault asynchronous |
All OB8x |
|
Module fault |
OB82, OB83, OB86 |
|
Stop/abort fault |
Stop and abort events direct |
|
H/F system fault |
OB71, OB72 |
|
Communications fault |
OB87 |
|
Fault in CP/FM module |
CPs and FMs direct to WinCC |
Keywords: BPC, Basic Process Control, Wizard, IC message
|