show the entry list
Industrial Ethernet Passive Network components -- Product information -- System description
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring PROFINET channel test profiles of 2x2 PROFINET cables?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring the end-to-end link of 2x2 PROFINET cables?
Which connector do you use to connect fiber-optic cables to the optical interface of network components and terminals?
Which settings have to be made on the Fluke DTX-1800 cable analyzer for testing cables in a PROFINET network?
PROFINET general -- Product information -- System description
Where can you find information about the configuration and calculation of RCoax systems?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring the end-to-end link of 2x2 PROFINET cables?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring PROFINET channel test profiles of 2x2 PROFINET cables?
How can you implement the the communication concept of PROFINET CBA with PROFINET IO?
Why is hardware support required for using clock-synchronized real-time communication (IRT) in PROFINET?
How is to possible to transmit real-time messages at the same time as TCP/IP communication in PROFINET?
How can real-time communication (RT) be used with standard Ethernet hardware?
What should you watch out for when reconfiguring in RUN (CiR) if the configuration contains CiR elements and a PROFINET IO system?
Which settings have to be made on the Fluke DTX-1800 cable analyzer for testing cables in a PROFINET network?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Switch on/off phase (central rack and distributed connection)
Comparison of the terms of PROFIBUS and PROFINET
Comparison of PROFINET and PROFIBUS
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring PROFINET channel test profiles of 2x2 PROFINET cables?
Part number:

Description
PROFINET is based on the international Ethernet cabling standard (ISO11801). The cables are tested in compliance with this standard.

Set the test profile below in the measuring instrument to test the cables installed in a PROFINET network.

  • ISO/IEC 11801 Edition 2.0, connector min. Category 5

In this example, LANTEK and LANTEK II from IDEAL are used to test the cables in the PROFINET network.

Note
Use the latest firmware of the LANTEK and LANTEK II measuring instruments.
How to do a firmware update is described in the measuring instrument manual.

The latest firmware of the LANTEK and LANTEK II measuring instruments is available for downloading on the home page of IDEAL INDUSTRIES, INC or together with the software update of the IDEAL DataCENETER.

You need the accessories below for measuring with LANTEK and LANTEK II.

  •  LANTEK CAT6 or CAT6A Universal Adapter

You need the additional accessories below depending on the system to be measured.
 
System Accessories Order number
RJ45 System IDEAL Test Set 1019-00-1116
M12 System IE Connecting Cable
M12-180/IE FC RJ45 Plug-145 (2m, for example)
6XV1871-5TH20
IE Connecting Cable M12-180/M12-180 (2m, for example) 6XV1870-8AH20
IE FC TP Standard Cable GP 4x2 (2m, for example) and
IE FC RJ45 Plug 4x2
6XV1870-2E
6GK1901-1BB11-2AA0
Table 01

Make the settings below on LANTEK or LANTEK II prior to cable testing.

  • Setting to save test details
  • Assignment of name for the measurement
  • Create a project
  • Perform a null measurement

Setting to save test details
Make the settings below on LANTEK and LANTEK II in order to save the details of each measurement.
 
No. Procedure
1 Select the "Test Standards" option in the main menu.


Fig. 01

2 Select the "ISO" menu.


Fig. 02

3 Select the "Twisted Pair Channel" menu.


Fig. 03

4 In the "Twisted Pair Channel" menu you mark the "ISO D STP 2nd Chan" option and press <F2> to create.


Fig. 04

5 Select the "Pin selection" item.


Fig. 05

6 Deselect the items below and press <ENTER>:
  • Pair 7, 8
  • Pair 5, 5


Fig. 06

7 Select the "Customer-specific name/NVP" menu and and press <ENTER>.


Fig. 07

8 In the "Customer-specific name/NVP" menu you enter a name, "PROFINET CHANNEL", for example.

You can set the NVP value for the SIEMENS SIMATIC NET cable types.

Press <F4> to save the settings.


Fig. 08

Table 02

Assignment of name for the measurement
Proceed as described below to assign a name for the measurement.
 
No. Procedure
1 Select the "Cable ID" option in the main menu.


Fig. 09

2 Select the "Select Cable ID" menu.


Fig. 10 

3 In the "Select Cable ID" menu you enter the cable name and current value. Confirm the settings with <ENTER>.


Fig. 11 

Table 03

Create project
You also have the option of creating a project or job. Proceed as follows.
 
No. Procedure
1 Select the "Stored Tests" option in the main menu.
2 Press <F2> to open the options and select the "New Job" item.
3

Enter a name for the job and press <ENTER> to apply the setting. All measurements are now stored in that folder.

4 Optionally you can assign a name to each end of the link. For this you select the "Double Cable ID" option.
5 Optionally you can select the following settings in the menu "Settings > Autotest Preferences":
  • You can switch off the "Simple Cable ID" option. In this way you can use more complex automatic numbering like 21A, 21B.
  • If you enable the "Stop on Fail" option, then the tester stops the test as soon as the first failure is discovered.
  • If you enable the "AutoSave" option, any passed AUTOTEST results are automatically named and saved.
  • If you enable the "Auto Increment" option, the counter is incremented automatically with each passed measurement.
Table 04

Field calibration
Run a field calibration if:

  • No field calibration has been performed in the last 7 days. The user has received a message informing that a field calibration is required.
  • The test adapter has been replaced.
  • A patch cable has been replaced.

To perform the field calibration in RJ45 systems, follow the instructions of the IDEAL Set 1019-00-1116. The instructions are included in the Set.

Proceed as described below to perform a field calibration in M12 systems.

Perform the steps below with an RJ45 patch cable.
 
No. Procedure
1 Use the arrow keys to navigate to the "Field Calibration" display and press <ENTER> to open the job list.


Fig. 12 

Note
The patch cables for the Display Handset (DH) and Remote Handset (RH) must not be mixed up and are to be used as such for cable testing.
We recommend that you mark the patch cables accordingly.

2 Connect the Display Handset (DH) and Remote Handset (RH) as shown in the figure on the display with the RJ45 patch cable.

Press <Start> softkey to start field calibration.


Fig. 13 

3 Leave the RJ45 patch cable plugged in and press the <Start> softkey again.


Fig. 14 

4 Now disconnect the Display Handset (DH) and the Remote Handset (RH).
Table 05

Perform the steps below with an RJ45/M12 patch cable.
 
No. Procedure
1 Connect an RJ45/M12 patch cable to the Display Handset (DH).
2 On the Display Handset (DH) press the <Start> softkey to start the last step of the field calibration.


Fig. 15 

3 Connect the second RJ45/M12 patch cable for the Remote Handset (RH) to the Remote Handset (RH).
4 On the Remote Handset (RH) press <Autotest> to start the last step of the field calibration.
5 Press <ENTER> to confirm the settings.


Fig. 16 

Table 06  

Note
If the latest version of the firmware is not available, you can set ISO 11801 Class D Channel, twisted pair shielded.

More information is available at this link:
http://www.idealindustries.com/

 Entry ID:60541487   Date:2012-05-22 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour