SINVERT PVS 600Series
Peak performance for the power plant market segment PVS585 and PVS630 - New power ratings
What's new? The range of existing inverter power ratings,
- PVS500, PVS1000, PVS1500 and PVS2000 with outputs of between 500kVA and 2000kVA
- PVS600, PVS1200, PVS1800 and PVS2400 with outputs of between 600kVA and 2400kVA
has been expanded by these products to include the following additional ratings:
- PVS585, PVS1170, PVS1755 and PVS2340 with outputs of between 585kVA and 2340kVA
- PVS630, PVS1260, PVS1890 and PVS2520 with outputs of between 630kVA and 2520kVA
More power The new power ratings offer maximum yield combined with perfect adaptability to different MPP windows. The SINVERT PVS585 has a 17% higher output than the SINVERT PVS500 through the implementation of a narrower MPP window and higher rated voltages. The SINVERT PVS630 has a 5% higher output than the SINVERT PVS600 through the implementation of higher rated voltages.
Higher yields and top earnings The new power ratings 585kVA, 1170kVA, 1755kVA and 2340kVA embody the perfect trade-off between maximum power output and a wide MPP window. The new power ratings 630kVA, 1260kVA, 1890kVA and 2520kVA are designed to achieve optimum yields from high-quality modules.
Expanded reactive power range
- The power factor setting range has been extended to 0.8cap...1...0.8ind for all SINVERT PVS 600Series inverters. These devices therefore fulfill the requirements relating to enhanced grid quality.
- The devices can also meet future demands for compensation of voltage variations within extensive medium-voltage networks and for compensation of reactive power in close-meshed medium-voltage networks.
Global or restricted release (standards and approvals): SINVERT PVS 600Series inverters can be employed for any application which requires compliance with the relevant IEC standards.
Other content: For catalogs - brochures - documentation relating to SINVERT products SINVERT Support, go to http://www.siemens.com/sinvert
For technical data and data sheets, go to https://support.automation.siemens.com
Technical assistance for SINVERT products
For technical queries, please call telephone no. +49 (911) 895-5900
Monday to Friday, 08:00 a.m. to 5 p.m. CET - Fax: +49 (911) 895-5907
E-mail: Technical Assistance mailto:technical-assistance@siemens.com |