show the entry list
ProTool -- Creating HMI configurations -- Creating pictures
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Programming the "Set_Bit" function by pressing a button on Windows-based devices
Picture change on the TP170A as tag function
CPU functions for S7-300 with OP7/OP17
Entering an S5TIME" variable in ProTool/Pro to provide values for a timer in the SIMATIC controller
Showing an "S5TIME" variable from a SIMATIC logic control with ProTool/Pro
Configuring the TAB order ProTool
Subsequent insertion of pictures in the configuration
Graying in the OP display of bitmap graphics
Description of the default name "PIC_xx" for a ProTool/Pro screen
Can I also program function keys in the message image?
Special characters and language-specific characters
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Settings required for implementation of the ProTool function "Start Program"
Display of help texts for a certain image object on a Touch Panel
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panel 170?
How do you configure screen selection on a line or graphics operator panel via controller job 51?
How do you configure screen selection on a Windows-based operator panel via controller job 51?
How can you make a screen selection on an OP3 via the controller?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can the display for the danger and warning area of an analog display be made in color?
How can you optimize the response time when changing screens via the controller?
How do you monitor and control tags on panels on which the status/control object is not available?
Configuring the TAB order ProTool
Part number:


QUESTION:
How can I edit the TAB order in ProTool?

ANSWER:
You have to change into a special mode to edit the TAB order. Click "Edit > TAB Order". In this mode a number is displayed on the operator-controllable image objects. This is the TAB order number.
Please proceed as follows to set a new order of the objects (starting with number 1):

  1. Click the image object that is to be the new number 1. Then set the remaining order of numbers by clicking the relevant image objects one after the other.
  2. If you want to correct the TAB order and make a different image object number 1, then keep the "Shift" key pressed and click the appropriate image object.
  3. Once you have assigned all the numbers, you can exit the TAB order mode with "Esc".

If you don't want to start with number 1, then please proceed as follows:

  1. Switch to the TAB order mode (proceed as described above).
  2. Define your "Start number" (not equal to 1) by pressing the "Ctrl" key and clicking the image object with the required number.
    Example:
    If you click the field with the number 5, then this is your start number.
  3. Release the "Ctrl" key.
  4. Define the subsequent order of numbers by clicking the relevant image objects one after the other.
  5. Once you have assigned all the numbers, you can exit the TAB order mode with "Esc".


 Entry ID:6034130   Date:2000-12-18 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour