show the entry list
SINVERT PVM Limiting output power to 70 % - EEG 2012
Part number:

QUESTION:

How can I limit the output power to 70 % on 6AG3120 SINVERT PVM inverter as required in EEG since 2012?

 

ANSWER:

Because of the guidelines of EEG 2012, the display in 6AG3120 SINVERT PVM photovoltaic inverter from firmware 29 was supplemented by menu item “Limitation PAC”. With this, the maximum active power of the inverter can be reduced.

To limit the output power (PAC) of SINVERT PVM to 70% as required in EEG, following steps via parameterization have to be done:

 

Enter user password:

Function key F1

            -> Configuration

                        -> Password

                                    -> 72555 [ENTER]

 

 

Adjust limitation PAC 70%:

Function key F1

            -> Configuration

                        -> Limitation PAC

                                    -> 70 [ENTER]

 

 Entry ID:60114764   Date:2012-04-19 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour