show the entry list
Download of Service Pack 2 for STEP 7 V5.5 Chinese
Part number:

DESCRIPTION:

Download of Service Pack 2 (SP2) for STEP 7 V5.5 Chinese

Installation requirements for Service Pack 2:

  • STEP 7 V5.5 Chinese

Please also read the information (What’s NEW, special hints, etc.) which we have compiled for you at entry ID 60014955.

If you wish to change to a new operating system, please note the following:

  • The precondition to be able to change the operating system with STEP7 is the Product DVD; for ordering please see entry ID 60014955
  • Before you change the operating system, the License Key must be saved from the PC to a floppy disk or USB stick. 
  • Please also note the changed PC hardware requirements of STEP 7; detailled information is provided on the Readme.rtf of STEP 7.

Download of Service Pack 2 for STEP 7 V5.5 Chinese
SIMATIC_STEP7_V55_SP2_Chinese.zip ( 667092 KB )

This free download includes the SP2 for STEP 7 V5.5 Chinese and NCM and can only be installed, if STEP 7 V5.5 Chinese has already been installed on the PC.

 

 Entry ID:60015784   Date:2012-04-18 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour