S7-400H Innovations
The fault-tolerant SIMATIC S7-400H controllers have been innovated.
This includes:
- Integrated PROFINET interface ( 2-port switch) in all CPUs
- Larger quantity structure for data and function blocks and larger memory (alignment with the quantity structures of the standard CPUs S7-400 V6)
- Enhanced communication performance and resources
- New CPU 416-5H PN/DP in addition to CPUs 412/414/417-5H PN/DP
- Support of H connections via TCP/IP (ISO on TCP)
- Support of T communication (OUC connections)
- Integrated Profibus interface as data record gateway
- User-programmable Master-Standby changeover
All controllers including the CPU 412-5H PN/DP have a MPI/DP and a DP interface, as well as a PROFINET interface with integral 2-port switch. The latter can be used for the system-redundant connection of the I/Os, or, if the I/Os are connected via PROFIBUS, for the plant communication. All CPUs including the CPU 412-5H PN/DP support data synchronization via fiber-optic conductors up to 10 km. Programming and configuration is as before in the SIMATIC STEP 7 engineering environment (STEP 7 V5.5 SP2).
Sync modules and FOC sync cables
The sync modules have also been newly designed and are not compatible with the old modules. The FOC sync cables have not changed.
Sync cables with customized lengths up to 10km are still available as described at entry ID 19913764
Compatibility
The new S7-400H controllers are based on a new hardware and the new operating system V6.0. The previous hardware cannot be upgraded and the V6.0 operating system will only run on the new hardware.
The new CPUs are largely compatible with the previous H-CPUs:
- Applications created for the previous CPUs can also be used for the new CPUs.
- In the case of a spare part replacement both CPUs of the H system including their sync modules must be replaced. If the upgrade is from V4 or V4.5 to V6, the Sync cables can be re-used.
Mixing the new CPUs with the previous CPUs in one S7-400H system is not permitted. Existing plant configurations with V4.x can be expanded with new redundancy systems with new V6 systems.
Engineering
To be able to use the new functions you require STEP7 V5.5 SP2 plus HF1 or later versions STEP 7 . The required Hotfix 1 can be downloaded at entry ID 59216386.
Supported PROFINET I/Os
At the time of delivery release, ET 200M stations are supported via the IM 153-4 High Feature (6ES7153-4BA00-0XB0). A new IM firmware is required for operation with the S7-400H; it is available for download at entry ID 26331274. Previous versions can be upgraded.
The new firmware has the new PROFINET function "System Redundancy" implemented, which is required for operation with the 400H. Other PN devices which do not support System Redundancy can be connected as "Onesided I/Os", i.e. allocated to only one of the two CPUs. Other PN devices that already support System Redundancy can be integrated via a suitable GSD file.
Safety
As was the case with the previous S7-400H versions, the new version can also be used as F/FH system. This requires the F Systems V6.1 + SP1 software and Lib V1.3 + SP1, S7 F Configuration Pack V5.5 + SP9 + Update1
PCS7
The V6 H-CPUs can be used with PCS 7 V8.0 Update 1 and higher. Update 1 will be released for delivery by end of April 2012 and will include the necessary additions.
Replacement strategy
The new product spectrum will completely replace the existing products. The current CPUs V4.5 will be declared mature products after approx 6 months and type discontinued one year later. As usual for SIMATIC, the CPUs will remain available for 9 more years on a spare part basis.
Technical data
| |
CPU 412-5H PN/DP |
CPU 414-5H PN/DP |
CPU 416-5H PN/DP |
CPU 417-5H PN/DP |
| |
|
|
|
| Memory |
| For program |
512 kB |
2 MB |
6 MB |
16 MB |
| For data |
512 kB |
2 MB |
10 MB |
16 MB |
| Integrated loading memory |
512 kB |
512 kB |
512 kB |
512 kB |
| Blocks |
DB
FB
FC |
6 000
3 000
3 000 |
16 000
8 000
8 000 |
| Permitted number band |
DB
FB
FC |
1 - 16 000
0 - 7 999
0 - 7 999 |
| Processing times |
Bit operations
Word operations
Fixed-point arithmetic
Floating-point arithmetic |
31.25 ns
31.25 ns
31.25 ns
62.5 ns |
18.75 ns
18.75 ns
18.75 ns
37.5 ns |
12.5 ns
12.5 ns
12.5 ns
25.0 ns |
7.5 ns
7.5 ns
7.5 ns
15.0 ns |
| Communication |
| No. of S7 connections |
48 |
64 |
96 |
120 |
| S7 Signalling functions |
| No. of OPs with AlarmS/AlarmD processing |
15 |
31 |
95 |
| Interfaces |
1st interface
2nd interface
3rd interface
4th interface
5th interface |
X1: MPI/DP interface
X2: DP interface
IF1: Sync module
IF2: Sync module
X5: Profinet |
| CPU order no.'s |
6ES7 412-5HK06-0AB0 |
6ES7 414-5HM06-0AB0 |
6ES7 416-5HS06-0AB0 |
6ES7 417-5HT06-0AB0 |
Dimensions
WxHxD (mm) |
50 x 290 x 219 |
50 x 290 x 219 |
50 x 290 x 219 |
50 x 290 x 219 |
| Sync modules |
| |
for FOC patch cables up to 10m |
for installation cables up to 10km |
| Sync module order no.'s |
6ES7960-1AA06-0XA0 |
6ES7960-1AB06-0XA0 |
Ordering information
| Previous Name |
Previous Order No. |
New Name |
New Order No. |
| CPU 412-3H |
6ES7 412-3HJ14-0AB0 |
CPU 412-5H PN/DP |
6ES7 412-5HK06-0AB0 |
| CPU 414-4H |
6ES7 414-4HM14-0AB0 |
CPU 414-5H PN/DP |
6ES7 414-5HM06-0AB0 |
| - |
- |
CPU 416-5H PN/DP |
6ES7 416-5HS06-0AB0 |
| CPU 417-4H |
CPU 417-4HT14-0AB0 |
CPU 417-5H PN/DP |
6ES7 417-5HT06-0AB0 |
| |
|
|
|
| Sync module near |
6ES7 960-1AA04-0XA0 |
Sync module V6 near |
6ES7 960-1AA06-0XA0 |
| Sync module remote |
6ES7 960-1AB04-0XA0 |
Sync module V6 remote |
6ES7 960-1AB06-0XA0 |
| Sync cable 1m |
6ES7 960-1AA04-5AA0 |
no change |
no change |
| Sync cable 2m |
6ES7 960-1AA04-5BA0 |
no change |
no change |
| Sync cable 10m |
6ES7 960-1AA04-5KA0 |
no change |
no change |
Sync cable
other lenghts and designs |
see 19913764 |
Bundles
| Product Name |
Order Number |
| S7-400H SYSTEM BUNDLE, CPU 412-5H, 10A, 230V AC |
6ES7 400-0HR01-4AB0 |
| S7-400H SYSTEM BUNDLE, CPU 412-5H,, 10A, 24V DC wide range |
6ES7 400-0HR51-4AB0 |
| S7-400H SYSTEM BUNDLE, CPU 414-5H, 10A, 230V AC |
6ES7 400-0HR02-4AB0 |
| S7-400H SYSTEM BUNDLE, CPU 414-5H,, 10A, 24V DC wide range |
6ES7 400-0HR52-4AB0 |
| S7-400H SYSTEM BUNDLE, CPU 416-5H, 10A, 230V AC |
6ES7 400-0HR03-4AB0 |
| S7-400H SYSTEM BUNDLE, CPU 416-5H,, 10A, 24V DC wide range |
6ES7 400-0HR53-4AB0 |
| S7-400H SYSTEM BUNDLE, CPU 417-5H, 10A, 230V AC |
6ES7 400-0HR04-4AB0 |
| S7-400H SYSTEM BUNDLE, CPU 417-5H,, 10A, 24V DC wide range |
6ES7 400-0HR54-4AB0 |
The bundles comprise:
Bundle 412-5H AC 6ES7 400-0HR01-4AB0:
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS407 120/230V AC/DC, 10A 6ES7407-0KA02-0AA0
2 x CPU 412-5H PN/DP 6ES7412-5HK06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
Bundle 412-5H DC 6ES7 400-0HR51-4AB0
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS 405 10A, 24/48/60V DC, 6ES7405-0KA02-0AA0
2 x CPU 412-5H PN/DP 6ES7412-5HK06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
Bundle 414-5H AC 6ES7 400-0HR02-4AB0:
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS407 120/230V AC/DC, 10A 6ES7407-0KA02-0AA0
2 x CPU 414-5H PN/DP 6ES7414-5HM06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
Bundle 414-5H DC 6ES7 400-0HR52-4AB0
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS 405 10A, 24/48/60V DC, 6ES7405-0KA02-0AA0
2 x CPU 414-5H PN/DP 6ES7414-5HM06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
Bundle 416-5H AC 6ES7 400-0HR03-4AB0:
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS407 120/230V AC/DC, 10A 6ES7407-0KA02-0AA0
2 x CPU 416-5H PN/DP 6ES7416-5HS06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
Bundle 416-5H DC 6ES7 400-0HR53-4AB0
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS 405 10A, 24/48/60V DC, 6ES7405-0KA02-0AA0
2 x CPU 416-5H PN/DP 6ES7416-5HS06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
Bundle 417-5H AC 6ES7 400-0HR04-4AB0:
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS407 120/230V AC/DC, 10A 6ES7407-0KA02-0AA0
2 x CPU 417-5H PN/DP 6ES7417-5HT06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
Bundle 417-5H DC 6ES7 400-0HR54-4AB0
1 x UR2-H 6ES7400-2JA00-0AA0
2 x PS 405 10A, 24/48/60V DC, 6ES7405-0KA02-0AA0
2 x CPU 417-5H PN/DP 6ES7417-5HT06-0AB0
4 x Syc modules 10m 6ES7960-1AA06-0XA0
2 x Sync cables 1m 6ES7960-1AA04-5AA0
4 x Backup batt. 6ES7971-0BA00
In addition, you require RAM or FEPROM memory cards, which must be ordered separately.
Further information:
Documentation portal
Documentation portal controllers
SIMATIC S7- 400H on the Internet (a new version will be released in mid. April 2012)
|