show the entry list
WinCC Web Navigator -- Operation and maintenance -- Diagnosing errors
Why is a download installation of a SIMATIC WinCC Web-Client not possible?
How can you disable the Protected Mode of the Internet Explorer when using the WinCC WebNavigator?
With WinCC Web Navigator, how can you have a display of which users are currently accessing the web project?
What is the meaning of the message "You must enable ActiveX Controls on your browser before you are able to install the WinCC Web Navigator Client software" and what can you do about it?
What causes the error message "Network request not supported" when starting the client Web Navigator site from the IIS?
Why do you get the error message "The maximum count of allowed users is connected to the WinCC server"?
Why aren't any tags updated on the WinCC web client?
How can you avoid the "DEMO mode" of the WinCC Web Navigator client?
Why, after migration of a WinCC project from WinCC V5.1 to WinCC V6.0 SP1, is the text originally configured no longer displayed on the Web Navigator client, but only "TEXT" in buttons and in static texts?
How can you prevent an empty page being displayed when you call the diagnostics information saved by the WinCC Web Navigator from the STATUS.HTML page?
Why, after a Microsoft update, can you no longer connect the Web Navigator clients to the Web Navigator server?
Why is there no automatic reconnect between a Web Navigator client and the Web Navigator server via a firewall or a proxy server?
Why can WinCC/Web Navigator or WinCC/Dat@Monitor clients no longer connect to the WinCC/Web Navigator or WinCC/Dat@Monitor server?
How can you disable the Protected Mode of the Internet Explorer when using the WinCC WebNavigator?
Part number:

Description
The "Protected Mode" of the Microsoft Internet Explorer is a feature that reduces the ability of malicious software being installed on your computer. The "Protected Mode" also affects the execution and display of ActiveX control elements used by the WinCC WebNavigator. The "Protected Mode" must therefore be disabled for the trusted sites, otherwise you get this error message displayed: "Low integrity level not supported - please disable Protected Mode".

Instructions
Below is the procedure for disabling the "Protected Mode" of the Internet Explorer for trusted sites.
 
No. Procedure
1 Start the Internet Explorer and open the settings of the Microsoft Internet Explorers by way of "Tools > Internet options".
2 Switch to the "Security" tab.
3 Mark the "Trusted sites" zone and disable the option "Enable Protected Mode (requires restarting the Internet Explorer)".


Fig. 01: Security settings of the Internet Explorer

4 Apply the settings and restart the Internet Explorer.
Table 01

Creation environment
The screens in this FAQ response were created with Windows 7 Ultimate.

Security Notes
Siemens offers products and solutions with industrial security functions which support the secure operation of plants, solutions, machines, devices and/or networks. They are important components in a comprehensive industrial security concept. The Siemens products and solutions continue to be developed under this aspect. Siemens recommends that you keep yourself regularly informed about product updates.
For the safe operation of Siemens products and solutions it is necessary to take appropriate security measures (cell protection concept, for example) and to integrate each component in an overall industrial security concept which is state of the art. This should also cover the third-party products used. Additional information about industrial security is available at:
http://www.siemens.com/industrialsecurity.
In order to keep yourself informed about product updates, we recommend subscribing to our product-specific newsletter. Additional information about this is available at
https://support.automation.siemens.com.

Additional Keywords
Protected Mode

 Entry ID:59902882   Date:2015-01-08 
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
Topics
Help
Online Help
Guided Tour