show the entry list
WinCC ProAgent -- Product information -- Information on WinCC ProAgent
Why do you get the message "WinCC ProAgent Module has stopped working" in SIMATIC WinCC/ProAgent V7.0 SP3?
With which Microsoft Windows operating systems is SIMATIC WinCC/ProAgent compatible?
What are the system requirements and order of installation for SIMATIC WinCC/ProAgent?
ProAgent editor cannot be seen in WinCC
Assignment of a block pair (FB/DB) to an S7-GRAPH step sequence
Displaying comparators in the ProAgent standard image
Installation of WinCC, AS OS Eng. Tool and ProAgent
Generating error - Error Create Variables for Connections
Standstill of the progress display when generating
Using function key F10 with an FI45
Installation ProAgent V4.02 for WinCC parallel to STEP7 V5.0
Why do you get the message "WinCC ProAgent Module has stopped working" in SIMATIC WinCC/ProAgent V7.0 SP3?
Part number:

Description
If the SIMATIC WinCC ProAgent Generation is started in WinCC Runtime, the "WinCC ProAgent Module" dialog issues this error message: "WinCC ProAgent Module has stopped working".


Fig. 01

You can ignore this message. SIMATIC WinCC ProAgent and WinCC continue running normally and do not have to be restarted.

Remedy
Only start the SIMATIC WinCC ProAgent Generation when WinCC Runtime is disabled. Then this message is not issued.

 Entry ID:59613371   Date:2012-04-13 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour