|  |
The STARTER V4.3 SP1 is downwards compatible with the previous STARTER versions and replaces them.
The following drive systems are supported (newly added versions are marked in bold):
- 4th Generation MICROMASTER
- SINAMICS DCM with Firmware V1.1, V1.2 and V1.3
- SIMATIC ET200S FC with Firmware V1.0.x and V3.0.x
- SIMATIC ET200pro FC with Firmware V3.0.x
- SINAMICS G110 with Firmware V1.0.x and V1.1.x
- SINAMICS G110D with Firmware V3.3.x and V3.4.x
- SINAMICS G120 with Firmware V2.0.x, V2.1.x, V3.0.x, V3.1.x, V3.2.x, V4.2, V4.3.0, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS G120C with Firmware V4.4 and (with SSP) V4.5
- SINAMICS G120D with Firmware V3.0.x, V3.1.x, V3.2.x and (with SSP) V4.5
- SINAMICS G120P with Firmware V4.2, V4.3.0, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS G120P BT with Firmware (with SSP) V4.4.1
- SINAMICS G130 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G130 with Firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS G150 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS G150 with Firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS GM150 with Firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GM150 with Firmware V4.3.1, V4.4.2 and (with SSP) V4.5
- SINAMICS GL150 with Firmware V2.5.1, V2.6.1 and V2.6.2
- SINAMICS GL150 with Firmware V4.3.1, V4.4.2 and (with SSP) V4.5
- SINAMICS S110 with Firmware V4.1, V4.3.1, V4.3.2 and (with SSP) V4.4
- SINAMICS S120 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S120 with Firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS S150 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
- SINAMICS S150 with Firmware V4.3.1, V4.3.2, V4.4 and (with SSP) V4.5
- SINAMICS SL150 with Firmware V4.3.1, V4.4.2 and (with SSP) V4.5
- SINAMICS SM120 with Firmware V4.4.2
- SINAMICS MV with Firmware (with SSP) V4.5
Further details regarding drive systems to be supported are provided in the following Excel overview.
Installed_Devices_STARTER_DVD_43010000.xls ( 83 KB )
The following functional extensions are included in the Version V4.3 SP1 compared to the previous version V4.2 HF1:
- Cross-device STARTER functional extensions
- Operating system Windows 7 (64 bit) in the versions Professional, Ultimate and Enterprise
- Write and know-how protection (only online in combination with the drive)
- Configuration of the PN-CUs as PROFINET Shared Device
- Extended PROFIsafe telegrams 31, 900 and 901 on PROFIBUS & PROFINET (e.g. for the safe transmission of actual position values and SLS limits)
- Extended telegram diagnosis incl. PROFIsafe telegrams
- Download and installation are supported without online helps; the helps can be installed later at any time by performing a new setup
- Extension of the script commands for automatic project creation (insertion of devices and objects via the command ….Add)
- SINAMICS S120/S150/G130/G150/GM150/GL150/SL150/SM120
- Operation of PM250 on CU310-2 (Cranes)
- Error filtering and assignment DO <--> component in the alarm window and alarm history incl. statement of the reference time of the operating hours counter in the alarm history
- Safety extensions (F-DI/F-DO on CU310-2, SLP )
- Comparative stages in the topology for component replacement can be preselected offline and stored
- Enhanced TIA configuring of PROFINET functions (e.g. IRT cycle 250 µs, media redundancy)
- Support for TM150 (temperature evaluation module), new module incl. screen support
The new Firmware Version V4.5 for the device series:
- SINAMICS S120/S150/G130/G150 is supported by the SSP SINAMICS V4.5 integrated in the STARTER setup.
- SINAMICS GM150/GL150/SL150/SM120 is supported by the SSP SINAMICS MV V4.5 integrated in the STARTER setup.
These SSPs are automatically installed during the STARTER setup if the selection checkbox is marked.
More detailed information regarding the drive functions included in the current SINAMICS Firmware V4.5 is provided in the delivery release for the SINAMICS S120 Firmware V4.5, see ProdIS info 59426801.
- SINAMICS G110/G120-2/G120C/G120D-2/G120P
- Supports the new PROFINET Control Units CU2xx PN
- Supports the new device series G120D-2 (incl. positioning)
- Extends the device series G120P for applications in the BT sector
- Extends the Power Module range PM2xx-2
The new Firmware Version V4.5 for the following device series:
- SINAMICS G120C, SINAMICS G120 with CU230P-2 and CU240x-2 is supported by the SSP SINAMICS G120 V4.5 integrated in the STARTER setup.
- SINAMICS G120D-2 with the CUs CU240D-2 and CU250D-2 is supported by the SSP SINAMICS G120D V4.5 integrated in the STARTER setup.
These SSPs are automatically installed during the STARTER setup if the selection checkbox is marked.
More detailed information regarding the drive functions of
- SINAMICS G120C is provided, for example, in the delivery release for SINAMICS G120C, see ProdIS info 51483985
- SINAMICS G120P with CU230P-2 is provided, for example, in the delivery release for SINAMICS G120P with CU230P-2, see ProdIS info 48405658
- SINAMICS G120 with CU240x-2 is provided, for example, in the ordering documentation for SINAMICS G120 with CU240x-2, see ProdIS info51410072
- SINAMICS G120D-2 with CU240D-2 / CU250D-2, is provided, for example, in the product announcement for SINAMICS G120D-2, see ProdIS info59057505
Information about DCC SINAMICS
A license is required for using DCC SINAMICS V2.1.
When upgrading DCC SINAMICS from the Version V2.0 SP5 (STARTER V4.1.5.5) to V2.2.1 and maintaining the CFC V7.0 SP1 HF3, you can continue to use the license for SINAMICS DCC V2.0 SP5 (CFC for SINAMCIS V7.0). To be able to use the full scope of functions of DCC V2.2.1, you must install CFC V7.1 SP2 HF2 (or later). For this, the license for DCC V2.1 (CFC for SINAMCIS V7.1) or the license for DCC V2.2.1 (CFC for SINAMCIS V8.0) is required.
If you wish to use DCC SINAMICS on a 64-bit operating system, install CFC V8.0. This CFC Version V8.0 is also stored on the STARTER DVD. If you have already obtained a license for DCC V2.1 (CFC for SINAMCIS V7.1), you can continue to use this. If you have not yet obtained this license, you must purchase a license for DCC V2.2.1 (CFC for SINAMCIS V8.0).
If you wish to purchase the licenses, order the relevant product DCC SINAMICS V2.2.1 (6AU1810-1HA22-1XA0 ) or DCC SIMOTION V2.2.1 with license. DCC SIMOTION comprises the license for DCC SIMOTION and DCC SINAMICS. Alternatively, you can also order a mere license stick DCC V2.2.1 (CFC for SINAMCIS V8.0) (6AU1810-1HA22-1XB0) for DCC SINAMICS V2.2.1 (temporarily).
During the setup for STARTER V4.3 SP1, the DCC libraries (DCB) are automatically installed and optionally also the DCC Editor (CFC V8.0). In this case, the orderable DCC DVD need not be installed separately. Only the license must always be installed separately.
Installation versions
STARTER can be operated in the following installation versions:
Sources of supply for the SINAMICS MICROMASTER STARTER
- This (the current) STARTER version can be ordered under the order number (MLFB) 6SL3072-0AA00-0AG0 on DVD incl. license ceritificate. A nominal charge of 26 € is incurred for order processing.
- This current STARTER Version (V4.3 SP1 or topical version) can also be downloaded under 26233208. All users who have already acquired any version of the STARTER license can use this version.
The SINAMICS MICROMASTER STARTER can be used free of charge.
How to install and open existing projects
Administrator rights on the PC/PG are required to install STARTER V4.3 SP1. User rights are sufficient to operate the STARTER (exception: Adding of additional PG/PC interfaces).
The STARTER V4.3 SP1 only provides one setup for both installation versions ("STARTER Standalone" and "STARTER DriveES").
- If no STEP 7 with Drive ES Basic is provided, the Standalone version is installed on your computer.
- If a STEP 7 installation with Drive ES Basic is already stored on your computer, the Drive ES version will be installed / updated.
Support
A Guided Tour can be downloaded which facilitates familiarization with the STARTER (see 21110668).
Note regarding the STARTER and other engineering software
The simultaneous operation of the versions STARTER, SIMOTION SCOUT and SIMATIC S7 technology in a shared partition on one PC/PG is not supported.
Minimum system requirements
The following minimum requirements must be complied with:
- Hardware
- PG or PC with Pentium III min. 1 GHz (recommended: >1 GHz)
- RAM 1 GB (recommended: 2 GB)
- Screen resolution 1024 × 768 pixel, 16-bit color depth
- Free hard disk memory: min. 3 GB
- Software
- Microsoft Internet Explorer V6.0 (or later)
- 32-bit operating systems:
- Microsoft Windows Server 2003 SP2
- Microsoft Windows Server 2008
- Microsoft Windows XP Professional SP2 *) and SP3
- Microsoft Windows 7 Professional incl. SP1
- Microsoft Windows 7 Ultimate incl. SP1
- Microsoft Windows 7 Enterprise incl. SP1 (Standard Installation)
- 64-bit operating systems ***):
- Microsoft Windows 7 Professional SP1
- Microsoft Windows 7 Ultimate SP1
- Microsoft Windows 7 Enterprise SP1 (Standard Installation)
- Microsoft Windows Server 2008 R2 **)
*) Limited test scope
**) Highly limited test scope, that means, you must install the software on your own risk after confirming the relevant warning
***) IMPORTANT: NO USS protocol is provided under 64-bit operating systems. Thus, with this STARTER version, you cannot operate MICROMASTER and SINAMICS G120 with Firmware Versions lower than V4.4 if they are not provided with a PROFIBUS / PROFINET interface. This limitation will be eliminated asap through a HF.
The STARTER setup can only be performed for "native" Windows versions with Far Eastern languages when using a MUI version of Windows XP or Windows 7. The executability in another software configuration than the one stated above has not been tested.
Languages supported
- German
- English
- French
- Italian
- Spanish
More detailed information regarding the compatibility of the STARTER is also provided under 26504133 For more detailed information, please contact your local Siemens office.
|  |  |