show the entry list
Industrial Security -- Product information -- System description
What should you watch out for when you enable the "SNMP" function in the configuration of the security module?
Which security modules support dynamic DNS and can use it to communicate with each other?
Why does the VPN LED of the SCALANCE M875 and MD741-1 continue to light although the secure IPsec tunnel connection is disconnected?
What should you watch out for when enabling and using the security functions of CP343-1 Advanced and CP443-1 Advanced?
How can you display the security status of the CP1628 over the Online View in the Security Configuration Tool (SCT)?
What remedies are there for weak points in WinCC flexible 2008 and WinCC V11?
Where can you find information on the topic of "Industrial Security"?
WinCC flexible RT -- Setting up systems -- Installing and upgrading software
What remedies are there for weak points in WinCC flexible 2008 and WinCC V11?
Which SQL database can you use for archiving tags and messages with WinCC flexible Runtime on an Industrial PC?
How do you install a WinCC flexible Runtime on a Microsoft Windows XP embedded operating system?
WinCC (TIA Portal) -- Setting up development environments -- Installing and upgrading software
What are the requirements for installing STEP 7 (TIA Portal) V12?
With which versions can you select the MP377 15" Touch daylight readable as operator panel?
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
What remedies are there for weak points in WinCC flexible 2008 and WinCC V11?
Which devices and modules are supported by STEP 7 Professional V11 and WinCC Professional V11?
What remedies are there for weak points in WinCC flexible 2008 and WinCC V11?
Part number:

Description
Siemens has analyzed the weak points in the web server of the Runtime system of SIMATIC WinCC flexible and WinCC (TIA Portal) and has prepared remedies.
There are remedies for the weak points available in the WinCC flexible Runtime versions 2004 to 2008 SP2, WinCC Runtime Advanced V11 and SIMATIC Panels (TP, OP, MP, Comfort Panels).

Information about the remedies and updates is available at the following links:

  • SIMATIC WinCC flexible 2008 Service Pack 3 - Information about delivery release (Entry ID: 57267466)
  • Update for WinCC V11 SP2 (Entry ID: 58112582)
  • Update for WinCC Runtime Advanced V11 SP2 (Entry ID: 58112587)

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

Additional Keywords
Security note

 Entry ID:59057488   Date:2012-03-23 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour