show the entry list
WinCC (TIA Portal) -- Working with projects -- Migrating projects
Why can you only use the functions of WinCC V11 in WinCC V12 projects for Runtime Advanced or for operator panels?
How do you do a program upload in STEP 7 (TIA Portal) V12 when the device has been configured withSTEP 7 V11?
How do you migrate a WinCC flexible 2008 SP3 project to WinCC V11 (TIA Portal) V11 SP2 in Windows 7 64-bit?
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
Which settings should be made in WinCC (TIA Portal) prior to copying an HMI screen into another HMI operator panel?
How can you transfer global libraries from WinCC flexible to WinCC (TIA Portal)?
How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)?
WinCC flexible ES -- Working with projects -- Upgrading to new version
How do you migrate a WinCC flexible 2008 SP3 project to WinCC V11 (TIA Portal) V11 SP2 in Windows 7 64-bit?
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)?
How can you transfer global libraries from WinCC flexible to WinCC (TIA Portal)?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
What are the solutions offered for working with different versions of WinCC flexible?
How do you migrate a ProTool project with SIMOTION CPU connection to a WinCC flexible project and SIMOTION SCOUT?
What connections are there between the version designations in WinCC flexible?
How do you adapt tag names to the name structure of WinCC flexible after a ProTool migration?
Which changes have to be made in WinCC flexible 2004 SP1 when changing over from TP 170micro to TP 177micro or from TP 170A to TP 177A?
Multi Panel -- Creating HMI configurations -- Upgrading to new versions
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)?
What connections are there between the version designations in WinCC flexible?
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?
Touch Panel / Operator Panel -- Creating HMI configurations -- Upgrading to new version
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)?
What connections are there between the version designations in WinCC flexible?
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?
Mobile Panels -- Creating HMI configurations -- Upgrading to new versions
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)?
How do you replace a mobile panel version 1 with a version 2 device?
What connections are there between the version designations in WinCC flexible?
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?
Basic Panels -- Creating HMI configurations -- Upgrading to new version
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
Micro Panels -- Creating HMI configurations -- Upgrading to new version
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
Part number:

Instructions
The webcast below shows you how to migrate a WinCC flexible 2008 SP2 project to WinCC V11 (TIA Portal).

The topics below are dealt with in the webcast.

  • Overview on the topic of migration
  • Requirements for migration
  • Procedure for migration
  • Additional Information

Webcast
WinCC flexible 2008 SP2 Migration to WinCC V11 (TIA Portal)

 
Contents of the download Download
Webcast:
The file has the *.mp4 format
(runtime: 9 minutes)
Webcast_Migration_WinCC_flexible_Projekt_e.zip ( 25926 KB )

Creation environment
The screens and downloads in this FAQ response were created with WinCC flexible 2008 SP2 and WinCC Advanced V11.

Download
The webcast is also available for downloading. You can run the webcast with soundtrack locally on your PC without any extra software. For this you download the relevant ZIP file to your computer, unpack the EXE file and start the file with a click. The webcast starts immediately and you can operate it using the player's menu bar.  

More Information
 
Topic

Entry-ID

Migration of a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)? 54695062
Migration from WinCC flexible 2008 SP3 to TIA Portal 59193155
Vverview of resolutions and mounting positions of the various HMI Panels and Panel PCs 56076296
Migration Guide Comfort Panels 49752044
System Manual WinCC Comfort/WinCC Advanced 53385672

Additional keywords
WinCC Basic, WinCC Comfort, WinCC Advanced, WinCC Professional, Upgrade

 Entry ID:58857225   Date:2012-03-13 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour