show the entry list

WinCC (TIA Portal) -- Setting up development environments -- Installing and upgrading software 
How do you restore the settings for registry, permissions, firewall, DCOM and user groups in STEP 7 (TIA Portal)? 
Where can you procure the current trial software for the products in the TIA Portal STEP 7 V13, WinCC V13 and Startdrive V13? 
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook? 
What are the requirements for installing STEP 7 (TIA Portal) V13? 
With which versions can you select the MP377 15" Touch daylight readable as operator panel? 
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11? 
What remedies are there for weak points in WinCC flexible 2008 and WinCC V11? 
Which devices and modules are supported by STEP 7 Professional and WinCC Professional in the TIA Portal? 

How do you restore the settings for registry, permissions, firewall, DCOM and user groups in STEP 7 (TIA Portal)?Go to beginning
Part number:

Description
When STEP 7 (TIA Portal) is being installed, the security settings in your operating system are changed, which you also have to confirm before the installation. If you make changes to your operating system after installation of STEP 7 (TIA Portal), the security settings made by the system for registry, permissions, firewall, DCOM and user groups might be changed. In STEP 7 (TIA Portal) V12 onwards you can restore these security settings with the Security Controller.

  1. Open the Security Controller using the menu command "Start > All Programs > Siemens Automation > Security Controller".

Note:
The Security Controller is a component of the setup and therefore cannot be installed separately. It makes the security settings required for STEP 7 (TIA Portal) during the setup.

  1. Confirm the message displayed about user account control with "Yes".
     
  2. In the "Security Controller" dialog you click the "Repeat Settings" button.
     
  3. The security settings below are then made, which can take a number of minutes. The progress bar indicates the course of the procedure. The bottom window shows your messages and any errors which might have occurred.
     
  4. Restore the security settings with the menu command "File > Close" and then close the Security Controller.


Fig. 01

After a successful procedure the settings are restored for the registry, permissions, firewall, DCOM and user groups.

Creation environment
The pictures in this FAQ response were created with Security Controller V2.0.

Additional Keywords
Antivirus updates, Domain updates

Where can you procure the current trial software for the products in the TIA Portal STEP 7 V13, WinCC V13 and Startdrive V13?Go to beginning
Part number:

Description
Siemens provides the software products below as trial versions for the TIA Portal V13.

  • SIMATIC STEP 7 
  • SIMATIC WinCC
  • SINAMICS Startdrive

You can download these products and test them for 21 days. Information about the products and links to the downloads are available in the entries below. Alternatively you can order the software in the form of a trial DVD.
 

SIMATIC STEP 7 V13

Link
Delivery release of SIMATIC STEP 7 Professional / Basic V13 84047138
Download of SIMATIC STEP 7 V13 TRIAL 78793685
Delivery of the trial version on DVD
  • Basic:
    Article number: 6ES7822-0AA03-0YA7
  • Professional:
    Article number: 6ES7822-1AA03-0YA7
 

 

SIMATIC WinCC V13

Link
Delivery release of SIMATIC WinCC V13 88360672
Download of SIMATIC WinCC V13 TRIAL 88360364
Delivery of the trial version on DVD
  • Basic: 
    Article number: 6AV2100-0AA03-0AA7
  • Comfort/Advanced:
    Article number: 6AV2102-0AA03-0AA7
  • Professional: 
    Article number: 6AV2103-0AA03-0AA7
 

 

SINAMICS Startdrive V13

Link
Delivery release of SINAMICS Startdrive V13 88851265
Download of SINAMICS Startdrive 68034568
Delivery on DVD:
Article number: 6SL3072-4DA02-0XG0
 

 

Further Information

Link
TIA Portal - An Overview of the Most Important Documents and Links 65601780
General information about the TIA Portal www.siemens.com/tia-portal

Additional Keywords
Trail software, License, Test software

What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?Go to beginning
Part number:

Description
With the installation of Service Pack 3 for WinCC flexible 2008 on HP notebooks there are incompatibilities with the HP keyboard driver. If you uninstall the keyboard driver, this might mean that a block of the task switching function configured in WinCC flexible 2008 no longer works on the notebook.

The following products are affected:

  • SIMATIC WinCC flexible 2008 SP3 Compact/Standard/Advanced
  • SIMATIC WinCC flexible 2008 SP3 Runtime

Products not affected:
The error is cleared in WinCC Comfort/Advanced/Professional and WinCC Runtime Advanced in version V11 SP2 SE incl. Update 2 onwards.

Remedy
There are two alternatives for avoiding this incompatibility. Either you uninstall the HP keyboard driver or you uninstall the keyboard driver that is installed along with WinCC flexible Runtime or the simulation.
Both alternatives must be executed at the latest before the concluding restart of the PC after installation of WinCC flexible 2008 SP3.

If the restart after installation has already been made and the system no longer starts or you have a blue screen, follow the instructions given under "Run_Windows_Repair".

The alternatives are described below each with their advantages and disadvantages.

  1. Uninstallation of the HP keyboard driver
  2. Uninstallation of the keyboard driver of WinCC flexible Runtime

1. Uninstallation of the HP keyboard driver
With this alternative the task switching function is retained for WinCC flexible Runtime. Uninstallation of the driver might limit use of the HP special keys. To continue with this alternative you must uninstall the HP keyboard driver as follows before installing WinCC flexible 2008 SP3.
 
No. Procedure
1 Open the Windows Device Manager.


Fig. 01

2 Navigate to: Keyboards, "Standard ... Keyboard with HP QLB " and right-click to open the Properties.


Fig. 02

3 Open the "Driver" tab and select Roll Back Driver for the HP keyboard driver.


Fig. 03

4 Confirm the dialogs that open with "Yes" and "OK".
The result is that the standard Microsoft keyboard driver is used.


Fig. 04

5 Quit the Device Manager and restart the PC.
Table 01

2. Uninstallation of the keyboard driver of WinCC flexible Runtime
This alternative retains the HP special key functions. Uninstallation of the driver disables the task switching function for WinCC flexible Runtime. To continue with this alternative you must uninstall the keyboard driver for WinCC flexible Runtime as follows before restarting the PC after installation of WinCC flexible 2008 SP3.
 
No. Procedure
1 Open the input prompt (CMD) with administrator rights.


Fig. 05


Fig. 06

2 Open the driver directory. The directory path for the driver directory depends on the installed operating system.

Driver directory on 32-bit operating systems:
"C:\Program Files\Common Files\Siemens\HmiRTmDriver32"

Driver directory on 64-bit operating systems:
"C:\Program Files\Common Files\Siemens\HmiRTmDriver64"


Fig. 07

3 Remove the driver with the following command:

For the WinCC flexible Runtime:
"FwKbdRTmRegister.exe -r fwkbdrtm -d fwkbdrtm.sys"


Fig. 08

4 Quit the Command Prompt and restart the PC.
Table 02

Run Windows Repair
If WinCC flexible 2008 SP3 is already installed and the ensuing restart already made, the system might no longer start or you get a blue screen.
Below is the procedure for this case.

Note
You need an additional USB keyboard for the steps below.
 
No. Procedure
1 Run a "Startup Repair" (displayed after boot problems) or start the HP notebook from the Windows DVD.
2 Select the "Launch Startup Repair" option after the "Startup Repair" or after the start from the Windows DVD.
3 Interrupt the "Startup Repair is checking your system for problems" message with "Cancel" (abort search).
4 Acknowledge the "Do you really want to abort?" question with "Yes".
5 Select the "View advanced options for system recovery and support" option.
6 Select the USB keyboard and log on.
7 Open the input prompt (CMD).
8 Switch to the driver directory ("C:\Windows\system32\drivers", for example).
9 Rename the HP driver: "ren hpqkbfiltr.sys hpqkbfiltr.sys_".
10 Quit the input prompt (CMD) and restart the PC.
11 Use the USB keyboard or USB mouse to continue with Alternative 1 or 2.
Table 03

What are the requirements for installing STEP 7 (TIA Portal) V13?Go to beginning
Part number:

Description
The latest version of STEP 7 (TIA Portal) V13 is available from your Sales partner. You should observe the points below before installing STEP 7 (TIA Portal) V13.

  1. Hardware requirements
  2. Software requirements
  3. Administrator rights
  4. Parallel installation of STEP 7 (TIA Portal) V13 and other versions of STEP 7
  5. Compatibility with other SIMATIC HMI products
  6. Compatibility with projects from STEP 7 V5.4 and V5.5
  7. Uninstallation of STEP 7 V13
  8. Repair of the STEP 7 V13 software
  9. Uninstallation of WinCC (TIA Portal) Professional
  10. Order of installation of SIMATIC products for the TIA Portal
  11. Compatibility with other products

The table below gives an overview of the general requirements for installing STEP 7 Basic / Professional V13.
 
No. Requirements for installing STEP 7 Basic / Professional V13
1 Hardware requirements
Your PC must meet the following minimum requirements for installing STEP 7 Basic / Professional V13:
  • Processor: CoreTM i5-3320M 3.3 GHz  or comparable
  • Main memory: 8 GB or more
  • Hard disk: 300 GB SSD
  • Graphics: Min. 1920 x 1080
  • Screen: 15.6" Wide Screen Display (1920 x 1080)
2 Software requirements
STEP 7 Professional / Basic V13 is released for the following operating systems (64-bit, also 32-bit for Windows 7):
  • MS Windows 7 Home Premium SP1 (only for STEP 7 Basic)
  • MS Windows 7 Professional SP1
  • MS Windows 7 Enterprise SP1
  • MS Windows 7 Ultimate SP1
  • Microsoft Windows 8.1 (STEP 7 Basic only)
  • Microsoft Windows 8.1 Pro
  • Microsoft Windows 8.1 Enterprise
  • Microsoft Server 2012 R2 Standard Edition
  • MS Windows 2008 Server R2 Standard Edition SP2 (only for STEP 7 Professional)
3 Administrator rights
You need administrator rights for your PC to install STEP 7 (TIA Portal) V13.
4 Parallel installation of STEP 7 (TIA Portal) V13 and other versions of STEP 7
You can also install other versions of STEP 7 on your computer in parallel to STEP 7 (TIA Portal) V13:
  • STEP 7 (TIA Portal) V11, V12
  • STEP 7 V5.4 SP5 or V5.5
  • STEP 7 Professional 2010 SR2
  • STEP 7 Micro/WIN V4.0 SP9

Note
Parallel online operation of STEP 7 V5.5 or older versions and STEP 7 Basic / Professional V13 is not enabled.

5 Compatibility with other SIMATIC HMI products
You can install the following SIMATIC HMI products on your hard disk in parallel to STEP 7 (TIA Portal) V13:
  • WinCC flexible (from 2008 SP2, SP3) and
  • WinCC (V7.0 SP2, SP3 and V7.2)

WinCC and WinCC TIA cannot be installed simultaneously on one and the same computer. WinCC flexible and WinCC TIA can be installed simultaneously on one and the same computer.

Note on WinCC and WinCC flexible

  • You can install WinCC flexible and WinCC (TIA Portal) simultaneously on one and the same computer.
  • You cannot install WinCC and WinCC (TIA Portal) simultaneously on one and the same computer.
6 Compatibility with projects from STEP 7 V5.4 and V5.5
Using the "Project > Migrate Project..." function in STEP 7 V13 you can migrate projects created with STEP 7 V5.5 and STEP 7 Professional 2010 to STEP 7 V13. The STEP 7 projects that contain a configuration with WinCC or WinCC flexible can also be migrated to the TIA Portal V13 with the included WinCC flexible parts. Included configurations created with WinCC V7.0+SP2 or lower are currently not migrated as well. The components below must be installed on your computer for this:  
  • STEP 7 V5.4+SP5 or STEP 7 V5.5
  • WinCC V7.0+SP2 and higher or WinCC flexible 2008+SP2

Note
You cannot migrate WinCC V7.0+SP1 or lower.

7 Uninstallation of STEP 7 V13
You have two options for uninstalling STEP 7 Basic / Professional V13:

1. Uninstallation via the Control Panel (in Windows 7)

  1. In the Control Panel you click "Programs" and then select "Programs and Functions".
  2. In the "Change/Remove Programs" dialog you double-click the "Siemens Totally Integrated Automation Portal V13" application and then "Yes" in the message that opens.
  3. Follow the instructions on the screen.

2. Uninstallation using the SIMATIC STEP 7 V13 CD

  1. Insert the STEP 7 V13 CD in your computer's CD drive.
  2. If the Setup program does not start automatically, open the "Start.exe" file.
  3. Select the language in which you want the dialogs displayed.
  4. Select the "Uninstall" option field and click the "Next >" button.
  5. Follow the instructions on the screen.
8 Repairing the STEP 7 V13 software
If the installation of STEP 7 Basic / Professional V13 is defective or damaged by an event, you have the option of repairing the STEP 7 V13 software.
  1. Insert the STEP 7 V13 CD in your computer's CD drive.
  2. If the Setup program does not start automatically, open the "Start.exe" file.
  3. Select the language in which you want the dialogs displayed.
  4. Select the "Repair" option field and click the "Next >" button.
  5. Follow the instructions on the screen.
9 Uninstallation of WinCC (TIA Portal) Professional
If installation of STEP 7 (TIA Portal) V13 aborts and you receive the message that you must uninstall an earlier version of WinCC Professional beforehand even though you have already done the uninstallation, this might be due to a Registry code. Proceed as follows to remove the Registry entry in Windows 7, for example:
  1. In Windows 7 you open the Registry by going to "Search programs and files" and entering "Regedit". Confirm with Enter.
  2. Open the path:

In Windows 7 (32-bit):
HKEY_LOCAL_MACHINE\SOFTWARE\Siemens\Automation\_InstalledSW\
TIAP11\TIA_ES_V11\PrivateProperties\INST_TYPE_LEVEL_INTERNAL

In Windows 7 (64-bit)
HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Siemens\
Automation\_InstalledSW\TIAP11\TIA_ES_V11\PrivateProperties\
INST_TYPE_LEVEL_INTERNAL

  1. Remove the entry "4_0_Professional".
  2. Do a restart and then you can install STEP 7 (TIA Portal) V13.


Fig. 01

10 Order of installation of SIMATIC products for the TIA Portal
First install STEP 7 (TIA Portal), because the HMI products integrate in STEP 7. Then the HMI products followed by the optional software packages (STARTER, SINAMICS Startdrive, for example). Below is an example for the order of installation:
  1. SIMATIC STEP 7 Professional V13
  2. SIMATIC WinCC Professional V13
  3. SINAMICS Startdrive V13
  4. STEP 7 Safety Advanced V13

More information about compatibility is available in Entry ID: 64847781.

11 Compatibility with other products
Refer to the information in the STEP 7 (TIA Portal) Readme under "General Information" - "Information on Operation".

Note on Deltalogic
If you have the Deltalogic software installed on your computer, faults might occur during the online connection. In this case, check whether the "s7oiehsx64" service (SIMATIC IEPG Help Service) is being executed in the Task Manager.
Remedy
In the Task Manager and in the "Services" register you right-click the "s7oiehsx64" service to open the pop-up menu. Close and restart the services.

Note on the Matrox PowerDesk
If you have installed the Matrox PowerDesk desktop management software on your computer, there might be failures with the TIA Portal start screen.
Remedy
To prevent this behavior from reoccurring, disable the additional screen output.

Important
This entry contains information for editing the Registry. You should make a backup copy of the Registry before editing it. More information about making a backup copy, restoring and editing the registry is available in the Microsoft Knowledge Base in Entry ID 256986. Incorrect use of the Registry editor can cause serious problems that affect the complete system and make it necessary to reinstall the operating system. You use the Registry editor at your own risk.

Discuss this FAQ
Do you have another solution or a different application?
Is this solution not the right one for you? 

Discuss this FAQ here.

With which versions can you select the MP377 15" Touch daylight readable as operator panel?Go to beginning
Part number:

Description
The MP 377 15" Touch daylight readable is already integrated in the HMI software WinCC flexible 2008 SP3 and WinCC V12 and can be selected in the hardware catalog; it is not necessary to install a supplied AddOn here nor are the procedures described under "Install ProSave Options" necessary.

Requirements
If you are using WinCC flexible 2008 SP1 HF2 or WinCC flexible 2008 SP2, you must install the WinCC flexible AddOn in order to be able to select the MP377 15" Touch daylight readable as operator panel in WinCC flexible and ProSave. By installing the AddOn you can also configure the "Set Brightness" function.
 
WinCC flexible AddOn "Set Brightness" Availability of AddOn
WinCC flexible 2008 SP1 HF1 V01.00.01.01_01.05 Operator panel delivery package
WinCC flexible 2008 SP1 HF2 V01.00.01.02_01.02 MP377_Daylight_SW_AddOn_SP1_HF2.zip ( 11403 KB )
 
WinCC flexible 2008 SP2 V01.00.02.01_01.08 MP377_Daylight_SW_AddOn_SP2.zip ( 23840 KB )
 
WinCC flexible 2008 SP3 Already integrated Installation of AddOn not necessary
WinCC V12 Already integrated Installation of AddOn not necessary
Table 01

Entry ID 28531852 contains possible solutions for working with different versions of WinCC flexible on one system.

Installation
 
No. Procedure
1 Depending on the version of WinCC flexible, insert the AddOn CD from the operator panel delivery package in the CD/DVD drive of your PC or download the AddOn and unpack it on your hard disk.
2 Start the installation by double-clicking on the "MP377 Daylight*.msi" file or "Setup.exe".
  • Version V01.00.01.01_01.05 is located in the "WCF_Addon" folder.
  • Version V01.00.01.02_01.02 is located in the "WCF2008SP1HF2\WCF_Addon" folder.
  • Version V01.00.02.01_01.08 is located in the "WCF2008SP2\WCF_Addon" folder.
3 Now follow the instructions of the installation wizard until the installation is completed.
4 Now you can select and configure the Multi Panel 377 15" Touch daylight readable as operator panel in WinCC flexible and ProSave.
Table 02

Configuring the AddOn
More information on configuring the AddOn "Set Brightness" is available in the manual of the MP377 15" Touch daylight readable in Entry ID: 37954241 in the section "Appendix > The Addon 'Set Brightness' > Configure".

Installing ProSave options
Proceed as described below to be able to use options with ProSave on the MP 377 15"Touch Daylight.
 
No. Procedure
1 Close ProSave.
2 Insert the AddOn CD from the operator panel delivery package in the CD/DVD drive of your PC.
3 Start the "ModifyPii.bat" file from the "Tools" folder with a double-click.
4 Open ProSave.
5 Under "Device Type" select the MP 377 15" Touch Daylight.
6 In the "Options" tab select the option that you want to install and transfer it to the operator panel.
Table 03

Note
The MP 377 15" Touch daylight readable is already integrated in the HMI software WinCC flexible 2008 SP3 and WinCC V12 and the procedure described under "Installing ProSave options" is not necessary here.

Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?Go to beginning
Part number:

Description
If you have WinCC flexible or WinCC V7.0 RT installed on your computer, you need either the license for the upgrade (or for the PowerPack).
The table below explains the options available for license upgrading.

If you still do not have a version of WinCC flexible or WinCC V7.0 RT installed on your computer, you need the full license for WinCC V11 Engineering, WinCC Runtime Advanced V11 or WinCC Runtime Professional V11.

WinCC flexible 2008 (ES and RT) to WinCC V11
(WinCC flexible 2008 Advanced to WinCC V11 Advanced, for example)

  Upgrade_WinCCflexible_to_WinCC_V11_e.pdf ( 14 KB )

Note

  • If you upgrade WinCC flexible 2008 to WinCC V11 with a upgrade license you get a combo license. This combo license is valid for WinCC flexible 2008 and WinCC V11.
    With a full license for WinCC V11 you can only operate with WinCC V11.
  • Versions older than WinCC flexible 2008 should be upgraded to WinCC flexible 2008.

WinCC V7 Runtime to WinCC Runtime Professional V11
(WinCC V7.0 Runtime 8k PowerTags to WinCC V11 Professional Runtime 8k PowerTags, for example)

  Upgrade_WinCC_V7_RT_to_WinCC_V11_RT_e.pdf ( 13 KB )

Note
It is not possible to upgrade from WinCC V7 RC  to V11.

Upgrading in WinCC V11
(WinCC V11 Advanced to WinCC V11 Professional, for example)

  Powerpacks_WinCC_V11_ES_RT_e.pdf ( 15 KB )

Additional information about upgrading STEP 7
Information about upgrading STEP 7 is available in Entry ID 57775228.

TIA Portal Readiness Check Tool
The TIA Portal Readiness Check Tool delivers an easy way of checking whether the TIA Portal supports the hardware in the project.
Information about this is available in Entry ID 60162195.

Additional Keywords
Order number, MLFB, TIA Portal, Migration, Update, Upgrade, Successor, Replacement, Change, License Key, Authorization, License key

What remedies are there for weak points in WinCC flexible 2008 and WinCC V11?Go to beginning
Part number:

Description
Siemens has analyzed the weak points in the web server of the Runtime system of SIMATIC WinCC flexible and WinCC (TIA Portal) and has prepared remedies.
There are remedies for the weak points available in the WinCC flexible Runtime versions 2004 to 2008 SP2, WinCC Runtime Advanced V11 and SIMATIC Panels (TP, OP, MP, Comfort Panels).

Information about the remedies and updates is available at the following links:

  • SIMATIC WinCC flexible 2008 Service Pack 3 - Information about delivery release (Entry ID: 57267466)
  • Update for WinCC V11 SP2 (Entry ID: 58112582)
  • Update for WinCC Runtime Advanced V11 SP2 (Entry ID: 58112587)

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

Additional Keywords
Security note

Which devices and modules are supported by STEP 7 Professional and WinCC Professional in the TIA Portal?Go to beginning
Part number:

Description
The list attached contains modules that are supported by a joint installation of STEP 7 Professional V11 and WinCC Professional V11.

STEP7_V11_Support_HW_List.pdf ( 91 KB )   

Additional Keywords
Hardware update

 Entry ID:58064754   Date:2014-07-02