show the entry list
Micromaster 4 -- Commissioning and operation -- Control via Terminal Blocks
MICROMASTER 4: Can I also use pushbuttons (without relay interconnection) to control my MICROMASTER?
MICROMASTER 4: Is it possible to switch-on the inverter via digital inputs and ON/OFF1 and switch-off the inverter via digital inputs and OFF2?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Can an analogue output be used as a digital output?
How can I suppress noise on measuring signals at the analog outputs of a drive inverter so that I can carry-out measurements using an oscilloscope?
MICROMASTER 4 (MM4): What parameters do I have to set on an MM440 to give the same binary fixed frequency selection functionality as 6SE32?
MICROMASTER 4 (MM4), SINAMICS G120: What is the difference between the control terminals for MM4 and SINAMICS G120?
Are the binary input command functions RUN right and RUN left the same on the MM4/SINAMICS G120 as on previous MICROMASTER products?
MICROMASTER 4 (MM4): How do I switch between two analogue inputs on MM440?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How can I parameterize a changeover between main and additional setpoint?
MICROMASTER 4 (MM4): How can I implement a center zero setpoint operation with the motor potentiometer?
MICROMASTER 420 (MM4): Is 3-wire control possible on the MM420?
MICROMASTER 420 (MM4): How do I set up the analogue input of the MM420 as a 4-20mA current loop?
MICROMASTER 4 (MM4), SINAMICS G120/G120D (CU2x0x): How can I switch between different ramp times?
MICROMASTER 420 (MM4): Is 3-wire control possible on the MM420?
Part number:

Applies to: MM420

Yes. This is possible using BiCo technology as follows:

The following example shows 3-wire control with an analogue setpoint, where DIN1 receives the RUN impulse (0 V ® 24 V) and DIN3 receives the STOP impulse (24 V ® 0 V).

Diagram:

Parameter settings:

P0003 = 3 allows access to level 3 parameters

P0700 = 2 (command source: terminals / BiCo)

P0701 = 99 (BiCo)
P0702 = 99 (BiCo)
P0703 = 99 (BiCo)
- this disconnects all previous connections and allows use of BiCo command connections.

P0848 = 722.2 (this configures OFF3 to DIN3)
P1135 = xxxx s (required (OFF3) ramp down time (usually set to same value as P1121))

P1000 = 23 (main setpoint fixed frequency; additional setpoint analogue: see Note 1)

P1001 = 0.0 Hz (fixed frequency 1 = 0.0 Hz)
P1002 = 0.0 Hz (fixed frequency 2 = 0.0 Hz)

P1016 = 2 (fixed frequency with RUN command)
P1017 = 2 (fixed frequency with RUN command)

P1020 = 722.0 (DIN1 - source of fixed frequency 1)
P1021 = 52.2 (inverter running - source of fixed frequency 2)

With the above settings, the pulse on DIN1 causes the inverter to RUN with FF1 (0.0 Hz) + analogue setpoint. Once the inverter has started this sets status bit 52.2 (inverter running), which then selects RUN with FF2 (0.0 Hz) + analogue setpoint. Therefore the inverter will continue to run after the signal has been removed from DIN1. To stop the inverter, a low pulse must be set on DIN3 which causes an OFF3 and the inverter will stop using the OFF3 ramp down time.

Notes

1. On the MM420 it is not usually possible to have two separate RUN commands acting simultaneously. The fixed frequency mechanism, however, allows this. In this case the mechanism is used so that DIN1 selects RUN + FF1 and 52.2 selects RUN + FF2. To enable the RUN commands by this method, fixed frequencies must be a setpoint source. However by setting each fixed frequency to 0Hz and using the analogue setpoint as an additional setpoint (P1000 = 23), the fixed frequencies themselves have no influence on the total setpoint.

2. In the above example, 52.2 is used to give the second RUN command. This leads to the restriction that the inverter cannot be restarted after an OFF3 until Bit 52.2 is no longer high, i.e. the inverter has stopped. Depending on the user application it might be possible to use a different second RUN source to optimise the command sequence (e.g. 53.2 inverter freq > Fmin).

 

 Entry ID:5800810   Date:2000-11-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour