show the entry list
STEP 7 (TIA Portal) -- Setting up development environments -- Installing / transferring licenses
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
Why is the license not recognized when opening STEP 7?
STEP 7 (TIA Portal) -- Working with projects -- Migrate projects
PLC migration to S7-1500 with STEP 7 (TIA Portal) V12
What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
Where are the standard blocks and instructions stored in STEP 7 V11 (TIA Portal) and in V5.5 (SIMATIC Manager)?
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
What are the differences in the keyboard operation of STEP 7 Basic V10.5, V11 and STEP 7 V5.5?
Which devices and modules are supported by STEP 7 Professional V11 and WinCC Professional V11?
What are the requirements for installing STEP 7 (TIA Portal) V12?
What are the prerequisites for migrating STEP 7 V5.x projects to STEP 7 (TIA Portal) V11?
STEP 7 (TIA Portal) -- Setting up development environments -- Installing and upgrading software
How do you perform the firmware update V3.0 for the S7-1200 in STEP 7 (TIA Portal) by means of the web server?
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
Which SIMATIC software can you install in 64-bit operating systems?
How can you install STEP 7 V11 in Windows XP with Turkish installed as Regional and Language option?
Why do you get a prompt to restart MS Windows after installing STEP 7 V11, although the PC has already been booted?
How do you update the hardware catalog in STEP 7 (TIA Portal)?
What are the requirements for installing STEP 7 (TIA Portal) V12?
Which devices and modules are supported by STEP 7 Professional V11 and WinCC Professional V11?
WinCC (TIA Portal) -- Product information -- Determining performance and quantity frameworks
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
Which external storage locations are available on the various operator panels (TIA Portal/WinCC flexible/ProTool) for archiving data?
What are the functional differences between the different SIMATIC panels?
STEP 7 -- Setting up development environments -- Installing and upgrading software
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
Which SIMATIC software can you install in 64-bit operating systems?
Why can't STEP 7 be installed because of NCM?
Information on the topic of "Installing and upgrading software"
How do you uninstall STEP 7 completely, including all the software packages?
Tips and tricks for installing and upgrading software in STEP 7
How can you update the hardware catalog without direct internet access?
How do you update the STEP 7 hardware catalog in STEP 7 V5.2 onwards?
How can you work with two different versions of STEP 7 on one computer?
Which settings and procedures are to be observed with regard to InstallShield when installing STEP 7?
How in Windows XP/Vista/7 can you disable the message "Please reboot before installing any more programs"?
Why can the current software upgrade not be installed?
What are the requirements for installing STEP 7 version V5.5?
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
Part number:

Description
If you still do not have a version of STEP 7 installed on your computer, you need the full license for STEP 7 Basic V12 or for STEP 7 Professional V12. If you have a version of STEP 7 installed on your PC, you need either the license for the upgrade or for the PowerPack. The table below shows the different licenses needed for a new installation or for updating your version of STEP 7.
 
Case Procedure
1 No version of STEP 7 installed on your computer.
  • For STEP 7 Basic V12 you need the floating license with order number: 6ES7822-0AA02-0YA5
  • and for STEP 7 Professional V12 you need the floating license with order number: 6ES7822-1AA02-0YA5.

You can also install the trial license for each product:

  • Order number 6ES7822-0AA02-0YA7 for STEP 7 Basic V12.
  • Order number 6ES7822-1AA02-0YA7 for STEP 7 Professional V12.

Note
As registered customer you can download the trial for SIMATIC STEP 7 Professional V12 and test it for 21 days. The Professional edition also includes the functions from SIMATIC STEP 7 Basic V12. More information is available in Entry ID: 67639464.

2 You have STEP 7 Professional 2006 or 2010 installed on your computer and you want to upgrade to STEP 7 Professional V12.
  • Here you need the upgrade with the COMBO floating license (order number: 6ES7822-1AA02-0XE5).
3 You have STEP 7 Basic V10.5 installed on your computer and you want to upgrade to STEP 7 Basic V11.
  • Here you need the upgrade with the single license (order number: 6ES7822-0AA01-0YE0).
4 You have STEP 7 Basic V11 installed on your computer and you want to upgrade to STEP 7 Basic V12.
  • Here you need the floating upgrade package license (order number: 6ES7822-0AA02-0YE5).

Note
Valid for STEP 7 V11 Single and for STEP 7 V11 Floating.

5 You have STEP 7 Professional V11 installed on your computer and you want to upgrade to STEP 7 Professional V12.
  • Here you need the upgrade with the floating license (order number: 6ES7822-1AA02-0YE5).

Note
It is not possible to use this upgrade to upgrade from STEP 7 Professional 2010.

6 You have STEP 7 V5.4 or V5.5 installed on your computer and you want to upgrade to STEP 7 Professional V12.
  • Here you need the PowerPack & Upgrade with the floating license (order number: 6ES7822-1AA02-0XC5).
7 You have STEP 7 Basic V12 installed on your computer and you want to change to STEP 7 Professional V12.
  • Here you need the PowerPack with the floating license (order number: 6ES7822-1AA02-0YC5).
8 You have the STEP 7 Professional 2006/2010 Upgrade installed on your computer and you want to upgrade to STEP 7 Professional 2010/V11.
  • Here you need the Combo Floating License (order number: 6ES7822-1AA11-0XE5) for the SIMATIC STEP 7 PROF. 2010/V11 UPGRADE

Note
The requirement here is that an SUS (Software Update Service) is available.

9 You have STEP 7 Professional 2010/V11 installed on your computer and you want to upgrade to STEP 7 Professional 2010/V12.
  • Here you need the Combo Floating License (order number: 6ES7822-1AA02-0YE5) for SIMATIC STEP 7 PROFESSIONAL V12 ENGINEERING SOFTWARE.
Table 01

The floating licenses are also available here for downloading. Entry 67851956 contains the list with the order numbers at the link "STEP_7_V12_Orderlist". The order numbers are linked with the associated downloads.

The table below shows the features of the different license keys that you can order and install.
 
License Key Meaning
Single License Unlimited use on any one computer.
Floating License Unlimited use on any one computer or through the network.
Rental License Limited use as stipulated in the rental contract.
Trial License Limited use (max. 21 days) for tests and for validating (with disclaimer).
Upgrade License An Upgrade License converts a license for an earlier version x to a license for version >x+... .
Table 02

You can also install STEP 7 V5.4/V5.5, STEP 7 Basic V10.5, WinCC flexible 2008 onwards and WinCC V7.0 SP2 onwards in parallel to STEP 7 V12.

  • With an Upgrade License / Combo License for STEP 7 V12 (TIA Portal) you can operate both STEP 7 V5.4/V5.5 or STEP 7 Professional 2006/2010 and STEP 7 Professional V12.
  • With an Full License for STEP 7 V12 (TIA Portal) you cannot operate STEP 7 V5.4/V5.5 or STEP 7 Professional 2006/2010.

Follow the instructions in the table below to upgrade a License Key.
 
No. Procedure
1 Open the Automation License Manager and select "View > Administration".
2 Transfer the Upgrade License Key to the hard disk on which you want to carry out the upgrade.
3 Also transfer the License Key of the previous version to the hard disk if the license is not yet located on your computer.
4 Select the storage location in the navigation area where the license key to be upgraded is located (previous version).
5 In the Object area you select the license key that is to be upgraded.
6 Execute the menu command "License Key > Upgrade...". The upgrade is now made.


Fig. 01

Table 03

Note
More information about licenses and the differences between the authorizations and licenses is available in Entry ID: 19020864

Creation environment
The screen in this FAQ was created with ALM V5.1+Upd 1.

 Entry ID:57775228   Date:2013-05-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour