|
Description If you still do not have a version of STEP 7 installed on your computer, you need the full license for STEP 7 Basic V12 or for STEP 7 Professional V12. If you have a version of STEP 7 installed on your PC, you need either the license for the upgrade or for the PowerPack. The table below shows the different licenses needed for a new installation or for updating your version of STEP 7.
| Case |
Procedure |
| 1 |
No version of STEP 7 installed on your computer.
- For STEP 7 Basic V12 you need the floating license with order number: 6ES7822-0AA02-0YA5
- and for STEP 7 Professional V12 you need the floating license with order number: 6ES7822-1AA02-0YA5.
You can also install the trial license for each product:
- Order number 6ES7822-0AA02-0YA7 for STEP 7 Basic V12.
- Order number 6ES7822-1AA02-0YA7 for STEP 7 Professional V12.
Note
As registered customer you can download the trial for SIMATIC STEP 7 Professional V12 and test it for 21 days. The Professional edition also includes the functions from SIMATIC STEP 7 Basic V12. More information is available in Entry ID: 67639464. |
| 2 |
You have STEP 7 Professional 2006 or 2010 installed on your computer and you want to upgrade to STEP 7 Professional V12.
- Here you need the upgrade with the COMBO floating license (order number: 6ES7822-1AA02-0XE5).
|
| 3 |
You have STEP 7 Basic V10.5 installed on your computer and you want to upgrade to STEP 7 Basic V11.
- Here you need the upgrade with the single license (order number: 6ES7822-0AA01-0YE0).
|
| 4 |
You have STEP 7 Basic V11 installed on your computer and you want to upgrade to STEP 7 Basic V12.
- Here you need the floating upgrade package license (order number: 6ES7822-0AA02-0YE5).
Note
Valid for STEP 7 V11 Single and for STEP 7 V11 Floating. |
| 5 |
You have STEP 7 Professional V11 installed on your computer and you want to upgrade to STEP 7 Professional V12.
- Here you need the upgrade with the floating license (order number: 6ES7822-1AA02-0YE5).
Note
It is not possible to use this upgrade to upgrade from STEP 7 Professional 2010. |
| 6 |
You have STEP 7 V5.4 or V5.5 installed on your computer and you want to upgrade to STEP 7 Professional V12.
- Here you need the PowerPack & Upgrade with the floating license (order number: 6ES7822-1AA02-0XC5).
|
| 7 |
You have STEP 7 Basic V12 installed on your computer and you want to change to STEP 7 Professional V12.
- Here you need the PowerPack with the floating license (order number: 6ES7822-1AA02-0YC5).
|
| 8 |
You have the STEP 7 Professional 2006/2010 Upgrade installed on your computer and you want to upgrade to STEP 7 Professional 2010/V11.
- Here you need the Combo Floating License (order number: 6ES7822-1AA11-0XE5) for the SIMATIC STEP 7 PROF. 2010/V11 UPGRADE
Note
The requirement here is that an SUS (Software Update Service) is available. |
| 9 |
You have STEP 7 Professional 2010/V11 installed on your computer and you want to upgrade to STEP 7 Professional 2010/V12.
- Here you need the Combo Floating License (order number: 6ES7822-1AA02-0YE5) for SIMATIC STEP 7 PROFESSIONAL V12 ENGINEERING SOFTWARE.
|
Table 01
The floating licenses are also available here for downloading. Entry 67851956 contains the list with the order numbers at the link "STEP_7_V12_Orderlist". The order numbers are linked with the associated downloads.
The table below shows the features of the different license keys that you can order and install.
| License Key |
Meaning |
| Single License |
Unlimited use on any one computer. |
| Floating License |
Unlimited use on any one computer or through the network. |
| Rental License |
Limited use as stipulated in the rental contract. |
| Trial License |
Limited use (max. 21 days) for tests and for validating (with disclaimer). |
| Upgrade License |
An Upgrade License converts a license for an earlier version x to a license for version >x+... . |
Table 02
You can also install STEP 7 V5.4/V5.5, STEP 7 Basic V10.5, WinCC flexible 2008 onwards and WinCC V7.0 SP2 onwards in parallel to STEP 7 V12.
- With an Upgrade License / Combo License for STEP 7 V12 (TIA Portal) you can operate both STEP 7 V5.4/V5.5 or STEP 7 Professional 2006/2010 and STEP 7 Professional V12.
- With an Full License for STEP 7 V12 (TIA Portal) you cannot operate STEP 7 V5.4/V5.5 or STEP 7 Professional 2006/2010.
Follow the instructions in the table below to upgrade a License Key.
| No. |
Procedure |
| 1 |
Open the Automation License Manager and select "View > Administration". |
| 2 |
Transfer the Upgrade License Key to the hard disk on which you want to carry out the upgrade. |
| 3 |
Also transfer the License Key of the previous version to the hard disk if the license is not yet located on your computer. |
| 4 |
Select the storage location in the navigation area where the license key to be upgraded is located (previous version). |
| 5 |
In the Object area you select the license key that is to be upgraded. |
| 6 |
Execute the menu command "License Key > Upgrade...". The upgrade is now made.

Fig. 01
|
Table 03
Note
More information about licenses and the differences between the authorizations and licenses is available in Entry ID: 19020864
Creation environment
The screen in this FAQ was created with ALM V5.1+Upd 1.
|