show the entry list
WinCC (TIA Portal) -- Working with projects -- Migrating projects
Why can you only use the functions of WinCC V11 in WinCC V12 projects for Runtime Advanced or for operator panels?
How do you do a program upload in STEP 7 (TIA Portal) V12 when the device has been configured withSTEP 7 V11?
How do you migrate a WinCC flexible 2008 SP3 project to WinCC V11 (TIA Portal) V11 SP2 in Windows 7 64-bit?
How do you migrate a WinCC flexible 2008 project to WinCC V11 (TIA Portal)?
Which settings should be made in WinCC (TIA Portal) prior to copying an HMI screen into another HMI operator panel?
How can you transfer global libraries from WinCC flexible to WinCC (TIA Portal)?
How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)?
Which settings should be made in WinCC (TIA Portal) prior to copying an HMI screen into another HMI operator panel?
Part number:

Task
You have configured an MP 277 Touch with multiple screens. A TP1200 Comfort Panel is to be added to this configuration.
The screens of the MP 277 Touch are to be adopted by the new operator panel.

WinCC (TIA Portal) provides the option of using "Drag & Drop" or "Copy & Paste" to transfer screens from one operator panel into another.

Prior to copying you should check the settings for resizing screens and objects. This resizing is important in particular when the operator panels have different display resolutions.
In this example, the MP 277 Touch has a resolution of 640 x 480 and the TP1200 Comfort a resolution of 1280 x 800.

In advance you can define how the contents of the project screens are tp be resized and applied upon transfer.
For this, in WinCC (TIA Portal), you select the menu command "Options > Settings".
Under the "Visualization > Resize screen" item you can define various options (see figure below).


Fig. 01

A detailed description of the effect of the different settings on the operator panel is given in the document "Migration guidelines for Comfort Panels", section 3.3 (Change Screen from 4:3 to Wide Screen).

Additional information
 
Title

Link

Overview of resolutions and different screen formats of the panels Entry ID: 56076296
SIMATIC HMI Operator Panels Migration Guide for Comfort Panels Entry ID: 49752044
System Manual for WinCC Comfort / WinCC Advanced V11.0 SP1 Entry ID: 53385672

Keywords
Transfer screens, Migration, Migrate

 Entry ID:57439921   Date:2012-01-30 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour