show the entry list

Industrial Security -- Product information -- System description 
What should you watch out for when you enable the "SNMP" function in the configuration of the security module? 
Which security modules support dynamic DNS and can use it to communicate with each other? 
Why does the VPN LED of the SCALANCE M875 and MD741-1 continue to light although the secure IPsec tunnel connection is disconnected? 
What should you watch out for when enabling and using the security functions of CP343-1 Advanced and CP443-1 Advanced? 
How can you display the security status of the CP1628 over the Online View in the Security Configuration Tool (SCT)? 
What remedies are there for weak points in WinCC flexible 2008 and WinCC V11? 
Where can you find information on the topic of "Industrial Security"? 

What should you watch out for when you enable the "SNMP" function in the configuration of the security module?Go to beginning
Part number:

Description
The security module supports the transfer of management information over the Simple Network Management Protocol (SNMP). For this, there is an "SNMP agent" installed on the security module and this receives and answers the SNMP requests.
Information about the properties of SNMP-compatible devices is available in the so-called MIB files (Management Information Base), but the user must have the necessary rights for this.

SNMPv1
With SNMPv1 a "Community String" is also sent. The "Community String" is like a password sent together with the SNMP request. If the "Community String" is correct, the security module answers with the requested information. If the "Community String" is incorrect, the security module rejects the request and does not answer.

The security modules use the standard values for the community strings below to control the access rights in the SNMP agent:

  • For read access: Public
  • For read and write access: Private

Note
In the Security Configuration Tool (SCT) the write access over the "Private" community string can be configured by enabling the "Allow write access via community string "private"". The SCALANCE S V3 security modules do not support writing of values over SNMP and do not react to written access attempts. There is no error message nor inconsistency of the projected if you store the settings.


Fig. 01

SNMPv3
With SNMPv3 you can transfer the data encrypted to the network analysis. The security module SCALANCE S does not support writing of values over SNMP.

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information is available in Entry ID: 50203404.

Additional Information
Detailed information about Industrial Ethernet Security is available in the manual "SIMATIC NET Industrial Ethernet Security Basics and Applications Configuration Manual" in Entry ID 56577508.

Which security modules support dynamic DNS and can use it to communicate with each other?Go to beginning
Part number:

Description
Using dynamic DNS you can access a module with dynamic IP address over the Fully Qualified Domain Name (FQDN).

The security module reports the current WAN IP over which the module can be reached to a provider for dynamic DNS (DynDNS.org, no-ip.com, for example). The provider makes sure that DNS queries to the FQDN of the module are answered with the WAN IP of the module.

The overview below shows which security modules support dynamic DNS as VPN server and VPN client and can use it to communicate with each other.
 
VPN client VPN server
SCALANCE S V3 SCALANCE M875
MD741-1
SOFTNET Security Client (SSC) yes2) yes1)
SCALANCE S V3
SCALANCE M875
MD741-1
yes yes
Table 01

1) Communication using dynamic DNS is possible with SSC V3 onwards.
2) Communication using dynamic DNS is possible with SSC V4 onwards.

Note

  • The CPx43-1 Advanced does not support dynamic DNS.

  • The SCALANCE S V3 is not a DNS client. It can only transmit its current IP address to the DNS server, but cannot resolve any domain names.

  • The SCALANCE S V3 supports the following providers: DynDNS.org, non-ip.com or a freely defined service.

  • The SCALANCE M875 is compatible with the DNS services of the provider DynDNS.org. For dynDNS the M875 needs a public IP address that can be reached from the internet.

Additional information
More information about the security modules is available in the manuals below.
 
Manual Entry ID
Where can you find information on the topic of "Industrial Security"? 50203404
SIMATIC NET Industrial Ethernet Security SCALANCE S V3.0 Installation and Commissioning Manual 56576669
SIMATIC NET Industrial Ethernet Security Basics and Applications Configuration Manual 56577508
SIMATIC NET Industrial Ethernet Security Getting Started 60166939
UMTS Router with HSDPA SCALANCE M873-0 49507278
SIMATIC NET Telecontrol SCALANCE M875 Operating Instructions 58122394
SIMATIC NET S7-400 - Industrial Ethernet CP 443-1 Advanced (GX30) Device Manual Part B 59187252
SIMATIC NET S7-300 - Industrial Ethernet S7 CPs for Industrial Ethernet
CP 343-1 Advanced (GX30) Device Manual Part B
61199572
Table 02

Why does the VPN LED of the SCALANCE M875 and MD741-1 continue to light although the secure IPsec tunnel connection is disconnected?Go to beginning
Part number:

Description
The VPN LED of the SCALANCE M875 indicates whether or not a VPN connection is established.

If the SOFTNET Security Client (SSC) establishes a secure IPsec tunnel connection to the SCALANCE M875, the VPN LED of the M875 lights. The IPsec tunnel connection is monitored by the Dead Peer Detection (DPD). The SSC does not support the DPD. In this way the VPN LED of the M875 does not go out when the IPsec tunnel connection of the SSC is disconnected, but only when the certificate lifetime has expired.

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information is available in Entry ID: 50203404.

Additional information

  • More information about SCALANCE M875 is available in the manual "SIMATIC NET Telecontrol SCALANCE M875 Operating Instructions" in Entry ID 58122394.
  • More information about configuring secure IPsec tunnel connections between the security modules is available in the manual "SIMATIC NET Industrial Ethernet Security Basics and Applications Configuration Manual" in Entry ID: 56577508.

What should you watch out for when enabling and using the security functions of CP343-1 Advanced and CP443-1 Advanced?Go to beginning
Part number:

Description
By combining different security functions such as firewall, NAT/NAPT router and VPN (Virtual Private Network) over IPsec tunnel the CPx43-1 Advanced protects individual S7-400 stations, S7-300 stations and even complete automation cells against unauthorized access.

When you enable and use the security functions of the CPx43-1 Advanced you ensure that the CP has the current time and current date. Having the current time and date is extremely important for verifying the validity of the certificates used, for example, when you establish a secure IPsec tunnel connection to one or more security modules.
If you do not take the time from the station (CPU), you can synchronize the time using a SIMATIC procedure or the Network Time Protocol (NTP).

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information is available in Entry ID: 50203404.

Additional Information
More information about time synchronization is available in the entries below.
 
Subject Entry ID
How do you configure the SIMATIC S7-300 as time master or time slave for time-of-day synchronization via Industrial Ethernet in SIMATIC mode? 44049612
How do you configure the SIMATIC S7-400 as time master or time slave for time-of-day synchronization via Industrial Ethernet in SIMATIC mode? 18130164
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization? 17990844

How can you display the security status of the CP1628 over the Online View in the Security Configuration Tool (SCT)?Go to beginning
Part number:

Description
The CP1628 enables safe connection to the Industrial Ethernet for SIMATIC PG/PC and PCs with PCI Express slot.

The security functions of the CP1628 are configured in the Security Configuration Tool (SCT).

Local and remote diagnostics of a CP1628
The SCT enables you to diagnose a CP1628 locally or remotely. You can have the security status of the CP1628 displayed in the Online View of the SCT.
The document below describes 3 scenarios of the local and remote diagnostics of one or more CP1628s:

  • Local and remote diagnostics of a CP1628 when the NDIS IP address and the Industrial Ethernet IP address of the module are in the same subnet.
  • Local and remote diagnostics of a CP1628 when the NDIS IP address and the Industrial Ethernet IP address of the module are in the same subnet.
  • Local and remote diagnostics of several CP1628 when the NDIS IP address and the Industrial Ethernet IP address of the module are not in the same subnet.

NET_OnlineDiagnostic_CP1628_with_SCT_en.pdf ( 1116 KB )

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information is available in Entry ID: 50203404.

What remedies are there for weak points in WinCC flexible 2008 and WinCC V11?Go to beginning
Part number:

Description
Siemens has analyzed the weak points in the web server of the Runtime system of SIMATIC WinCC flexible and WinCC (TIA Portal) and has prepared remedies.
There are remedies for the weak points available in the WinCC flexible Runtime versions 2004 to 2008 SP2, WinCC Runtime Advanced V11 and SIMATIC Panels (TP, OP, MP, Comfort Panels).

Information about the remedies and updates is available at the following links:

  • SIMATIC WinCC flexible 2008 Service Pack 3 - Information about delivery release (Entry ID: 57267466)
  • Update for WinCC V11 SP2 (Entry ID: 58112582)
  • Update for WinCC Runtime Advanced V11 SP2 (Entry ID: 58112587)

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

Additional Keywords
Security note

Where can you find information on the topic of "Industrial Security"?Go to beginning
Part number:

Description
This entry provides an overview of:

Industrial Security
The growing networking of industrial plants increases productivity. At the same time, however, IT security risks increase likewise, which must be tackled with appropriate protective mechanisms for Industrial Security. It is essential here to have an overall perception that includes both technical measures and staff training as well as the definition of guidelines and processes. This is necessary to achieve optimum security and ensure secure operation of the plant.
More information about technical solutions and our service offering for industrial security is available in the internet at:
http://www.industry.siemens.com/industrial-security

Applications & Tools
The Applications & Tools below provide information on the topic of "Industrial Security".
 
Applications & Tools Description Entry ID
Security with SIMATIC NET This application provides an overview of possible security configurations in the Local Area Network (LAN) and WAN (Wide Area Network) with SCALANCE S61x modules and the SOFTNET security client. 27043887
Industrial Security with SCALANCE S modules via IPSec VPN tunnel (Configuration 4) These applications show safe teleservicing with SCALANCE S via a Virtual Private Network (VPN). 22056713
Secure remote access to SIMATIC stations via Internet and EGPRS router MD741-1 and SCALANCE S612 (Configuration 9)  24960449
Protection of an automation cell by the Security Module SCALANCE S602 via firewall (bridge/routing) (Configuration 5) This application shows the configuration of a secure automation cell with SCALANCE S firewall. 22376747
SINAUT ST7 Telecontrol sample configurations in Ethernet, secure Internet and (E)GPRS environment (Configuration 8) This application shows the configuration of secure internet connections for Telecontrol stations with SINAUT ST7 23810112
User login on the operator panel via HMI-RFI This application shows how to carry out a secure user login on an operator panel with an HMI-RFI (card reader). 35214239
Diagnostics and teleservicing of SIMATIC Industry PCs This application shows you how to use the teleservicing option with SIMATIC Industry PCs and the integrated Intel AMT technology. 52310936
Table 01

Microsoft Security Updates
The entries below provide information about using Microsoft Security Updates together with WinCC, PCS 7, SIMOTION and SINUMERIK.
 
Product Entry title Entry ID
WinCC Which Microsoft Security Patches are released for use with SIMATIC WinCC? 18752994
PCS 7 Which Microsoft Security Patches have been tested for compatibility with SIMATIC PCS 7? 18490004
SIMOTION SIMOTION P350: Compatibility of Microsoft security patches 22159441
SINUMERIK   SINUMERIK 810D/840Di/840D: Compatibility of Microsoft security patches with SINUMERIK PCU 50/70 19739695
Table 02

Virus Protection
The manuals and entries below provide information about virus protection for PCS 7 and SINUMERIK.
 
Product Entry or manual title Entry ID
STEP 7
STEP 7 V5.3, V5.4 and V5.5. Which virus scanner versions can you use for STEP 7 V5.3, V5.4 and V5.5? 37208360
PCS 7
Trend Micro Office Scan SIMATIC Process Control System PCS 7 Configuration Trend Micro Office Scan V7.3 incl. Patch 2 38006151
Configuration Trend Micro OfficeScan V8.0 38006929
Symantec AntiVirus SIMATIC Process Control System PCS 7 Configuration Symantec AntiVirus V10.2 38006339
Symantec Endpoint Protection SIMATIC Process Control System PCS 7 Configuration Symantec Endpoint Protection 11.0 38004530
McAfee VirusScan SIMATIC Process Control System PCS 7 Configuration McAfee VirusScan (V8.5; V8.5i; V8.7) 38006821
SINUMERIK  
SINUMERIK   Notes on virus protection for SINUMERIK 840D sl / 840Di sl 19577116
Table 03

Whitelisting Protection Mechanisms
The entries below provide information about using whitelisting protection mechanisms with SIMATIC products.
 
Product Entry title Entry ID
STEP 7 V5.5 Using whitelisting protection mechanisms with SIMATIC products 49382928
PCS7 V7.1 + SP2
WinCC V7.0 + SP1
WinCC V7.0 + SP2
WinCC flexible 2008 + SP2
Table 04

Firewall
The entries below provide information about configuring a firewall.
 
Product Entry title Entry ID
SCALANCE S Which firewall rules should you configure for SCALANCE S in order to have access to the internet with the PG/PC via the SCALANCE and router? 26517928
Which firewall rules do you have to define for SCALANCE S in the Security Configuration Tool to allow data traffic between internal and external networks for a specific IP address area? 34675703
EGPRS Router Which firewall rules should you configure for the EGPRS router MD741-1 in order to have access to the internet with the PG/PC from the LAN of the MD741-1? 31525978
Security Configuration Tool What are the restrictions when configuring the bandwidth limit of a firewall rule with the Security Configuration Tool V2.1? 27080202
Table 05

Virtual Private Network (VPN)
The entries below provide information about configuring a Virtual Private Network (VPN) with SCALANCE S and SOFTNET Security Client.
 
Product Entry title Entry ID
SOFTNET Security Client How do you configure a VPN tunnel between a PC station and SCALANCE S61x via the internet with the 2008 edition of SOFTNET Security Client? 32447942
How do you configure a VPN tunnel between a PC station and SCALANCE S61x V2.1 via the internet with the SOFTNET Security Client Edition 2005 HF1? 24953806
SCALANCE S How is a VPN tunnel between two SCALANCE S S 61x modules configured in Routing mode via the internet? 24968210
How do you configure a VPN tunnel between a PC station with Windows XP SP2 and SCALANCE S61x V2.1 via the internet with the Microsoft Management Console? 26098354
What can you do if there is no VPN tunnel set up in the SCALANCE S 61x, the SOFTNET Security Client or the MD740-1? 26361542
What configuration steps are necessary to forward the coded data packages incoming on the SCALANCE S61x from the VPN tunnel to specific internal nodes only? 24533873
Table 06  

Access Control
The entries below provide information about access control in process control systems like PCS 7.
 
Product Entry title Entry ID / Link
WinCC / PCS 7 Process Control System Which safety precautions help against unauthorized access in the SIMATIC PCS 7 / WinCC environment? 44443744
WinCC / PCS 7 SCADA System
PCS 7 Process Control System Security concept 60119725
Table 07

Remote Access via Internet, Gateways
The entries below provide information about Remote Access via the internet and you you can use an Industrial Ethernet CP or SCALANCE S as a gateway.
 
Product Entry title Entry ID
Remote Access with WinCC flexible What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the internet (WAN)? 19865167
Industrial Ethernet CP or SCALANCE S as Gateway How do you use an Industrial Ethernet CP or SCALANCE S as a gateway? 45632056
Table 08

Stuxnet
The entries below provide information about the latest developments and the measures recommended by Siemens for handling Stuxnet.
 
Product Entry title Entry ID
WinCC / PCS 7 SIMATIC WinCC / SIMATIC PCS 7: Information about malware / viruses / Trojan horses 43876783
SIMOTION SIMOTION: Latest information about malware / viruses / Trojan horses 44050544
SINUMERIK   SINUMERIK PCU: Latest information about malware / viruses / Trojan horses 44050056
Table 09

Protection against Manipulation
Information about how to recognize and prevent program code manipulation in STEP 7 V5.5 is available in Entry ID: 51577287.

 Entry ID:57351029   Date:2012-09-04 
I regard this article....as helpfulas not helpful                                 






























related links
SIMATIC PCS 7 process control sy ...
Security with SIMATIC NET
Which safety precautions help aga ...
SIMATIC Process Control System PC ...
Software update with utilization ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour