Problem
SIMATIC S7-1200 can be operated as PROFINET controller as well as
PROFIBUS master (with CM 1243-5). As PROFINET device respectively
as PROFIBUS slave a SINAMICS G120C is to be employed. The PLC shall
have read/write access to the process data (control word and speed
setpoint respectively status word and actual speed) and parameters
of the drive.
Figure 1: PROFINET connection
Figure 2: PROFIBUS connection
Solution
This application example includes a PROFINET project and a PROFIBUS
project. It demonstrates how to connect a SINAMICS G120C PN or a
G120C DP to a
SIMATIC S7-1200. The drive integration into the STEP 7 program is
done by GSDML/GSD files. You can apply the used function blocks
directly with your own applications.
The G120C is configured with STARTER. In the PROFINET version this
is done via Ethernet, in the PROFIBUS version via USB.
Downloads
Security Notice
Caution The functions and solutions described in this
article confine themselves to the realization of the automation
task predominantly. Please take into account furthermore that
corresponding protective measures have to be taken up in the
context of Industrial Security when connecting your equipment to
other parts of the plant, the enterprise network or the Internet.
Further information can be found under the Entry-ID 50203404.
Last Changes Addition of an application example with
PROFINET connection.
Revision of the PROFIBUS version.
Extended to TIA Portal V12.
Additional Keywords motioncontrol_apc_applications
|